TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Data Fields
snpCharWriteCnf_t Struct Reference

Parameter Structure for SNP_writeCharCnf / SNP_CHAR_WRITE_CNF. More...

Data Fields

uint16_t connHandle
 2 Byte Handle of the connection
 
uint8_t status
 1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.)
 

Detailed Description

Parameter Structure for SNP_writeCharCnf / SNP_CHAR_WRITE_CNF.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale