TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Files | Functions
SNP GATT API

Files

file  simple_np_gatt.h
 SNP GATT Layer API.
 

Functions

uint8_t SNP_addCharValueDecl (snpAddCharValueDeclReq_t *pReq, uint8_t uuidLen, snpAddCharValueDeclRsp_t *pRsp)
 SNP Add Characteristic Value Declaration. More...
 
uint8_t SNP_addDescriptionValue (snpAddCharDescDeclReq_t *lDescReq, snpAddCharDescDeclRsp_t *lDescRsp)
 SNP Add Characteristic Descriptor Declaration. More...
 
uint8_t SNP_addService (snpAddServiceReq_t *pReq, uint8_t uuidLen, snpAddServiceRsp_t *pRsp)
 SNP Add Service. More...
 
uint8_t SNP_getAttrValue (snpGetAttrValueReq_t *pReq, snpGetAttrValueRsp_t *pRsp, uint16_t *pDataLenght)
 SNP Get Attribute Value. More...
 
uint8_t SNP_getGATTParam (snpGetGattParamReq_t *pReq, snpGetGattParamRsp_t *pRsp, uint16_t *pDataLen)
 SNP Get GATT Parameter. More...
 
uint8_t SNP_processCharConfigUpdatedCnf (snpCharCfgUpdatedRsp_t *pReq)
 SNP Characteristic Configuration Update Confirm (0x8B) More...
 
uint8_t SNP_readCharCnf (snpCharReadCnf_t *pReq, uint16_t dataSize)
 SNP Read Characteristic Confirmation. More...
 
uint8_t SNP_registerService (snpRegisterServiceRsp_t *pRsp)
 SNP Register Service. More...
 
uint8_t SNP_sendNotifInd (snpNotifIndReq_t *pCmdStruct, int16_t length)
 SNP Send Notification Indication. More...
 
uint8_t SNP_setAttrValue (snpSetAttrValueReq_t *pReq, uint16_t dataLenght, snpSetAttrValueRsp_t *pRsp)
 SNP Set Attribute Value. More...
 
uint8_t SNP_setGATTParam (snpSetGattParamReq_t *pReq, uint16_t reqDataLen, snpSetGattParamRsp_t *pRsp)
 SNP Set GATT Parameter. More...
 
uint8_t SNP_writeCharCnf (snpCharWriteCnf_t *pReq)
 SNP Write Characteristic Confirmation. More...
 

Detailed Description

Function Documentation

§ SNP_addCharValueDecl()

uint8_t SNP_addCharValueDecl ( snpAddCharValueDeclReq_t pReq,
uint8_t  uuidLen,
snpAddCharValueDeclRsp_t pRsp 
)

SNP Add Characteristic Value Declaration.

AP -> NP (SNP_addCharValueDecl)

CMD 0 CMD 1
0x35 0x82
SNP_NPI_SYNC_REQ_TYPE SNP_ADD_CHAR_VAL_DECL_REQ

NP -> AP (SNP_addCharValueDecl)

CMD 0 CMD 1
0x75 0x82
SNP_NPI_SYNC_RSP_TYPE SNP_ADD_CHAR_VAL_DECL_RSP

This command is sent to the SNP to add the two Bluetooth Specification mandatory attributes for a characteristic:

  • characteristic value
  • characteristic declaration

This command should be sent after SNP_addService (0x81) command has been sent to begin service declaration.

It is possible to add optional attributes to the characteristic using SNP_addDescriptionValue (0x83) command.

Additional Notes

This command must be called before adding additional attributes with SNP_addDescriptionValue (0x83).

If the GATT Notify or GATT Indicate properties are enabled, a CCCD characteristic must be added with the SNP_addDescriptionValue (0x83) command.

The TI BLE Stack expects the properties to be aligned logically with the permissions. For example, a characteristic with read properties would most likely have read permissions.

Corresponding Events/Commands
SNP_ADD_CHAR_VAL_DECL_REQ (from AP) | SNP_ADD_CHAR_VAL_DECL_RSP (from SNP)
Payload Structures

AP -> NP
snpAddCharValueDeclReq_t

Size Description
1 Byte Permissions of the value attribute GATT Attribute Access Permissions Bit Fields
2 Byte Properties of the value attribute GATT Characteristic Properties Bit Fields
1 Byte Reserved
2 Byte Reserved
2 Byte 2 Byte UUID dealing with UUID

NP -> AP
snpAddCharValueDeclRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
2 Byte Attribute Handle
Parameters
[in]pReq: Add Characteristic Value & Declaration Request Structure snpAddCharValueDeclReq_t
[in]uuidLen: 1 Byte UUID Length of Service
[out]pRsp: Add Characteristic Value & Declaration Response Structure snpAddCharValueDeclRsp_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_addDescriptionValue()

uint8_t SNP_addDescriptionValue ( snpAddCharDescDeclReq_t lDescReq,
snpAddCharDescDeclRsp_t lDescRsp 
)

SNP Add Characteristic Descriptor Declaration.

AP -> NP (SNP_addDescriptionValue)

CMD 0 CMD 1
0x35 0x83
SNP_NPI_SYNC_REQ_TYPE SNP_ADD_CHAR_DESC_DECL_REQ

NP -> AP (SNP_addDescriptionValue)

CMD 0 CMD 1
0x75 0x83
SNP_NPI_SYNC_RSP_TYPE SNP_ADD_CHAR_DESC_DECL_RSP

This command is used to add one or more of the following attributes to a characteristic:

User Description String
CCCD
Presentation format
Server Characteristic Config (Reserved)
Aggregate format
Generic Attribute using short UUID
Generic Attribute using long UUID

For User Description String, the attribute permissions is forced to be read-only.

Additional Notes

All those attributes are optional. At least one needs to be added when using this command.
CCCD, Presentation Format, and User Description String attributes can be added once for each characteristic.
Trying to create a second will lead to a SNP_CMD_REJECTED.

If the NOTIFY and INDICATE properties are enabled by the CCCD attribute, and a GATT Clint writes to this attribute - SNP_writeCharCnf is forwarded to AP. AP must then determine if the write is authorized and send write to the attribute via SNP_setGATTParam.

Corresponding Events/Commands
SNP_ADD_CHAR_DESC_DECL_REQ (from AP) | SNP_ADD_CHAR_DESC_DECL_RSP (from SNP)
Payload Structures

AP -> NP
snpAddCharDescDeclReq_t

Size Description
1 Byte Header of Attributes to add SNP GATT Descriptors Header
X Byte Depending on Header, the length can very

NP -> AP
snpAddCharDescDeclRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
1 Byte Header of Added Attributes SNP GATT Descriptors Header
X Byte Handles of Attributes added, depending on header
Related Structures

snpAddCharDescDeclReq_t for SNP_ADD_CHAR_DESC_DECL_REQ
snpAddCharDescDeclRsp_t for SNP_ADD_CHAR_DESC_DECL_RSP
snpAddAttrGenShortUUID_t for Short UUID
snpAddAttrGenLongUUID_t for Long UUID
snpAddAttrCccd_t for CCCD
snpAddAttrFormat_t for Presentation Format
snpAddAttrUserDesc_t for User Description

Parameters
[in]lDescReq: Add Descriptor Request Structure, snpAddCharDescDeclReq_t
[out]lDescRsp: Add Descriptor Response Structure, snpAddCharDescDeclRsp_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_addService()

uint8_t SNP_addService ( snpAddServiceReq_t pReq,
uint8_t  uuidLen,
snpAddServiceRsp_t pRsp 
)

SNP Add Service.

AP -> NP (SNP_addService)

CMD 0 CMD 1
0x35 0x81
SNP_NPI_SYNC_REQ_TYPE SNP_ADD_SERVICE_REQ

NP -> AP (SNP_addService)

CMD 0 CMD 1
0x75 0x81
SNP_NPI_SYNC_RSP_TYPE SNP_ADD_SERVICE_RSP

The SNP Add Service command is sent to the SNP to start the addition of a new service to the GATT server running on the SNP.

This command should be followed by SNP_addCharValueDecl (0x82) command and optionally SNP_addDescriptionValue (0x83) command to add characteristics to the service.

Lastly, when all characteristics have been added, SNP_registerService (0x84) command should be sent to the device.

Only one service can be added at a time. That is, once this command has been sent, all characteristics must then be added and the service must to be registered before adding another service.

Additional Notes

Services and characteristic cannot be added if the Device has started.
Device is started when SNP_startAdv or SNP_setAdvData is send to the SNP.
Once started, the only way to stop the device is to reset it.

When NP is reset, all previously added services and characteristics are lost.

Corresponding Events/Commands
SNP_ADD_SERVICE_REQ (from AP) | SNP_ADD_SERVICE_RSP (from SNP)
Payload Structures

AP -> NP
snpAddServiceReq_t

Size Description
1 Byte Type of the service to add Service Type
2 Byte 2 Byte UUID dealing with UUID

NP -> AP
snpAddServiceRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
Parameters
[in]pReq: Add Service Request Structure, snpAddServiceReq_t
[in]uuidLen: 1 Byte UUID Length of Service
[out]pRsp: Add Service Response Structure, snpAddServiceRsp_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_getAttrValue()

uint8_t SNP_getAttrValue ( snpGetAttrValueReq_t pReq,
snpGetAttrValueRsp_t pRsp,
uint16_t *  pDataLenght 
)

SNP Get Attribute Value.

AP -> NP (SNP_getAttrValue)

CMD 0 CMD 1
0x35 0x85
SNP_NPI_SYNC_REQ_TYPE SNP_GET_ATTR_VALUE_REQ

NP -> AP (SNP_getAttrValue)

CMD 0 CMD 1
0x75 0x85
SNP_NPI_SYNC_RSP_TYPE SNP_GET_ATTR_VALUE_RSP

This command is sent to the SNP to retrieve the value of an attribute on the GATT server. This includes non-user added Services, the Device Information Service and the Generic Access Service.

This command can only be used to get read from User Description and Presentation Format Attributes. These attribute values are stored on SNP. Other attribute values are Reserved for Future Use.

For getting the value of a SNP managed attribute, the command SNP_getAttrValue (0x8D) should be used.

Corresponding Events/Commands
SNP_GET_ATTR_VALUE_REQ (from AP) | SNP_GET_ATTR_VALUE_RSP (from SNP)
Payload Structures

AP -> NP
snpGetAttrValueReq_t

Size Description
2 Byte Attribute Handle to get Value from

NP -> AP
snpGetAttrValueRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
2 Byte Attribute Handle of where Value is from
X Byte Value of the Attribute Handle
Parameters
[in]pReq: Get Attribute Value Request Structure, snpGetAttrValueReq_t
[out]pRsp: Get Attribute Value Response Structure, snpGetAttrValueRsp_t
[out]pDataLenght: Length in Bytes of snpGetAttrValueRsp_t::pData
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_getGATTParam()

uint8_t SNP_getGATTParam ( snpGetGattParamReq_t pReq,
snpGetGattParamRsp_t pRsp,
uint16_t *  pDataLen 
)

SNP Get GATT Parameter.

AP -> NP (SNP_getGATTParam)

CMD 0 CMD 1
0x35 0x8D
SNP_NPI_SYNC_REQ_TYPE SNP_GET_GATT_PARAM_REQ

NP -> AP (SNP_getGATTParam)

CMD 0 CMD 1
0x75 0x8D
SNP_NPI_SYNC_RSP_TYPE SNP_GET_GATT_PARAM_RSP

This command is used to get the value of a Characteristic Value attribute from a characteristic managed by SNP GATT Server. This includes non-user added Services, the Device Information Service and the Generic Access Service.

For reading other types of Attributes, use SNP_getAttrValue (0x85)

For writing the value of a Characteristic Value Attribute, use SNP_setGATTParam (0x8C)

Corresponding Event
SNP_GET_GATT_PARAM_RSP
Payload Structures

AP -> NP
snpGetGattParamReq_t

Size Description
1 Byte Service ID containing parameter Predefined services
2 Byte Parameter ID to get data from

NP -> AP
snpGetGattParamRsp_t

Size Description
1 Byte Service ID containing parameter Predefined services
2 Byte Parameter ID to get data from
X Byte Parameter Data
Parameters
[in]pReq: Get GATT Parameter Request Structure, snpGetGattParamReq_t
[out]pRsp: Get GATT Parameter Response Structure, snpGetGattParamRsp_t
[out]pDataLen: Length in Bytes of snpGetGattParamRsp_t::pData
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_processCharConfigUpdatedCnf()

uint8_t SNP_processCharConfigUpdatedCnf ( snpCharCfgUpdatedRsp_t pReq)

SNP Characteristic Configuration Update Confirm (0x8B)

NP -> AP (N/A)

CMD 0 CMD 1
0x55 0x8B
SNP_NPI_ASYNC_CMD_TYPE SNP_CCCD_UPDATED_IND

AP -> NP (SNP_processCharConfigUpdatedCnf)

CMD 0 CMD 1
0x55 0x8B
SNP_NPI_ASYNC_CMD_TYPE SNP_CCCD_UPDATED_CNF

The SNP_CCCD_UPDATED_IND event is sent from the SNP when the remote GATT Client has requested to update the CCCD value added by the AP.

Upon receiving this event, if snpCharCfgUpdatedRsp_t::rspNeeded is SNP_RESPONSE_NEEDED then within 30 seconds the AP must:

  • determine if CCCD update is allowed by application-specific rules
  • send this command / SNP_CCCD_UPDATED_CNF with the proper parameters

If there is no response within 30 seconds, an ATT timeout will occur and BLE connection will be lost.

AP is responsible for remembering the CCCD value, accept/decline authorize the CCCD, and if associated characteristic value changes, the AP must send out notification or indication of the change.

If snpCharCfgUpdatedRsp_t::rspNeeded is SNP_RESPONSE_NOT_NEEDED then no response is needed.

Corresponding Event
SNP_CCCD_UPDATED_IND (from SNP) | SNP_CCCD_UPDATED_CNF (from AP)
Payload Structures

NP -> AP
snpCharCfgUpdatedInd_t

Size Description
2 Byte Connection Handle generating request to write
2 Byte Handle to CCCD attribute being written to
1 Byte Indicate if Response is Needed from AP Options for Response Needed Field
2 Byte Value to write to CCCD

AP -> NP
snpCharCfgUpdatedRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
2 Byte Connection Handle generating request to read
Parameters
[in]pReq: structure of the confirmation, see snpCharCfgUpdatedRsp_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_readCharCnf()

uint8_t SNP_readCharCnf ( snpCharReadCnf_t pReq,
uint16_t  dataSize 
)

SNP Read Characteristic Confirmation.

NP -> AP (N/A)

CMD 0 CMD 1
0x55 0x87
SNP_NPI_ASYNC_CMD_TYPE SNP_CHAR_READ_IND

AP -> NP (SNP_readCharCnf)

CMD 0 CMD 1
0x55 0x87
SNP_NPI_ASYNC_CMD_TYPE SNP_CHAR_READ_CNF

If a GATT client requests a read of a characteristic that was added by the AP, the SNP GATT server will forward an SNP_CHAR_READ_IND (0x87) to the AP.

The AP then has 30 seconds to do the following:

If no response occurs in 30 seconds, an ATT timeout will occur and BLE connection will be lost.

Corresponding Event
SNP_CHAR_READ_IND (from SNP) | SNP_CHAR_READ_CNF (from AP)
Payload Structures

NP -> AP
snpCharReadInd_t

Size Description
2 Byte Connection Handle generating request to read
2 Byte Attribute Handle of Characteristic Value to read from
2 Byte Offset in Bytes
2 Byte Max Size of Data to read

AP -> NP
snpCharReadCnf_t

Size Description
1 Byte Status list of status generated by the SNP.
2 Byte Connection Handle generating request to read
2 Byte Attribute Handle of Characteristic Value to read
2 Byte Offset in Bytes
X Byte Data to write to characteristic
Parameters
[in]pReq: Read Characteristic Confirmation Structure, snpCharReadCnf_t
[in]dataSize: Length in Bytes of snpCharReadCnf_t::pData
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_registerService()

uint8_t SNP_registerService ( snpRegisterServiceRsp_t pRsp)

SNP Register Service.

AP -> NP (SNP_registerService)

CMD 0 CMD 1
0x35 0x84
SNP_NPI_SYNC_REQ_TYPE SNP_REGISTER_SERVICE_REQ

NP -> AP (SNP_registerService)

CMD 0 CMD 1
0x75 0x84
SNP_NPI_SYNC_RSP_TYPE SNP_REGISTER_SERVICE_RSP

This command should be sent to the device to register the previously added service and characteristics to the devices GATT server.

This command should be sent after SNP_addService and SNP_addCharValueDecl; along with any optional attributes desired from SNP_addDescriptionValue.

When NP is reset, all previously added services and characteristics are lost.

Corresponding Events/Commands
SNP_REGISTER_SERVICE_REQ (from AP) | SNP_REGISTER_SERVICE_RSP (from SNP)
Payload Structures

AP -> NP
No Parameter Structure

NP -> AP
snpRegisterServiceRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
2 Byte Start Handle of the Registered Service
2 Byte End Handle of Registered Service
Parameters
[out]pRsp: Register Service Response Structure, snpRegisterServiceRsp_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_sendNotifInd()

uint8_t SNP_sendNotifInd ( snpNotifIndReq_t pCmdStruct,
int16_t  length 
)

SNP Send Notification Indication.

AP -> NP (SNP_sendNotifInd)

CMD 0 CMD 1
0x55 0x89
SNP_NPI_ASYNC_CMD_TYPE SNP_SEND_NOTIF_IND_REQ

NP -> AP (N/A)

CMD 0 CMD 1
0x55 0x89
SNP_NPI_ASYNC_CMD_TYPE SNP_SEND_NOTIF_IND_CNF

This command is used to request SNP to send a Notification or Indication to the GATT Client. This is only possible if a CCCD for the characteristic has been created and notifications / indications have been enabled by the GATT Client writing to the CCCD.

If CCCD Attribute of a characteristic is not configured correctly, the GATT server may not send out notification or indication.

Indications require a confirmation from the GATT client. Thus only one indication can be sent at a time. Once confirmation is received, it is then forwarded to AP via SNP_SEND_NOTIF_IND_CNF with a SNP_SUCCESS.

If no confirmation is received from the GATT Client within 30 seconds, SNP_SEND_NOTIF_IND_CNF with a SNP_FAILURE will be sent back to AP. An ATT timeout will also occur, dropping the BLE connection.

Notifications don't require a confirmation from the GATT Client. SNP will produce a SNP_SEND_NOTIF_IND_CNF with a SNP_SUCCESS when command has been forwarded to BLE-Stack Host.

Additional Notes

The maximum size possible for a notification or indication value is ATT_MTU_SIZE. If the value sent is larger than ATT_MTU_SIZE bytes, it will be truncated.

Corresponding Event
SNP_SEND_NOTIF_IND_REQ (from AP) | SNP_SEND_NOTIF_IND_CNF (from SNP)
Payload Structures

AP -> NP
snpNotifIndReq_t

Size Description
2 Byte Connection Handle to send Notification/Indication
2 Byte Attribute Handle of Characteristic Value to notify/indicate
1 Byte Reserved
1 Byte Type of the Request SNP indication type
X Byte Characteristic Value to Send

NP -> AP
snpNotifIndCnf_t

Size Description
1 Byte Status list of status generated by the SNP.
2 Byte Connection Handle Notified/Indicated
Parameters
[in]pCmdStruct:Parameter Structure for Notification/Indication, snpNotifIndReq_t
[in]length:Length in Bytes of snpNotifIndReq_t::pData
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_setAttrValue()

uint8_t SNP_setAttrValue ( snpSetAttrValueReq_t pReq,
uint16_t  dataLenght,
snpSetAttrValueRsp_t pRsp 
)

SNP Set Attribute Value.

AP -> NP (SNP_setAttrValue)

CMD 0 CMD 1
0x35 0x86
SNP_NPI_SYNC_REQ_TYPE SNP_SET_ATTR_VALUE_REQ

NP -> AP (SNP_setAttrValue)

CMD 0 CMD 1
0x75 0x86
SNP_NPI_SYNC_RSP_TYPE SNP_SET_ATTR_VALUE_RSP

This command is sent to the SNP in order to write the value of an attribute on the GATT server. This includes non-user added Services, the Device Information Service and the Generic Access Service.

This command can only be used to write User Description and Presentation Format Attributes.

For writing to Characteristic Value Attributes, use SNP_setGATTParam (0x8C)

For reading the value of a SNP managed attribute, the command SNP_getAttrValue (0x85) should be used.

Corresponding Events/Commands
SNP_SET_ATTR_VALUE_REQ (from AP) | SNP_SET_ATTR_VALUE_RSP (from SNP)
Payload Structures

AP -> NP
snpSetAttrValueReq_t

Size Description
2 Byte Attribute Handle to get Value from
X Byte Value to Set the Attribute

NP -> AP
snpSetAttrValueRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
2 Byte Attribute Handle of where Value is from
Parameters
[in]pReq: Set Attribute Value Request Structure, snpSetAttrValueReq_t
[in]dataLenght: Length in Bytes of snpSetAttrValueReq_t::pData
[out]pRsp: Set Attribute Value Response Structure, snpSetAttrValueRsp_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_setGATTParam()

uint8_t SNP_setGATTParam ( snpSetGattParamReq_t pReq,
uint16_t  reqDataLen,
snpSetGattParamRsp_t pRsp 
)

SNP Set GATT Parameter.

AP -> NP (SNP_setGATTParam)

CMD 0 CMD 1
0x35 0x8C
SNP_NPI_SYNC_REQ_TYPE SNP_SET_GATT_PARAM_REQ

NP -> AP (SNP_setGATTParam)

CMD 0 CMD 1
0x75 0x8C
SNP_NPI_SYNC_RSP_TYPE SNP_SET_GATT_PARAM_RSP

This command is used to write the attribute value of a characteristic managed on the SNP GATT Server. This includes non-user added Services, the Device Information Service and the Generic Access Service.

This command can only write to Characteristic Value attributes.

For other types of Attributes, use SNP_setAttrValue (0x86)

For reading the value of a SNP managed attribute, the command SNP_getAttrValue (0x85) should be used.

Additional Information

The SNP_setGATTParam::reqDataLen should never exceed the maximum length of the attribute value

Corresponding Event
SNP_SET_GATT_PARAM_REQ (from AP) | SNP_SET_GATT_PARAM_RSP (from SNP)
Payload Structures

AP -> NP
snpSetGattParamReq_t

Size Description
1 Byte Service ID containing parameter Predefined services
2 Byte Parameter ID
X Byte Value to Set the Parameter

NP -> AP
snpSetGattParamRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
Parameters
[in]pReq: Set GATT Parameter Request Structure, snpSetGattParamReq_t
[in]reqDataLen: Length in Bytes of snpSetGattParamReq_t::pData
[out]pRsp: Set GATT Parameter Response Structure, snpSetGattParamRsp_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_writeCharCnf()

uint8_t SNP_writeCharCnf ( snpCharWriteCnf_t pReq)

SNP Write Characteristic Confirmation.

NP -> AP (N/A)

CMD 0 CMD 1
0x55 0x88
SNP_NPI_ASYNC_CMD_TYPE SNP_CHAR_WRITE_IND

AP -> NP (SNP_writeCharCnf)

CMD 0 CMD 1
0x55 0x88
SNP_NPI_ASYNC_CMD_TYPE SNP_CHAR_WRITE_CNF

If a GATT client requests a write of a characteristic that was added by the AP, the SNP GATT server will forward an SNP_CHAR_WRITE_IND (0x88) to the AP.

The AP then has 30 seconds to do the following:

If no response occurs in 30 seconds, an ATT timeout will occur and BLE connection will be lost.

Corresponding Event
SNP_CHAR_WRITE_IND (from SNP) | SNP_CHAR_WRITE_CNF (from AP)
Payload Structures

NP -> AP
snpCharWriteInd_t

Size Description
2 Byte Connection Handle generating request to write
2 Byte Attribute Handle of Characteristic Value to write to
1 Byte Indicate if Response is Needed from AP Options for Response Needed Field
2 Byte Offset in Bytes
X Byte Data to write to characteristic

AP -> NP
snpCharWriteCnf_t

Size Description
1 Byte Status list of status generated by the SNP.
2 Byte Connection Handle Confirmation
Parameters
[in]pReq: Characteristic Write Confirmation Request Structure, snpCharWriteCnf_t
Returns
1 Byte Error Code, list of status generated by the SNP.
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale