TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Data Fields
snpSetAuthDataReq_t Struct Reference

Parameter Structure for SNP_setAuthenticationData / SNP_SET_AUTHENTICATION_DATA_REQ. More...

Data Fields

uint32_t authData
 4 Byte Authentication Data. 000000 - 999999 or TRUE/FALSE
 

Detailed Description

Parameter Structure for SNP_setAuthenticationData / SNP_SET_AUTHENTICATION_DATA_REQ.

For Passcode: 000000 - 999999

For Numeric Comparison: TRUE(match) or FALSE(no match)

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale