TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Files | Functions
SNP GAP API

Files

file  simple_np_gap.h
 SNP GAP Layer API.
 

Functions

uint8_t SNP_getGapParam (snpGetGapParamReq_t *cmdStruct)
 SNP Get GAP Parameter. More...
 
uint8_t SNP_sendSecurityRequest (void)
 SNP Send Security Request. More...
 
uint8_t SNP_setAdvData (snpSetAdvDataReq_t *cmdData, uint8_t len)
 SNP Set Advertisement Data. More...
 
uint8_t SNP_setAuthenticationData (snpSetAuthDataReq_t *pReq)
 SNP Set Authentication Data. More...
 
uint8_t SNP_setGapParam (snpSetGapParamReq_t *cmdStruct)
 SNP Set GAP Parameter. More...
 
uint8_t SNP_setSecurityParams (snpSetSecParamReq_t *pReq)
 SNP Set Security Parameters. More...
 
uint8_t SNP_setWhiteListFilterPolicy (snpSetWhiteListReq_t *pReq)
 SNP Set White List Filter Policy. More...
 
uint8_t SNP_startAdv (snpStartAdvReq_t *cmdStartAdv)
 SNP Start Advertisement. More...
 
uint8_t SNP_stopAdv (void)
 SNP Stop Advertisement. More...
 
uint8_t SNP_terminateConn (snpTermConnReq_t *cmdStruct)
 SNP Terminate Connection. More...
 
uint8_t SNP_updateConnParam (snpUpdateConnParamReq_t *cmdData)
 SNP Update Connection Parameters. More...
 

Detailed Description

Function Documentation

§ SNP_getGapParam()

uint8_t SNP_getGapParam ( snpGetGapParamReq_t cmdStruct)

SNP Get GAP Parameter.

AP -> NP (SNP_getGapParam)

CMD 0 CMD 1
0x35 0x49
SNP_NPI_SYNC_REQ_TYPE SNP_GET_GAP_PARAM_REQ

NP -> AP (SNP_getGapParam)

CMD 0 CMD 1
0x75 0x49
SNP_NPI_SYNC_RSP_TYPE SNP_GET_GAP_PARAM_RSP

The SNP Get GAP Parameter command is sent to the SNP to read the value of a GAP parameter.

The GAP parameters that can be retrieved are GAP Parameter IDs

Corresponding Events/Commands
SNP_GET_GAP_PARAM_REQ (from AP) | SNP_GET_GAP_PARAM_RSP (from SNP)
Payload Structures

AP -> NP
snpGetGapParamReq_t

Size Description
2 Byte GAP Parameter ID to Get value from. GAP Parameter IDs

NP -> AP
snpGetGapParamRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
2 Byte GAP Parameter ID, GAP Parameter IDs
2 Byte Value of GAP Parameter
Parameters
[in]cmdStruct:Get GAP Parameter Request Structure, snpGetGapParamReq_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_sendSecurityRequest()

uint8_t SNP_sendSecurityRequest ( void  )

SNP Send Security Request.

AP -> NP (SNP_sendSecurityRequest)

CMD 0 CMD 1
0x55 0x4B
SNP_NPI_ASYNC_CMD_TYPE SNP_SEND_SECURITY_REQUEST_REQ

NP -> AP (N/A)

CMD 0 CMD 1
0x55 0x05
SNP_NPI_ASYNC_CMD_TYPE SNP_EVENT_IND

The SNP Send Security command is sent to the SNP to request the central device to establish security.

Corresponding Events/Commands
SNP_SEND_SECURITY_REQUEST_REQ (from AP)
SNP_EVENT_IND with SNP_SECURITY_EVT (from SNP)

This command does not start pairing or bonding, the central may or may not choose to start the pairing/bonding process.

If the central does require pairing/bonding, SNP_EVENT_IND with SNP_SECURITY_EVT will be sent to the AP.

Payload Structures

AP -> NP
No Parameter Structure

NP -> AP
snpEvt_t

Size Description
2 Byte SNP_SECURITY_EVT
1 Byte Security State Security States
1 Byte Status list of status generated by the SNP.
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_setAdvData()

uint8_t SNP_setAdvData ( snpSetAdvDataReq_t cmdData,
uint8_t  len 
)

SNP Set Advertisement Data.

AP -> NP (SNP_stopAdv)

CMD 0 CMD 1
0x55 0x43
SNP_NPI_ASYNC_CMD_TYPE SNP_SET_ADV_DATA_REQ

NP -> AP (N/A)

CMD 0 CMD 1
0x55 0x43
SNP_NPI_ASYNC_CMD_TYPE SNP_SET_ADV_DATA_CNF

The SNP Set Advertisement Data command is sent to the SNP to update the raw data of either the scan response or the advertisement information.

There are 2 buffers for the advertisement data:

  • A buffer for the non-connected state (device is not in a connection)
  • A buffer for the connected state (device is in a connection)

When not in a connection, if advertisement is requested, the advertisement data stored in the non-connected state buffer will be advertised.

When in a connection, if advertisement is requested, the advertisement data stored in the connected state buffer will be advertised. If the connected state buffer has not been set, then the advertising data of the non-connected mode will be used. If the user does not care about differentiating advertising data in connected mode and non-connected modes, the connected mode data buffer does not have to be set.

Additional Notes

The maximum advertisement / scan response size is 31 Bytes.

Default Advertisement Data

[(length of flags) 0x02, (Adv type flags) 0x01, (General Disc, no BDEDR) 0x06, 'S' 0x53, 'N' 0x4E, 'P' 0x50]

Corresponding Events/Commands
SNP_SET_ADV_DATA_REQ (from AP) | SNP_SET_ADV_DATA_CNF (from SNP)
Payload Structures

AP -> NP
snpSetAdvDataReq_t

Size Description
1 Byte Type of Advertisement Data to update Adv. data buffer
X Byte New Advertisement data to update with, up to 31 Bytes

NP -> AP
snpSetAdvDataCnf_t

Size Description
1 Byte Status list of status generated by the SNP.
Parameters
[in]*cmdData: Advertisement Data Structure, snpSetAdvDataReq_t
[in]len: Length in Bytes of snpSetAdvDataReq_t::pData
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_setAuthenticationData()

uint8_t SNP_setAuthenticationData ( snpSetAuthDataReq_t pReq)

SNP Set Authentication Data.

AP -> NP (SNP_setAuthenticationData)

CMD 0 CMD 1
0x35 0x4C
SNP_NPI_SYNC_REQ_TYPE SNP_SET_AUTHENTICATION_DATA_REQ

NP -> AP (SNP_setAuthenticationData)

CMD 0 CMD 1
0x75 0x4C
SNP_NPI_SYNC_RSP_TYPE SNP_SEND_AUTHENTICATION_DATA_RSP

The SNP Set Authentication data command is sent to the SNP to provide Authentication data for the pairing process.

Corresponding Events/Commands
SNP_SET_AUTHENTICATION_DATA_REQ (from AP) | SNP_SEND_AUTHENTICATION_DATA_RSP (from SNP)
Payload Structures

AP -> NP
snpSetAuthDataReq_t

Size Description
4 Byte Authentication Data, 000000 - 999999 for passcode or TRUE/FALSE

NP -> AP
snpSetAuthDataRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
Parameters
[in]pReq: Set Authentication Data Request Structure, snpSetAuthDataReq_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_setGapParam()

uint8_t SNP_setGapParam ( snpSetGapParamReq_t cmdStruct)

SNP Set GAP Parameter.

AP -> NP (SNP_setGapParam)

CMD 0 CMD 1
0x35 0x48
SNP_NPI_SYNC_REQ_TYPE SNP_SET_GAP_PARAM_REQ

NP -> AP (SNP_setGapParam)

CMD 0 CMD 1
0x75 0x48
SNP_NPI_SYNC_RSP_TYPE SNP_SET_GAP_PARAM_RSP

The SNP Set GAP Parameter command is sent to the SNP to modify the value of a GAP parameter.

The GAP parameters that can be set are GAP Parameter IDs

Corresponding Events/Commands
SNP_SET_GAP_PARAM_REQ (from AP) | SNP_SET_GAP_PARAM_RSP (from SNP)
Payload Structures

AP -> NP
snpSetGapParamReq_t

Size Description
2 Byte GAP Parameter ID to Set value to. GAP Parameter IDs
2 Byte Value to set

NP -> AP
snpSetGapParamRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
Parameters
[in]cmdStruct:Set GAP Parameter Request Structure, snpSetGapParamReq_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_setSecurityParams()

uint8_t SNP_setSecurityParams ( snpSetSecParamReq_t pReq)

SNP Set Security Parameters.

AP -> NP (SNP_setSecurityParams)

CMD 0 CMD 1
0x35 0x4A
SNP_NPI_SYNC_REQ_TYPE SNP_SET_SECURITY_PARAM_REQ

NP -> AP (SNP_setSecurityParams)

CMD 0 CMD 1
0x75 0x4A
SNP_NPI_SYNC_RSP_TYPE SNP_SET_SECURITY_PARAM_RSP

The SNP Set Security Parameter command is used to set how device responses to security requests.

Corresponding Events/Commands
SNP_SET_SECURITY_PARAM_REQ (from AP) | SNP_SET_SECURITY_PARAM_RSP (from SNP)

SNP_SUCCESS in SNP_SET_SECURITY_PARAM_RSP does not mean parameters have been changed, only that the NP has successfully sent the request.

Payload Structures

AP -> NP
snpSetSecParamReq_t

Size Description
2 Byte GAP Parameter ID to Set value to. GAP Parameter IDs
2 Byte Value to set

NP -> AP
snpSetSecParamRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
Parameters
[in]pReq:Security parameter to set, snpSetSecParamReq_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_setWhiteListFilterPolicy()

uint8_t SNP_setWhiteListFilterPolicy ( snpSetWhiteListReq_t pReq)

SNP Set White List Filter Policy.

AP -> NP (SNP_setGapParam)

CMD 0 CMD 1
0x35 0x4D
SNP_NPI_SYNC_REQ_TYPE SNP_SET_WHITE_LIST_POLICY_REQ

NP -> AP (SNP_setGapParam)

CMD 0 CMD 1
0x75 0x4D
SNP_NPI_SYNC_RSP_TYPE SNP_SET_WHITE_LIST_POLICY_RSP

This command is can be sent to the SNP in order to set the White List Filter Policy for Scanning and Connections.

Corresponding Events/Commands
SNP_SET_WHITE_LIST_POLICY_REQ (from AP) | SNP_SET_WHITE_LIST_POLICY_RSP (from SNP)
Payload Structures

AP -> NP
snpSetWhiteListReq_t

Size Description
1 Byte Requested white list filter policy Advertisement Filter Policy Type

NP -> AP
snpSetWhiteListRsp_t

Size Description
1 Byte Status list of status generated by the SNP.
Parameters
[in]pReq: Set White List Request Structure, snpSetWhiteListReq_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_startAdv()

uint8_t SNP_startAdv ( snpStartAdvReq_t cmdStartAdv)

SNP Start Advertisement.

AP -> NP (SNP_startAdv)

CMD 0 CMD 1
0x55 0x42
SNP_NPI_ASYNC_CMD_TYPE SNP_START_ADV_REQ

NP -> AP (N/A)

CMD 0 CMD 1
0x55 0x05
SNP_NPI_ASYNC_CMD_TYPE SNP_EVENT_IND

The SNP Start Advertisement command is sent to the SNP to start advertising on all 3 channels.

Note that the SNP_setAdvData (0x43) command should be called before this command in order to set the advertising data.

Additional Notes

If a timeout value equal to 0 is used, the SNP will advertise infinitely if it is in general advertisement mode or for 180 seconds if it is in limited discovery mode. See SNP_setGapParam (0x49) command for setting the advertising mode.

If an interval value equal to 0 is used, the default value of 100 ms will be used.

Since the SNP only supports one connection, advertisement in a connection can only be non-connectable advertisement.

If the behavior parameter is set to SNP_ADV_RESTART_ON_CONN_EST, advertising will continue with non-connectable advertising when a connection is established. The advertising interval in this case is set by the TGAP_CONN_ADV_INT_MIN and TGAP_CONN_ADV_INT_MAX parameters.

By default, those parameters are set to 1280ms. They can be changed by using SNP_setGapParam (0x49) command.

Directed Advertisements are not supported.

Corresponding Event/Command
SNP_START_ADV_REQ (from AP)
SNP_EVENT_IND with SNP_ADV_STARTED_EVT (from SNP) when Advertisement is starting.

This event also gets sent upon power up, upon reception of this event previous connection is lost.

Payload Structures

AP -> NP
snpStartAdvReq_t

Size Description
1 Byte Type of Advertisement Advertisement Type
2 Byte Timeout of advertisement (in multiple of 625us)
2 Byte Advertisement Interval (in multiple of 625us)
1 Byte (Reserved) Advertisement Filter Policy
1 Byte (Reserved) Initiator Address Type
6 Byte (Reserved) Initiator Address
1 Byte Behavior of Advertisement upon Connection Adv. behavior when connection are established or terminated.

NP -> AP
snpEvt_t

Size Description
2 Byte SNP_ADV_STARTED_EVT
1 Byte Status list of status generated by the SNP.
Parameters
[in]*cmdStartAdv:advertising request structure, snpStartAdvReq_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_stopAdv()

uint8_t SNP_stopAdv ( void  )

SNP Stop Advertisement.

AP -> NP (SNP_stopAdv)

CMD 0 CMD 1
0x35 0x44
SNP_NPI_SYNC_REQ_TYPE SNP_STOP_ADV_REQ

NP -> AP (N/A)

CMD 0 CMD 1
0x75 0x05
SNP_NPI_SYNC_RSP_TYPE SNP_EVENT_IND

The SNP Stop Advertisement command is sent to the SNP to stop advertising.

Corresponding Event/Command
SNP_STOP_ADV_REQ (from AP)
SNP_EVENT_IND with SNP_ADV_ENDED_EVT (from SNP) upon advertisement stop.
Payload Structures

AP -> NP
No Parameter Structure

NP -> AP
snpEvt_t

Size Description
2 Byte SNP_ADV_ENDED_EVT
1 Byte Status list of status generated by the SNP.
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_terminateConn()

uint8_t SNP_terminateConn ( snpTermConnReq_t cmdStruct)

SNP Terminate Connection.

AP -> NP (SNP_terminateConn)

CMD 0 CMD 1
0x55 0x46
SNP_NPI_ASYNC_CMD_TYPE SNP_TERMINATE_CONN_REQ

NP -> AP (N/A)

CMD 0 CMD 1
0x55 0x05
SNP_NPI_ASYNC_CMD_TYPE SNP_EVENT_IND

Terminate current BLE connection.

Corresponding Events/Commands
SNP_TERMINATE_CONN_REQ (from AP)
SNP_EVENT_IND with SNP_CONN_TERM_EVT (from SNP)

Once connection has been terminated, SNP_EVENT_IND with SNP_CONN_TERM_EVT is sent to the AP.

Payload Structures

AP -> NP
snpTermConnReq_t

Size Description
2 Byte Connection Handle to Terminate
1 Byte Termination Method GAP GATT Terminate connection request option field

NP -> AP
snpEvt_t

Size Description
2 Byte SNP_ADV_ENDED_EVT
2 Byte Connection Handle Terminated
1 Byte Reason of Termination connection termination reason.
Parameters
[in]cmdStruct:Terminate Connection Request Structure, snpTermConnReq_t
Returns
1 Byte Error Code, list of status generated by the SNP.

§ SNP_updateConnParam()

uint8_t SNP_updateConnParam ( snpUpdateConnParamReq_t cmdData)

SNP Update Connection Parameters.

AP -> NP (SNP_updateConnParam)

CMD 0 CMD 1
0x55 0x45
SNP_NPI_ASYNC_CMD_TYPE SNP_UPDATE_CONN_PARAM_REQ

NP -> AP (N/A)

CMD 0 CMD 1
0x55 0x45
SNP_NPI_ASYNC_CMD_TYPE SNP_UPDATE_CONN_PARAM_CNF

NP -> AP (N/A)

CMD 0 CMD 1
0x55 0x05
SNP_NPI_ASYNC_CMD_TYPE SNP_EVENT_IND

This command is sent to the SNP to update the connection parameters while in a connection.

Corresponding Events/Commands
SNP_UPDATE_CONN_PARAM_REQ (from AP) | SNP_UPDATE_CONN_PARAM_CNF (from SNP)
SNP_EVENT_IND with SNP_CONN_PARAM_UPDATED_EVT (from SNP)

SNP_UPDATE_CONN_PARAM_CNF will follow the request SNP_UPDATE_CONN_PARAM_REQ, containing the status of the request as snpUpdateConnParamCnf_t structure.

Once connection parameters are updated and active, SNP_EVENT_IND with SNP_CONN_PARAM_UPDATED_EVT is sent to the AP.

Payload Structures

AP -> NP
snpUpdateConnParamReq_t

Size Description
2 Byte Connection Handle to update parameters on
2 Byte Connection Interval Minimum (multiple of 1.25 ms) 7.5 ms to 4 s
2 Byte Connection Interval Maximum (multiple of 1.25 ms) 7.5 ms to 4 s
2 Byte Slave Latency (number of connection events) 0x0000 to 0x0C80
2 Byte Supervision Timeout (multiple of 10 ms) 0x000A to 0x0C80

NP -> AP
snpUpdateConnParamCnf_t

Size Description
1 Byte Status list of status generated by the SNP.
2 Byte Connection Handle that connection parameter updates will occur for

NP -> AP
snpEvt_t

Size Description
2 Byte SNP_CONN_PARAM_UPDATED_EVT
2 Byte Connection Handle to update parameters on
2 Byte Connection Interval (multiple of 1.25 ms) 7.5 ms to 4 s
2 Byte Slave Latency (number of connection events) 0x0000 to 0x0C80
2 Byte Supervision Timeout (multiple of 10 ms) 0x000A to 0x0C80
Parameters
[in]*cmdData: Update Connection Parameter Request Structure, snpUpdateConnParamReq_t
Returns
1 Byte Error Code, list of status generated by the SNP.
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale