TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Data Fields
snpSetGapParamReq_t Struct Reference

Parameter Structure for SNP_setGapParam / SNP_SET_GAP_PARAM_REQ. More...

Data Fields

uint16_t paramId
 2 Byte GAP Parameter ID, GAP Parameter IDs or snpSetSecParamReq_t
 
uint16_t value
 2 Byte Parameter Value set if for SET command
 

Detailed Description

Parameter Structure for SNP_setGapParam / SNP_SET_GAP_PARAM_REQ.

This does not mean parameters have been changed, only that the NP has successfully sent the request.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale