TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Data Fields
snpSetGattParamReq_t Struct Reference

Parameter Structure for SNP_setGATTParam / SNP_SET_GATT_PARAM_RSP. More...

Data Fields

uint8_t paramID
 1 Byte ID of the parameter of the service to update/retrieved
 
uint8_t * pData
 Pointer of Data to write/retrieved.
 
uint8_t serviceID
 

Detailed Description

Parameter Structure for SNP_setGATTParam / SNP_SET_GATT_PARAM_RSP.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale