TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Data Fields
snpUpdateConnParamReq_t Struct Reference

Parameter Structure for SNP_updateConnParam. More...

Data Fields

uint16_t connHandle
 2 Byte handle of the connection to update parameters to.
 
uint16_t intervalMax
 2 Byte Maximum value for the connection event interval. More...
 
uint16_t intervalMin
 2 Byte Minimum value for the connection event interval. More...
 
uint16_t slaveLatency
 2 Byte Slave latency for the connection in number of connection events. More...
 
uint16_t supervisionTimeout
 2 Byte Supervision timeout for the LE Link. More...
 

Detailed Description

Parameter Structure for SNP_updateConnParam.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale