Data Structures | Macros | Typedefs | Functions
dma.h File Reference
#include <stdbool.h>
#include <ti/devices/msp432p4xx/inc/msp.h>
#include <ti/devices/msp432p4xx/driverlib/interrupt.h>

Go to the source code of this file.

Data Structures

struct  _DMA_ControlTable
 

Macros

#define DMA_TaskStructEntry(transferCount,itemSize,srcIncrement,srcAddr,dstIncrement,dstAddr,arbSize,mode)
 
#define UDMA_ATTR_USEBURST   0x00000001
 
#define UDMA_ATTR_ALTSELECT   0x00000002
 
#define UDMA_ATTR_HIGH_PRIORITY   0x00000004
 
#define UDMA_ATTR_REQMASK   0x00000008
 
#define UDMA_ATTR_ALL   0x0000000F
 
#define UDMA_MODE_STOP   0x00000000
 
#define UDMA_MODE_BASIC   0x00000001
 
#define UDMA_MODE_AUTO   0x00000002
 
#define UDMA_MODE_PINGPONG   0x00000003
 
#define UDMA_MODE_MEM_SCATTER_GATHER   0x00000004
 
#define UDMA_MODE_PER_SCATTER_GATHER   0x00000006
 
#define UDMA_MODE_ALT_SELECT   0x00000001
 
#define UDMA_DST_INC_8   0x00000000
 
#define UDMA_DST_INC_16   0x40000000
 
#define UDMA_DST_INC_32   0x80000000
 
#define UDMA_DST_INC_NONE   0xc0000000
 
#define UDMA_SRC_INC_8   0x00000000
 
#define UDMA_SRC_INC_16   0x04000000
 
#define UDMA_SRC_INC_32   0x08000000
 
#define UDMA_SRC_INC_NONE   0x0c000000
 
#define UDMA_SIZE_8   0x00000000
 
#define UDMA_SIZE_16   0x11000000
 
#define UDMA_SIZE_32   0x22000000
 
#define UDMA_DST_PROT_PRIV   0x00200000
 
#define UDMA_SRC_PROT_PRIV   0x00040000
 
#define UDMA_ARB_1   0x00000000
 
#define UDMA_ARB_2   0x00004000
 
#define UDMA_ARB_4   0x00008000
 
#define UDMA_ARB_8   0x0000c000
 
#define UDMA_ARB_16   0x00010000
 
#define UDMA_ARB_32   0x00014000
 
#define UDMA_ARB_64   0x00018000
 
#define UDMA_ARB_128   0x0001c000
 
#define UDMA_ARB_256   0x00020000
 
#define UDMA_ARB_512   0x00024000
 
#define UDMA_ARB_1024   0x00028000
 
#define UDMA_NEXT_USEBURST   0x00000008
 
#define UDMA_PRI_SELECT   0x00000000
 
#define UDMA_ALT_SELECT   0x00000008
 
#define DMA_CH0_RESERVED0   0x00000000
 
#define DMA_CH0_EUSCIA0TX   0x01000000
 
#define DMA_CH0_EUSCIB0TX0   0x02000000
 
#define DMA_CH0_EUSCIB3TX1   0x03000000
 
#define DMA_CH0_EUSCIB2TX2   0x04000000
 
#define DMA_CH0_EUSCIB1TX3   0x05000000
 
#define DMA_CH0_TIMERA0CCR0   0x06000000
 
#define DMA_CH0_AESTRIGGER0   0x07000000
 
#define DMA_CH1_RESERVED0   0x00000001
 
#define DMA_CH1_EUSCIA0RX   0x01000001
 
#define DMA_CH1_EUSCIB0RX0   0x02000001
 
#define DMA_CH1_EUSCIB3RX1   0x03000001
 
#define DMA_CH1_EUSCIB2RX2   0x04000001
 
#define DMA_CH1_EUSCIB1RX3   0x05000001
 
#define DMA_CH1_TIMERA0CCR2   0x06000001
 
#define DMA_CH1_AESTRIGGER1   0x07000001
 
#define DMA_CH2_RESERVED0   0x00000002
 
#define DMA_CH2_EUSCIA1TX   0x01000002
 
#define DMA_CH2_EUSCIB1TX0   0x02000002
 
#define DMA_CH2_EUSCIB0TX1   0x03000002
 
#define DMA_CH2_EUSCIB3TX2   0x04000002
 
#define DMA_CH2_EUSCIB2TX3   0x05000002
 
#define DMA_CH2_TIMERA1CCR0   0x06000002
 
#define DMA_CH2_AESTRIGGER2   0x07000002
 
#define DMA_CH3_RESERVED0   0x00000003
 
#define DMA_CH3_EUSCIA1RX   0x01000003
 
#define DMA_CH3_EUSCIB1RX0   0x02000003
 
#define DMA_CH3_EUSCIB0RX1   0x03000003
 
#define DMA_CH3_EUSCIB3RX2   0x04000003
 
#define DMA_CH3_EUSCIB2RX3   0x05000003
 
#define DMA_CH3_TIMERA1CCR2   0x06000003
 
#define DMA_CH3_RESERVED1   0x07000003
 
#define DMA_CH4_RESERVED0   0x00000004
 
#define DMA_CH4_EUSCIA2TX   0x01000004
 
#define DMA_CH4_EUSCIB2TX0   0x02000004
 
#define DMA_CH4_EUSCIB1TX1   0x03000004
 
#define DMA_CH4_EUSCIB0TX2   0x04000004
 
#define DMA_CH4_EUSCIB3TX3   0x05000004
 
#define DMA_CH4_TIMERA2CCR0   0x06000004
 
#define DMA_CH4_RESERVED1   0x07000004
 
#define DMA_CH5_RESERVED0   0x00000005
 
#define DMA_CH5_EUSCIA2RX   0x01000005
 
#define DMA_CH5_EUSCIB2RX0   0x02000005
 
#define DMA_CH5_EUSCIB1RX1   0x03000005
 
#define DMA_CH5_EUSCIB0RX2   0x04000005
 
#define DMA_CH5_EUSCIB3RX3   0x05000005
 
#define DMA_CH5_TIMERA2CCR2   0x06000005
 
#define DMA_CH5_RESERVED1   0x07000005
 
#define DMA_CH6_RESERVED0   0x00000006
 
#define DMA_CH6_EUSCIA3TX   0x01000006
 
#define DMA_CH6_EUSCIB3TX0   0x02000006
 
#define DMA_CH6_EUSCIB2TX1   0x03000006
 
#define DMA_CH6_EUSCIB1TX2   0x04000006
 
#define DMA_CH6_EUSCIB0TX3   0x05000006
 
#define DMA_CH6_TIMERA3CCR0   0x06000006
 
#define DMA_CH6_EXTERNALPIN   0x07000006
 
#define DMA_CH7_RESERVED0   0x00000007
 
#define DMA_CH7_EUSCIA3RX   0x01000007
 
#define DMA_CH7_EUSCIB3RX0   0x02000007
 
#define DMA_CH7_EUSCIB2RX1   0x03000007
 
#define DMA_CH7_EUSCIB1RX2   0x04000007
 
#define DMA_CH7_EUSCIB0RX3   0x05000007
 
#define DMA_CH7_TIMERA3CCR2   0x06000007
 
#define DMA_CH7_ADC14   0x07000007
 
#define DMA_INT0   INT_DMA_INT0
 
#define DMA_INT1   INT_DMA_INT1
 
#define DMA_INT2   INT_DMA_INT2
 
#define DMA_INT3   INT_DMA_INT3
 
#define DMA_INTERR   INT_DMA_ERR
 
#define DMA_CHANNEL_0   0
 
#define DMA_CHANNEL_1   1
 
#define DMA_CHANNEL_2   2
 
#define DMA_CHANNEL_3   3
 
#define DMA_CHANNEL_4   4
 
#define DMA_CHANNEL_5   5
 
#define DMA_CHANNEL_6   6
 
#define DMA_CHANNEL_7   7
 

Typedefs

typedef struct _DMA_ControlTable DMA_ControlTable
 

Functions

void DMA_enableModule (void)
 
void DMA_disableModule (void)
 
uint32_t DMA_getErrorStatus (void)
 
void DMA_clearErrorStatus (void)
 
void DMA_enableChannel (uint32_t channelNum)
 
void DMA_disableChannel (uint32_t channelNum)
 
bool DMA_isChannelEnabled (uint32_t channelNum)
 
void DMA_setControlBase (void *controlTable)
 
void * DMA_getControlBase (void)
 
void * DMA_getControlAlternateBase (void)
 
void DMA_requestChannel (uint32_t channelNum)
 
void DMA_enableChannelAttribute (uint32_t channelNum, uint32_t attr)
 
void DMA_disableChannelAttribute (uint32_t channelNum, uint32_t attr)
 
uint32_t DMA_getChannelAttribute (uint32_t channelNum)
 
void DMA_setChannelControl (uint32_t channelStructIndex, uint32_t control)
 
void DMA_setChannelTransfer (uint32_t channelStructIndex, uint32_t mode, void *srcAddr, void *dstAddr, uint32_t transferSize)
 
void DMA_setChannelScatterGather (uint32_t channelNum, uint32_t taskCount, void *taskList, uint32_t isPeriphSG)
 
uint32_t DMA_getChannelSize (uint32_t channelStructIndex)
 
uint32_t DMA_getChannelMode (uint32_t channelStructIndex)
 
void DMA_assignChannel (uint32_t mapping)
 
void DMA_requestSoftwareTransfer (uint32_t channel)
 
void DMA_assignInterrupt (uint32_t interruptNumber, uint32_t channel)
 
void DMA_enableInterrupt (uint32_t interruptNumber)
 
void DMA_disableInterrupt (uint32_t interruptNumber)
 
uint32_t DMA_getInterruptStatus (void)
 
void DMA_clearInterruptFlag (uint32_t channel)
 
void DMA_registerInterrupt (uint32_t interruptNumber, void(*intHandler)(void))
 
void DMA_unregisterInterrupt (uint32_t interruptNumber)
 

Copyright 2018, Texas Instruments Incorporated