Data Fields
PWMTimerMSP432_Object Struct Reference

PWMTimerMSP432 Object. More...

#include <PWMTimerMSP432.h>

Collaboration diagram for PWMTimerMSP432_Object:
Collaboration graph
[legend]

Data Fields

PWMTimerMSP432_StatustimerStatus
 
uint32_t baseAddress
 
PWM_Duty_Units dutyUnits
 
PWM_IdleLevel idleLevel
 
uint8_t compareOutputNum
 

Detailed Description

PWMTimerMSP432 Object.

The application must not access any member variables of this structure!

Field Documentation

§ timerStatus

PWMTimerMSP432_Status* PWMTimerMSP432_Object::timerStatus

§ baseAddress

uint32_t PWMTimerMSP432_Object::baseAddress

§ dutyUnits

PWM_Duty_Units PWMTimerMSP432_Object::dutyUnits

§ idleLevel

PWM_IdleLevel PWMTimerMSP432_Object::idleLevel

§ compareOutputNum

uint8_t PWMTimerMSP432_Object::compareOutputNum

The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale