Go to the documentation of this file.
75 #define DLOG_4CH_F_MACRO(v) \
79 if(*v.input_ptr1>v.trig_value && v.prev_value<v.trig_value) \
87 if(v.skip_count==v.pre_scalar) \
90 v.output_ptr1[v.count]=*v.input_ptr1; \
91 v.output_ptr2[v.count]=*v.input_ptr2; \
92 v.output_ptr3[v.count]=*v.input_ptr3; \
93 v.output_ptr4[v.count]=*v.input_ptr4; \
105 v.prev_value=*v.input_ptr1; \
float32_t * output_ptr3
Definition: dlog_4ch_f.h:59
float float32_t
Definition: sfra_f32.h:42
float32_t * output_ptr2
Definition: dlog_4ch_f.h:58
int16_t count
Definition: dlog_4ch_f.h:67
float32_t * input_ptr1
Definition: dlog_4ch_f.h:53
void DLOG_4CH_F_FUNC(DLOG_4CH_F *v)
float32_t * output_ptr4
Definition: dlog_4ch_f.h:60
int16_t size
Definition: dlog_4ch_f.h:66
float32_t * output_ptr1
Definition: dlog_4ch_f.h:57
float32_t trig_value
Definition: dlog_4ch_f.h:62
Definition: dlog_4ch_f.h:52
float32_t * input_ptr4
Definition: dlog_4ch_f.h:56
float32_t * input_ptr2
Definition: dlog_4ch_f.h:54
int16_t skip_count
Definition: dlog_4ch_f.h:65
int16_t pre_scalar
Definition: dlog_4ch_f.h:64
float32_t * input_ptr3
Definition: dlog_4ch_f.h:55
void DLOG_4CH_F_init(DLOG_4CH_F *v)
float32_t prev_value
Definition: dlog_4ch_f.h:61
int16_t status
Definition: dlog_4ch_f.h:63
Copyright 2023, Texas Instruments Incorporated