Go to the documentation of this file.
51 #define DLOG_BUF_SIZE 512
52 #define DLOG_SCALER_NUM 10
void DLOG_6CH_F_FUNC(DLOG_6CH_F *v)
uint16_t skipCount
Definition: dlog_6ch_f.h:62
float float32_t
Definition: sfra_f32.h:42
float32_t refValue
Definition: dlog_6ch_f.h:58
Definition: dlog_6ch_f.h:55
uint16_t status
Definition: dlog_6ch_f.h:60
uint16_t size
Definition: dlog_6ch_f.h:63
uint16_t preScalar
Definition: dlog_6ch_f.h:61
void DLOG_6CH_F_init(DLOG_6CH_F *v)
float32_t prevValue
Definition: dlog_6ch_f.h:59
uint16_t count
Definition: dlog_6ch_f.h:64
#define DLOG_CH_NUM
Definition: dlog_6ch_f.h:50
Copyright 2023, Texas Instruments Incorporated