Data Structures | |
struct | _PI_Obj_ |
Defines the PI controller object. More... | |
Typedefs | |
typedef struct _PI_Obj_ | PI_Obj |
Defines the PI controller object. More... | |
typedef struct _PI_Obj_ * | PI_Handle |
Defines the PI handle. More... | |
Functions | |
static float32_t | PI_getFbackValue (PI_Handle handle) |
Gets the feedback value in the PI controller. More... | |
static float32_t | PI_getFfwdValue (PI_Handle handle) |
Gets the feedforward value in the PI controller. More... | |
static void | PI_getGains (PI_Handle handle, float32_t *pKp, float32_t *pKi) |
Gets the gains in the PI controller. More... | |
static float32_t | PI_getKi (PI_Handle handle) |
Gets the integral gain in the PI controller. More... | |
static float32_t | PI_getKp (PI_Handle handle) |
Gets the proportional gain in the PI controller. More... | |
static void | PI_getMinMax (PI_Handle handle, float32_t *pOutMin, float32_t *pOutMax) |
Gets the minimum and maximum output value allowed in the PI controller. More... | |
static float32_t | PI_getOutMax (PI_Handle handle) |
Gets the maximum output value allowed in the PI controller. More... | |
static float32_t | PI_getOutMin (PI_Handle handle) |
Gets the minimum output value allowed in the PI controller. More... | |
static float32_t | PI_getRefValue (PI_Handle handle) |
Gets the reference value in the PI controller. More... | |
static float32_t | PI_getUi (PI_Handle handle) |
Gets the integrator start value in the PI controller. More... | |
PI_Handle | PI_init (void *pMemory, const size_t numBytes) |
Initializes the PI controller. More... | |
PI_Handle | cla_PI_init (void *pMemory, const size_t numBytes) |
static void | PI_setFbackValue (PI_Handle handle, const float32_t fbackValue) |
Sets the feedback value in the PI controller. More... | |
static void | PI_setFfwdValue (PI_Handle handle, const float32_t ffwdValue) |
Sets the feedforward value in the PI controller. More... | |
static void | PI_setGains (PI_Handle handle, const float32_t Kp, const float32_t Ki) |
Sets the gains in the PI controller. More... | |
static void | PI_setKi (PI_Handle handle, const float32_t Ki) |
Sets the integral gain in the PI controller. More... | |
static void | PI_setKp (PI_Handle handle, const float32_t Kp) |
Sets the proportional gain in the PI controller. More... | |
static void | PI_setMinMax (PI_Handle handle, const float32_t outMin, const float32_t outMax) |
Sets the minimum and maximum output value allowed in the PI controller. More... | |
static void | PI_setOutMax (PI_Handle handle, const float32_t outMax) |
Sets the maximum output value allowed in the PI controller. More... | |
static void | PI_setOutMin (PI_Handle handle, const float32_t outMin) |
Sets the minimum output value allowed in the PI controller. More... | |
static void | PI_setRefValue (PI_Handle handle, const float32_t refValue) |
Sets the reference value in the PI controller. More... | |
static void | PI_setUi (PI_Handle handle, const float32_t Ui) |
Sets the integrator start value in the PI controller. More... | |
static void | PI_run_parallel (PI_Handle handle, const float32_t refValue, const float32_t fbackValue, const float32_t ffwdValue, float32_t *pOutValue) |
Runs the parallel form of the PI controller. More... | |
static void | PI_run_series (PI_Handle handle, const float32_t refValue, const float32_t fbackValue, const float32_t ffwdValue, float32_t *pOutValue) |
Runs the series form of the PI controller. More... | |
static void | PI_run (PI_Handle handle, const float32_t refValue, const float32_t fbackValue, float32_t *pOutValue) |
Runs the series form of the PI controller. More... | |
Gets the feedback value in the PI controller.
[in] | handle | The PI controller handle |
References _PI_Obj_::fbackValue.
Gets the feedforward value in the PI controller.
[in] | handle | The PI controller handle |
References _PI_Obj_::ffwdValue.
Gets the gains in the PI controller.
[in] | handle | The PI controller handle |
[out] | pKp | The pointer to the proportional gain value |
[out] | pKi | The pointer to the integrator gain value |
References _PI_Obj_::Ki, and _PI_Obj_::Kp.
Gets the integral gain in the PI controller.
[in] | handle | The PI controller handle |
References _PI_Obj_::Ki.
Referenced by PI_run(), PI_run_parallel(), and PI_run_series().
Gets the proportional gain in the PI controller.
[in] | handle | The PI controller handle |
References _PI_Obj_::Kp.
Referenced by PI_run(), PI_run_parallel(), and PI_run_series().
|
inlinestatic |
Gets the minimum and maximum output value allowed in the PI controller.
[in] | handle | The PI controller handle |
[out] | pOutMin | The pointer to the minimum output value allowed |
[out] | pOutMax | The pointer to the maximum output value allowed |
References _PI_Obj_::outMax, and _PI_Obj_::outMin.
Gets the maximum output value allowed in the PI controller.
[in] | handle | The PI controller handle |
References _PI_Obj_::outMax.
Referenced by PI_run(), PI_run_parallel(), and PI_run_series().
Gets the minimum output value allowed in the PI controller.
[in] | handle | The PI controller handle |
References _PI_Obj_::outMin.
Referenced by PI_run(), PI_run_parallel(), and PI_run_series().
Gets the reference value in the PI controller.
[in] | handle | The PI controller handle |
References _PI_Obj_::refValue.
Referenced by CTRL_getRefValue().
Gets the integrator start value in the PI controller.
[in] | handle | The PI controller handle |
References _PI_Obj_::Ui.
Referenced by PI_run(), PI_run_parallel(), and PI_run_series().
PI_Handle PI_init | ( | void * | pMemory, |
const size_t | numBytes | ||
) |
Initializes the PI controller.
[in] | pMemory | A pointer to the memory for the PI controller object |
[in] | numBytes | The number of bytes allocated for the PI controller object, bytes |
PI_Handle cla_PI_init | ( | void * | pMemory, |
const size_t | numBytes | ||
) |
Sets the feedback value in the PI controller.
[in] | handle | The PI controller handle |
[in] | fbackValue | The feedback value |
References _PI_Obj_::fbackValue.
Referenced by PI_run(), PI_run_parallel(), and PI_run_series().
Sets the feedforward value in the PI controller.
[in] | handle | The PI controller handle |
[in] | ffwdValue | The feedforward value |
References _PI_Obj_::ffwdValue.
Referenced by PI_run_parallel(), and PI_run_series().
Sets the gains in the PI controller.
[in] | handle | The PI controller handle |
[in] | Kp | The proportional gain for the PI controller |
[in] | Ki | The integrator gain for the PI controller |
References _PI_Obj_::Ki, and _PI_Obj_::Kp.
Sets the integral gain in the PI controller.
[in] | handle | The PI controller handle |
[in] | Ki | The integral gain for the PI controller |
References _PI_Obj_::Ki.
Referenced by CTRL_setup(), FWC_setGains(), and FWC_setKi().
Sets the proportional gain in the PI controller.
[in] | handle | The PI controller handle |
[in] | Kp | The proportional gain for the PI controller |
References _PI_Obj_::Kp.
Referenced by CTRL_setup(), FWC_setGains(), and FWC_setKp().
|
inlinestatic |
Sets the minimum and maximum output value allowed in the PI controller.
[in] | handle | The PI controller handle |
[in] | outMin | The minimum output value allowed |
[in] | outMax | The maximum output value allowed |
References _PI_Obj_::outMax, and _PI_Obj_::outMin.
Referenced by CTRL_run(), and FWC_setAngleMinMax().
Sets the maximum output value allowed in the PI controller.
[in] | handle | The PI controller handle |
[in] | outMax | The maximum output value allowed |
References _PI_Obj_::outMax.
Sets the minimum output value allowed in the PI controller.
[in] | handle | The PI controller handle |
[in] | outMax | The minimum output value allowed |
References _PI_Obj_::outMin.
Referenced by FWC_setAngleMax().
Sets the reference value in the PI controller.
[in] | handle | The PI controller handle |
[in] | refValue | The reference value |
References _PI_Obj_::refValue.
Referenced by PI_run(), PI_run_parallel(), and PI_run_series().
Sets the integrator start value in the PI controller.
[in] | handle | The PI controller handle |
[in] | Ui | The integral start value for the PI controller |
References _PI_Obj_::Ui.
Referenced by CTRL_setup(), FWC_resetUi(), FWC_setUi(), PI_run(), PI_run_parallel(), and PI_run_series().
|
inlinestatic |
Runs the parallel form of the PI controller.
[in] | handle | The PI controller handle |
[in] | refValue | The reference value to the controller |
[in] | fbackValue | The feedback value to the controller |
[in] | ffwdValue | The feedforward value to the controller |
[in] | pOutValue | The pointer to the controller output value |
References _PI_Obj_::fbackValue, _PI_Obj_::ffwdValue, _PI_Obj_::Ki, _PI_Obj_::Kp, MATH_sat(), _PI_Obj_::outMax, _PI_Obj_::outMin, PI_getKi(), PI_getKp(), PI_getOutMax(), PI_getOutMin(), PI_getUi(), PI_setFbackValue(), PI_setFfwdValue(), PI_setRefValue(), PI_setUi(), _PI_Obj_::refValue, and _PI_Obj_::Ui.
|
inlinestatic |
Runs the series form of the PI controller.
[in] | handle | The PI controller handle |
[in] | refValue | The reference value to the controller |
[in] | fbackValue | The feedback value to the controller |
[in] | ffwdValue | The feedback value to the controller |
[in] | pOutValue | The pointer to the controller output value |
References _PI_Obj_::fbackValue, _PI_Obj_::ffwdValue, _PI_Obj_::Ki, _PI_Obj_::Kp, MATH_sat(), _PI_Obj_::outMax, _PI_Obj_::outMin, PI_getKi(), PI_getKp(), PI_getOutMax(), PI_getOutMin(), PI_getUi(), PI_setFbackValue(), PI_setFfwdValue(), PI_setRefValue(), PI_setUi(), _PI_Obj_::refValue, and _PI_Obj_::Ui.
Referenced by CTRL_run(), and FWC_computeCurrentAngle().
|
inlinestatic |
Runs the series form of the PI controller.
[in] | handle | The PI controller handle |
[in] | refValue | The reference value to the controller |
[in] | fbackValue | The feedback value to the controller |
[in] | pOutValue | The pointer to the controller output value |
References _PI_Obj_::fbackValue, _PI_Obj_::Ki, _PI_Obj_::Kp, MATH_sat(), _PI_Obj_::outMax, _PI_Obj_::outMin, PI_getKi(), PI_getKp(), PI_getOutMax(), PI_getOutMin(), PI_getUi(), PI_setFbackValue(), PI_setRefValue(), PI_setUi(), _PI_Obj_::refValue, and _PI_Obj_::Ui.