![]() |
![]() |
Functions | |
uint16_t | PM_tformat_setupCommand (uint16_t dataID, uint16_t eepromAddr, uint16_t eepromData, uint16_t crc) static |
Setup a command (Deprecated) More... | |
uint16_t | PM_tformat_receiveData (uint16_t dataID) static |
Receive data (Deprecated) More... | |
uint16_t PM_tformat_setupCommand | ( | uint16_t | dataID, |
uint16_t | eepromAddr, | ||
uint16_t | eepromData, | ||
uint16_t | crc | ||
) |
Setup a command (Deprecated)
To improve performance, this function has been split into command-specific functions shown below.
uint16_t PM_tformat_receiveData | ( | uint16_t | dataID | ) |
Receive data (Deprecated)
To improve performance, this function has been split into command-specific functions.