Data Structures | |
struct | _USER_Params_ |
Defines a structure for the user parameters. More... | |
Typedefs | |
typedef struct _USER_Params_ | USER_Params |
Defines a structure for the user parameters. More... | |
typedef struct _USER_Params_ * | userParams_Handle |
Defines the USER_Params handle. More... | |
typedef struct _USER_Params_ * | userParams_Handle |
Defines the USER_Params handle. More... | |
Enumerations | |
enum | MotorNum_e { MTR_1 = 0, MTR_2 = 1, MTR_3 = 2, MTR_1 = 0, MTR_2 = 1, MTR_3 = 2 } |
Enumeration for the Motor numbers. More... | |
enum | MotorNum_e { MTR_1 = 0, MTR_2 = 1, MTR_3 = 2, MTR_1 = 0, MTR_2 = 1, MTR_3 = 2 } |
Enumeration for the Motor numbers. More... | |
Functions | |
void | USER_setParams_priv (USER_Params *pUserParams) |
Sets the private user parameter values. More... | |
void | USER_setParams_priv (userParams_Handle handle) |
Sets the private user parameter values. More... | |
typedef struct _USER_Params_ USER_Params |
Defines a structure for the user parameters.
typedef struct _USER_Params_* userParams_Handle |
Defines the USER_Params handle.
typedef struct _USER_Params_* userParams_Handle |
Defines the USER_Params handle.
enum MotorNum_e |
enum MotorNum_e |
void USER_setParams_priv | ( | USER_Params * | pUserParams | ) |
Sets the private user parameter values.
[in] | pUserParams | The pointer to the user param structure |
void USER_setParams_priv | ( | userParams_Handle | handle | ) |
Sets the private user parameter values.
[in] | pUserParams | The pointer to the user param structure |