|
static float32_t | IPARK_getCosTh (IPARK_Handle handle) |
| Gets the cosine of the angle between the d,q and the alpha, beta coordinate systems. More...
|
|
static void | IPARK_getPhasor (IPARK_Handle handle, MATH_Vec2 *pPhasor) |
| Gets the cosine/sine phasor for the inverse Park transform. More...
|
|
static float32_t | IPARK_getSinTh (IPARK_Handle handle) |
| Gets the sine of the angle between the d,q and the alpha, beta coordinate systems. More...
|
|
IPARK_Handle | IPARK_init (void *pMemory, const size_t numBytes) |
| Initializes the inverse Park transform module. More...
|
|
IPARK_Handle | cla_IPARK_init (void *pMemory, const size_t numBytes) |
|
static void | IPARK_run (IPARK_Handle handle, const MATH_Vec2 *pInVec, MATH_Vec2 *pOutVec) |
| Runs the inverse Park transform module. More...
|
|
static void | IPARK_setCosTh (IPARK_Handle handle, const float32_t cosTh) |
| Sets the cosine of the angle between the d,q and the alpha, beta coordinate systems. More...
|
|
static void | IPARK_setPhasor (IPARK_Handle handle, const MATH_Vec2 *pPhasor) |
| Sets the cosine/sine phasor for the inverse Park transform. More...
|
|
static void | IPARK_setSinTh (IPARK_Handle handle, const float32_t sinTh) |
| Sets the sine of the angle between the d,q and the alpha, beta coordinate systems. More...
|
|
static void | IPARK_setup (IPARK_Handle handle, const float32_t Th) |
| Sets up the inverse Park transform module. More...
|
|