|
static float32_t | PARK_getCosTh (PARK_Handle handle) |
| Gets the cosine of the angle between the d,q and the alpha, beta coordinate systems. More...
|
|
static void | PARK_getPhasor (PARK_Handle handle, MATH_Vec2 *pPhasor) |
| Gets the cosine/sine phasor for the Park transform. More...
|
|
static float32_t | PARK_getSinTh (PARK_Handle handle) |
| Gets the sine of the angle between the d,q and the alpha, beta coordinate systems. More...
|
|
PARK_Handle | PARK_init (void *pMemory, const size_t numBytes) |
| Initializes the Park transform module. More...
|
|
PARK_Handle | cla_PARK_init (void *pMemory, const size_t numBytes) |
|
static void | PARK_run (PARK_Handle handle, const MATH_Vec2 *pInVec, MATH_Vec2 *pOutVec) |
| Runs the Park transform module. More...
|
|
static void | PARK_setCosTh (PARK_Handle handle, const float32_t cosTh) |
| Sets the cosine of the angle between the d,q and the alpha, beta coordinate systems. More...
|
|
static void | PARK_setPhasor (PARK_Handle handle, const MATH_Vec2 *pPhasor) |
| Sets the cosine/sine phasor for the inverse Park transform. More...
|
|
static void | PARK_setSinTh (PARK_Handle handle, const float32_t sinTh) |
| Sets the sine of the angle between the d,q and the alpha, beta coordinate systems. More...
|
|
static void | PARK_setup (PARK_Handle handle, const float32_t Th) |
| Sets up the Park transform module. More...
|
|