![]() |
![]() |
Go to the source code of this file.
Data Structures | |
struct | POWER_MEAS_FAST |
Defines the POWER_MEAS_SINE_ANALYZER structure. More... | |
Functions | |
static void | POWER_MEAS_FAST_reset (POWER_MEAS_FAST *v) |
Resets internal data to zero. More... | |
static void | POWER_MEAS_FAST_config (POWER_MEAS_FAST *v, float32_t isrFrequency, float32_t threshold, float32_t gridMaxFreq, float32_t gridMinFreq) |
Configures the power measurment module. More... | |
static void | POWER_MEAS_FAST_run (POWER_MEAS_FAST *v) |
Perform calculations using the POWER_MEAS_SINE_ANALYZER module. More... | |