![]() |
![]() |
Go to the source code of this file.
Data Structures | |
struct | SPLL_3PH_DDSRF_LPF_COEFF |
Defines the coefficients for a loop filter. More... | |
struct | SPLL_3PH_DDSRF |
Defines the SPLL_3PH_DDSRF structure. More... | |
Macros | |
#define | C2000_IEEE754_TYPES |
Typedefs | |
typedef float | float32_t |
typedef long double | float64_t |
Functions | |
static void | SPLL_3PH_DDSRF_init (float32_t grid_freq, float32_t delta_t, float32_t k1, float32_t k2, SPLL_3PH_DDSRF *spll_obj) |
Initialize SPLL_3PH_DDSRF module. More... | |
static void | SPLL_3PH_DDSRF_reset (SPLL_3PH_DDSRF *spll_obj) |
Reset SPLL_3PH_DDSRF module. More... | |
static void | SPLL_3PH_DDSRF_run (SPLL_3PH_DDSRF *spll_obj, float32_t d_p, float32_t d_n, float32_t q_p, float32_t q_n) |
Run spll_3PH_srf module. More... | |