![]() |
![]() |
Object for the DAC128S registers and commands. More...
#include <dac128s085.h>
Data Fields | |
volatile float32_t * | ptrData [(4U)] |
Input: First input pointer. More... | |
float32_t | gain [(4U)] |
the DAC data More... | |
uint32_t | spiHandle |
handle for the serial peripheral interface More... | |
int16_t | offset [(4U)] |
the DAC data More... | |
int16_t | dacData [(4U)] |
uint16_t | channelNum |
Object for the DAC128S registers and commands.
volatile float32_t* _DAC128S_Obj_::ptrData[(4U)] |
Input: First input pointer.
float32_t _DAC128S_Obj_::gain[(4U)] |
the DAC data
uint32_t _DAC128S_Obj_::spiHandle |
handle for the serial peripheral interface
int16_t _DAC128S_Obj_::offset[(4U)] |
the DAC data
int16_t _DAC128S_Obj_::dacData[(4U)] |
uint16_t _DAC128S_Obj_::channelNum |