Defines the estimator (EST) input data. More...
#include <est.h>
Data Fields | |
int32_t | timeStamp |
a time stamp for the input data buffer More... | |
MATH_Vec2 | Iab_A |
the alpha/beta current values, A More... | |
MATH_Vec2 | Vab_V |
the alpha/beta current values, V More... | |
float32_t | dcBus_V |
the DC bus voltage value, V More... | |
float32_t | speed_ref_Hz |
the speed reference value, Hz More... | |
float32_t | speed_int_Hz |
the speed int value, Hz More... | |
Defines the estimator (EST) input data.
int32_t _EST_InputData_::timeStamp |
a time stamp for the input data buffer
MATH_Vec2 _EST_InputData_::Iab_A |
the alpha/beta current values, A
MATH_Vec2 _EST_InputData_::Vab_V |
the alpha/beta current values, V
float32_t _EST_InputData_::dcBus_V |
the DC bus voltage value, V
float32_t _EST_InputData_::speed_ref_Hz |
the speed reference value, Hz
float32_t _EST_InputData_::speed_int_Hz |
the speed int value, Hz