Defines the estimator (EST) output data. More...
#include <est.h>
Data Fields | |
int32_t | timeStamp |
a time stamp for the output data buffer More... | |
float32_t | angle_rad |
the estimated angle value at t = m+1, rad More... | |
float32_t | fe_rps |
the electrical frequency estimate, rad/sec More... | |
float32_t | fm_rps |
the mechanical frequency estimate, rad/sec More... | |
float32_t | fm_lp_rps |
the low pass filtered mechanical frequency estimate, rad/sec More... | |
float32_t | fmDot_rps2 |
the mechanical acceleration estimate, rad/sec^2 More... | |
float32_t | fslip_rps |
the slip frequency estimate, rad/sec More... | |
MATH_Vec2 | Eab_V |
the alpha/beta back-EMF estimates, V More... | |
MATH_Vec2 | Edq_V |
the direction/quadrature back-EMF estimates, V More... | |
int16_t | direction |
the rotational direction estimate, unitless More... | |
float32_t | oneOverDcBus_invV |
the DC Bus inverse, 1/V More... | |
Defines the estimator (EST) output data.
int32_t _EST_OutputData_::timeStamp |
a time stamp for the output data buffer
float32_t _EST_OutputData_::angle_rad |
the estimated angle value at t = m+1, rad
float32_t _EST_OutputData_::fe_rps |
the electrical frequency estimate, rad/sec
float32_t _EST_OutputData_::fm_rps |
the mechanical frequency estimate, rad/sec
float32_t _EST_OutputData_::fm_lp_rps |
the low pass filtered mechanical frequency estimate, rad/sec
float32_t _EST_OutputData_::fmDot_rps2 |
the mechanical acceleration estimate, rad/sec^2
float32_t _EST_OutputData_::fslip_rps |
the slip frequency estimate, rad/sec
MATH_Vec2 _EST_OutputData_::Eab_V |
the alpha/beta back-EMF estimates, V
MATH_Vec2 _EST_OutputData_::Edq_V |
the direction/quadrature back-EMF estimates, V
int16_t _EST_OutputData_::direction |
the rotational direction estimate, unitless
float32_t _EST_OutputData_::oneOverDcBus_invV |
the DC Bus inverse, 1/V