![]() |
![]() |
Defines the notch filter (FILTER_NOTCH) object. More...
#include <filter_notch.h>
Data Fields | |
float32_t | out1 |
the output value at time sample n=-1 More... | |
float32_t | out2 |
the output value at time sample n=-2 More... | |
float32_t | in |
the input value More... | |
float32_t | in1 |
the input value at time sample n=-1 More... | |
float32_t | in2 |
the input value at time sample n=-2 More... | |
float32_t | out |
the output value More... | |
Defines the notch filter (FILTER_NOTCH) object.
float32_t _FILTER_NOTCH_Obj_::out1 |
the output value at time sample n=-1
Referenced by FILTER_NOTCH_get_out1(), FILTER_NOTCH_run(), and FILTER_NOTCH_set_out1().
float32_t _FILTER_NOTCH_Obj_::out2 |
the output value at time sample n=-2
Referenced by FILTER_NOTCH_get_out2(), FILTER_NOTCH_run(), and FILTER_NOTCH_set_out2().
float32_t _FILTER_NOTCH_Obj_::in |
the input value
Referenced by FILTER_NOTCH_run(), and FILTER_NOTCH_set_in().
float32_t _FILTER_NOTCH_Obj_::in1 |
the input value at time sample n=-1
Referenced by FILTER_NOTCH_get_in1(), FILTER_NOTCH_run(), and FILTER_NOTCH_set_in1().
float32_t _FILTER_NOTCH_Obj_::in2 |
the input value at time sample n=-2
Referenced by FILTER_NOTCH_get_in2(), FILTER_NOTCH_run(), and FILTER_NOTCH_set_in2().
float32_t _FILTER_NOTCH_Obj_::out |
the output value
Referenced by FILTER_NOTCH_get_out(), FILTER_NOTCH_run(), and FILTER_NOTCH_set_out().