Object for the DRV8316 STATUS00 register. More...
#include <drv8316s.h>
Data Fields | |
bool | FAULT:1 |
bool | OT:1 |
bool | OVP:1 |
bool | NPOR:1 |
bool | OCP:1 |
bool | SPI_FLT:1 |
bool | BK_FLT:1 |
bool | rsvd1:1 |
Object for the DRV8316 STATUS00 register.
bool DRV8316_STAT00_BITS::FAULT |
bool DRV8316_STAT00_BITS::OT |
bool DRV8316_STAT00_BITS::OVP |
bool DRV8316_STAT00_BITS::NPOR |
bool DRV8316_STAT00_BITS::OCP |
bool DRV8316_STAT00_BITS::SPI_FLT |
bool DRV8316_STAT00_BITS::BK_FLT |
bool DRV8316_STAT00_BITS::rsvd1 |