Object for the DRV8323 CTRL05 register. More...
#include <drv8323s.h>
Data Fields | |
DRV8323_CTRL05_VDSLVL_e | VDS_LVL:4 |
DRV8323_CTRL05_OcpDeg_e | OCP_DEG:2 |
DRV8323_CTRL05_OcpMode_e | OCP_MODE:2 |
DRV8323_CTRL05_DeadTime_e | DEAD_TIME:2 |
bool | TRETRY:1 |
uint16_t | rsvd:5 |
Object for the DRV8323 CTRL05 register.
DRV8323_CTRL05_VDSLVL_e DRV8323_CTRL05_BITS::VDS_LVL |
DRV8323_CTRL05_OcpDeg_e DRV8323_CTRL05_BITS::OCP_DEG |
DRV8323_CTRL05_OcpMode_e DRV8323_CTRL05_BITS::OCP_MODE |
DRV8323_CTRL05_DeadTime_e DRV8323_CTRL05_BITS::DEAD_TIME |
bool DRV8323_CTRL05_BITS::TRETRY |
uint16_t DRV8323_CTRL05_BITS::rsvd |