Barcodes are crucial in inventory management, asset tracking, ticketing, and information sharing. 1-D and 2-D barcodes condense information into a visually coded form. Laser-based scanners work well for 1-D barcodes, but cameras are required for 2-D, like QR codes. Camera based systems are often called "barcode imagers". The most compute-intensive task of barcode imagers is to find the barcode, rather to decode them. Deep learning is an effective technique for finding these barcodes.
This demo runs a custom trained YOLOX-nano neural network on the AM62A and performs object detection on images to find the 1-D and 2-D barcodes. Regions with detected codes are cropped and converted to grayscale for decoding using an open source library, zbar The decoded text is displayed along with the bounding box resulting from object detection.
The github repo hosting source code and user guides contains everything needed to reproduce or even expand on the demo. There are instructions to run the demo as-is on the AM62A.
Please find the following resources for reproducing the demo. This requires:
python3 apps_python/app_edgeai.py configs/barcode-reader.yaml
./apps_cpp/bin/Release/app_edgeai configs/barcode-reader.yaml
These steps are validated on the 8.6 and 9.0.0 Edge AI Linux SDK. Newer SDK versions may require recompiling the model using edgeai-tidl-tools and pulling from the main edgeai-gst-apps repository for any dependencies that differ.
The setup script will download a pretrained and precompiled model needed for this demo. Additional resources are linked for diving deeper into how the application works and how Edge AI tools were used to enable this application.
| Purpose | Link |
|---|---|
| Retail Source Code with detailed Readme | https://github.com/TexasInstruments/edgeai-gst-apps-barcode-reader/ |
| Application Brief on barcode readers for TI processors | https://www.ti.com/lit/pdf/sprad35 |
| Purpose | Link |
|---|---|
| Edge AI Studio; Model Analyzer and Model Composer | https://dev.ti.com/edgeaistudio/ |
| Top level github page for Edge AI | https://github.com/TexasInstruments/edgeai |
| AM62A Datasheet (superset device) | https://www.ti.com/product/AM62A7 |
| AM62A Academy (Basic Linux Training/bringup) | https://dev.ti.com/tirex/explore/node?node=A__AB.GCF6kV.FoXARl2aj.wg__AM62A-ACADEMY__WeZ9SsL__LATEST |
| Support Forums (See Processors -> AM62A7) | https://e2e.ti.com |