![]() |
![]() |
Z-Stack API Reference
4.30.00.21
|
#include <zstack.h>
Data Fields | |
bool | preConfigKeyEnable |
bool | securityModeEnable |
bool | useDefaultTCLK |
bool | disabledPollRate |
bool | pollRate |
bool | apsAckWaitDuration |
bool | bindingTime |
bool | panID |
bool | maxMissingMacAckLinkFailure |
bool | indirectMsgTimeout |
bool | apsFrameRetries |
bool | bcastRetries |
bool | passiveAckTimeout |
bool | bcastDeliveryTime |
bool | routeExpiryTime |
bool | userDesc |
bool | preConfigKey |
bool | chanList |
bool | multicastRadius |
bool | extendedPANID |
bool | ieeeAddr |
bool | macRxOnIdle |
bool | snifferFeature |
bool | concentratorEnable |
bool | concentratorDiscTime |
bool | nwkUseMultiCast |
bool | devPartOfNetwork |
Structure to send a system config read request. Set to "true" each of the fields that you would like returned in the response zstack_sysConfigReadRsp_t structure.
bool apsAckWaitDuration |
True to return APS Ack Waite Duration
bool apsFrameRetries |
True to return APS Frame Retries
bool bcastDeliveryTime |
True to return Broadcast Delivery Time
bool bcastRetries |
True to return Broadcast Retries
bool bindingTime |
True to return Binding Time
bool chanList |
True to return Channel List (bit masked)
bool concentratorDiscTime |
True to return the Concentrator Discovery Time parameter
bool concentratorEnable |
True to return the Concentrator Enable parameter
bool devPartOfNetwork |
True to return if the device is already part of a network
bool disabledPollRate |
True to return if the poll rate is disabled or not
bool extendedPANID |
True to return the extended PAN ID (APS USE)
bool ieeeAddr |
True to return the IEEE extended address
bool indirectMsgTimeout |
True to return Indirect Message Timeout
bool macRxOnIdle |
True to return the MAC's RxOnIdle parameter
bool maxMissingMacAckLinkFailure |
True to return zgMaxMissingMacAckLinkFailure
bool multicastRadius |
True to return the Multicast radius
bool nwkUseMultiCast |
True to return the Network Multicast Use parameter
bool panID |
True to return PAN ID
bool passiveAckTimeout |
True to return Passive Ack Timeout
bool pollRate |
True to return Poll Rate
bool preConfigKey |
True to return PreConfig Key (16 bytes)
bool preConfigKeyEnable |
True to return Pre Config Key Enable
bool routeExpiryTime |
True to return Route Expiry Time
bool securityModeEnable |
True to return Security Mode Enable (nwk)
bool snifferFeature |
True to return the Sniffer Feature active parameter
bool useDefaultTCLK |
True to return default TCLK flag
bool userDesc |
True to return User Descriptor (16 bytes max)