I2CCC26XX Object. More...
#include <I2CCC26XX.h>
Data Fields | |
I2C_BASE_OBJECT SwiP_Struct | swi |
uint32_t | bitRate |
PIN_State | pinState |
PIN_Handle | hPin |
void * | i2cPostFxn |
Power_NotifyObj | i2cPostObj |
I2CCC26XX Object.
The application must not access any member variables of this structure!
I2C_BASE_OBJECT SwiP_Struct I2CCC26XX_Object::swi |
uint32_t I2CCC26XX_Object::bitRate |
PIN_State I2CCC26XX_Object::pinState |
PIN_Handle I2CCC26XX_Object::hPin |
void* I2CCC26XX_Object::i2cPostFxn |
Power_NotifyObj I2CCC26XX_Object::i2cPostObj |