AES common module header for all devices.
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
Go to the source code of this file.
Data Structures | |
struct | AESCommon_Config |
AES Global configuration. More... | |
Macros | |
#define | AES_STATUS_SUCCESS ((int_fast16_t) 0) |
Successful status code. More... | |
#define | AES_STATUS_ERROR ((int_fast16_t) -1) |
Generic error status code. More... | |
#define | AES_STATUS_RESOURCE_UNAVAILABLE ((int_fast16_t) -2) |
An error status code returned if the hardware or software resource is currently unavailable. More... | |
#define | AES_STATUS_CANCELED ((int_fast16_t) -3) |
The ongoing operation was canceled. More... | |
#define | AES_STATUS_MAC_INVALID ((int_fast16_t) -4) |
The MAC verification failed. More... | |
#define | AES_STATUS_KEYSTORE_INVALID_ID ((int_fast16_t) -5) |
The operation tried to load a key from the keystore using an invalid key ID. More... | |
#define | AES_STATUS_KEYSTORE_GENERIC_ERROR ((int_fast16_t) -6) |
The key store module returned a generic error. See key store documentation for additional details. More... | |
#define | AES_STATUS_FEATURE_NOT_SUPPORTED ((int_fast16_t) -7) |
The operation requested is not supported. More... | |
#define | AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED ((int_fast16_t) -8) |
The operation does not support non-word-aligned input and/or output. More... | |
#define | AES_STATUS_DRIVER_SPECIFIC_ERROR ((int_fast16_t) -16) |
A driver shall use this error code and grow negatively until (AES_STATUS_RESERVED + 1) if more driver specific error codes are needed beyond the common codes listed above. More... | |
#define | AES_STATUS_RESERVED ((int_fast16_t) -32) |
Enumerations | |
enum | AES_ReturnBehavior { AES_RETURN_BEHAVIOR_CALLBACK = 1, AES_RETURN_BEHAVIOR_BLOCKING = 2, AES_RETURN_BEHAVIOR_POLLING = 4 } |
The return behavior of AES functions. More... | |
#define AES_STATUS_SUCCESS ((int_fast16_t) 0) |
Successful status code.
Functions return AES_STATUS_SUCCESS if the function was executed successfully.
#define AES_STATUS_ERROR ((int_fast16_t) -1) |
Generic error status code.
Functions return AES_STATUS_ERROR if the function was not executed successfully and no more pertinent error code could be returned.
#define AES_STATUS_RESOURCE_UNAVAILABLE ((int_fast16_t) -2) |
An error status code returned if the hardware or software resource is currently unavailable.
AES driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.
#define AES_STATUS_CANCELED ((int_fast16_t) -3) |
The ongoing operation was canceled.
#define AES_STATUS_MAC_INVALID ((int_fast16_t) -4) |
The MAC verification failed.
Functions return AES_STATUS_MAC_INVALID if the MAC computed for the provided (key, message) pair did not match the MAC provided.
#define AES_STATUS_KEYSTORE_INVALID_ID ((int_fast16_t) -5) |
The operation tried to load a key from the keystore using an invalid key ID.
This code is returned if the provided CryptoKey reference is returned as invalid by the key store module.
#define AES_STATUS_KEYSTORE_GENERIC_ERROR ((int_fast16_t) -6) |
The key store module returned a generic error. See key store documentation for additional details.
#define AES_STATUS_FEATURE_NOT_SUPPORTED ((int_fast16_t) -7) |
The operation requested is not supported.
#define AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED ((int_fast16_t) -8) |
The operation does not support non-word-aligned input and/or output.
#define AES_STATUS_DRIVER_SPECIFIC_ERROR ((int_fast16_t) -16) |
A driver shall use this error code and grow negatively until (AES_STATUS_RESERVED + 1) if more driver specific error codes are needed beyond the common codes listed above.
Example implementation specific status codes:
#define AES_STATUS_RESERVED ((int_fast16_t) -32) |
Common AES status code reservation offset. AES driver implementations should offset status codes with AES_STATUS_RESERVED growing negatively.
Example implementation specific status codes:
enum AES_ReturnBehavior |
The return behavior of AES functions.
Not all AES operations exhibit the specified return behavior. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specified return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.
AES functions exhibiting the specified return behavior have restrictions on the context from which they may be called.
Task | Hwi | Swi | |
---|---|---|---|
AES_RETURN_BEHAVIOR_CALLBACK | X | X | X |
AES_RETURN_BEHAVIOR_BLOCKING | X | ||
AES_RETURN_BEHAVIOR_POLLING | X | X | X |