Data Fields
ADCBufCC26X2_ParamsExtension Struct Reference

CC26X2 specific extension to ADCBuf_Params. More...

#include <ADCBufCC26X2.h>

Data Fields

ADCBufCC26X2_Sampling_Duration samplingDuration
 
ADCBufCC26X2_Sampling_Mode samplingMode
 
ADCBufCC26X2_Reference_Source refSource
 
bool inputScalingEnabled
 

Detailed Description

CC26X2 specific extension to ADCBuf_Params.

To use non-default CC26X2 specific parameters when calling ADCBuf_open(), a pointer to an instance of this struct must be specified in ADCBuf_Params::custom. Alternatively, these values can be set using the control function after calling ADCBuf_open().

Field Documentation

§ samplingDuration

ADCBufCC26X2_Sampling_Duration ADCBufCC26X2_ParamsExtension::samplingDuration

Amount of time the ADC spends sampling the analogue input

§ samplingMode

ADCBufCC26X2_Sampling_Mode ADCBufCC26X2_ParamsExtension::samplingMode

Specifies whether the ADC spends a fixed amount of time sampling or the entire time since the last conversion

§ refSource

ADCBufCC26X2_Reference_Source ADCBufCC26X2_ParamsExtension::refSource

Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed internal source

§ inputScalingEnabled

bool ADCBufCC26X2_ParamsExtension::inputScalingEnabled

Disable input scaling. Input scaling scales an external analogue signal between 0 and 4.3V to an internal signal of 0 to ~1.4785V. Since the largest permissible input to any pin is VDDS, the maximum range of the ADC is effectively less than 3.8V and continues to shrink as the battery voltage drops. With input scaling disabled, the external analogue signal is passed on directly to the internal electronics. Signals larger than ~1.4785V will damage the device with input scaling disabled.

Input scaling status Maximum permissible ADC input voltage
Enabled VDDS (Battery voltage level)
Disabled 1.4785V

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale