TI-15.4 Stack API
|
#include <api_mac.h>
Data Fields | |
bool | panCoord |
bool | ffd |
bool | mainsPower |
bool | rxOnWhenIdle |
bool | security |
bool | allocAddr |
Structure defines the Capabilities Information bit field.
bool _apimac_capabilityinfo::panCoord |
True if the device is a PAN Coordinator
bool _apimac_capabilityinfo::ffd |
True if the device is a full function device (FFD)
bool _apimac_capabilityinfo::mainsPower |
True if the device is mains powered
bool _apimac_capabilityinfo::rxOnWhenIdle |
True if the device's RX is on when the device is idle
bool _apimac_capabilityinfo::security |
True if the device is capable of sending and receiving secured frames
bool _apimac_capabilityinfo::allocAddr |
True if allocation of a short address in the associate procedure is needed.