TI-15.4 Stack API
|
#include <api_mac.h>
Data Fields | |
ApiMac_status_t | reason |
uint16_t | panId |
uint8_t | logicalChannel |
uint8_t | channelPage |
uint8_t | phyID |
ApiMac_sec_t | sec |
MAC_MLME_SYNC_LOSS_IND type
ApiMac_status_t _apimac_mlmesynclossind::reason |
Reason that the synchronization was lost
uint16_t _apimac_mlmesynclossind::panId |
The PAN ID of the realignment
uint8_t _apimac_mlmesynclossind::logicalChannel |
The logical channel of the realignment
uint8_t _apimac_mlmesynclossind::channelPage |
The channel page of the realignment
uint8_t _apimac_mlmesynclossind::phyID |
PHY ID corresponding to the PHY descriptor of the realignment
ApiMac_sec_t _apimac_mlmesynclossind::sec |
The security parameters for this message