![]() |
![]() |
TI BLE-Stack for Bluetooth 4.2 API Documentation
3.02.02.00
|
Parameter Structure for SNP_HCI_CMD_RSP. More...
Data Fields | |
uint16_t | opcode |
2 Byte HCI opcode that was executed in the request, list of all HCI commands allowed by the SNP. | |
uint8_t * | pData |
uint8_t | status |
1 Byte status of the request (SUCCESS or Error, list of status generated by the SNP.) | |
Parameter Structure for SNP_HCI_CMD_RSP.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.