TI BLE-Stack for Bluetooth API Documentation  3.03.00.00
snp.h
Go to the documentation of this file.
1 /******************************************************************************
2 
3  @file snp.h
4 
5  @brief main header file for the serial network processor
6 
7  Group: WCS, BTS
8  $Target Device: DEVICES $
9 
10  ******************************************************************************
11  $License: BSD3 2015 $
12  ******************************************************************************
13  $Release Name: PACKAGE NAME $
14  $Release Date: PACKAGE RELEASE DATE $
15  *****************************************************************************/
16 
25 #ifndef SNP_H
26 #define SNP_H
27 
28 #ifdef __cplusplus
29 extern "C"
30 {
31 #endif
32 
33 /*********************************************************************
34  * INCLUDES
35  */
36 
37 #include "hal_types.h"
38 
39 /*********************************************************************
40 * EXTERNAL VARIABLES
41 */
42 
48 /*********************************************************************
49  * CONSTANTS
50  */
51 
53 #define SNP_IMAGE_START 0x00000000
54 
56 
59 #define SNP_NPI_ASYNC_CMD_TYPE (RPC_SYS_BLE_SNP+(NPI_MSG_TYPE_ASYNC<<5))
61 #define SNP_NPI_SYNC_REQ_TYPE (RPC_SYS_BLE_SNP+(NPI_MSG_TYPE_SYNCREQ<<5))
63 #define SNP_NPI_SYNC_RSP_TYPE (RPC_SYS_BLE_SNP+(NPI_MSG_TYPE_SYNCRSP<<5))
65 
69 // Fixed size, must not exceed 2 bits!
71 // the upper two bits of NPI frame cmd1 field is reserved for subgroup value.
73  SNP_DEVICE_GRP = 0,
74  SNP_GAP_GRP,
75  SNP_GATT_GRP,
76  SNP_RFU_GRP
77 };
78 
83 #define SNP_MASK_EVT_REQ 0x02
84 #define SNP_GET_REVISION_REQ 0x03
85 #define SNP_HCI_CMD_REQ 0x04
86 #define SNP_GET_STATUS_REQ 0x06
87 #define SNP_GET_RAND_REQ 0x07
88 #define SNP_TEST_REQ 0x10
89 
95 #define SNP_POWER_UP_IND 0x01
96 #define SNP_MASK_EVENT_RSP 0x02
97 #define SNP_GET_REVISION_RSP 0x03
98 #define SNP_HCI_CMD_RSP 0x04
99 #define SNP_EVENT_IND 0x05
100 #define SNP_GET_STATUS_RSP 0x06
101 #define SNP_SYNC_ERROR_CMD_IND 0x07
102 #define SNP_GET_RAND_RSP 0x08
103 #define SNP_TEST_RSP 0x10
104 
110 #define SNP_INIT_DEVICE_REQ 0x41
111 #define SNP_START_ADV_REQ 0x42
112 #define SNP_SET_ADV_DATA_REQ 0x43
113 #define SNP_STOP_ADV_REQ 0x44
114 #define SNP_UPDATE_CONN_PARAM_REQ 0x45
115 #define SNP_TERMINATE_CONN_REQ 0x46
116 #define SNP_SET_GAP_PARAM_REQ 0x48
117 #define SNP_GET_GAP_PARAM_REQ 0x49
118 #define SNP_SET_SECURITY_PARAM_REQ 0x4A
119 #define SNP_SEND_SECURITY_REQUEST_REQ 0x4B
120 #define SNP_SET_AUTHENTICATION_DATA_REQ 0x4C
121 #define SNP_SET_WHITE_LIST_POLICY_REQ 0x4D
122 
128 #define SNP_INIT_DEVICE_CNF 0x41
129 #define SNP_SET_ADV_DATA_CNF 0x43
130 #define SNP_UPDATE_CONN_PARAM_CNF 0x45
131 #define SNP_SET_GAP_PARAM_RSP 0x48
132 #define SNP_GET_GAP_PARAM_RSP 0x49
133 #define SNP_SET_SECURITY_PARAM_RSP 0x4A
134 #define SNP_SEND_AUTHENTICATION_DATA_RSP 0x4C
135 #define SNP_SET_WHITE_LIST_POLICY_RSP 0x4D
136 
142 #define SNP_ADD_SERVICE_REQ 0x81
143 #define SNP_ADD_CHAR_VAL_DECL_REQ 0x82
144 #define SNP_ADD_CHAR_DESC_DECL_REQ 0x83
145 #define SNP_REGISTER_SERVICE_REQ 0x84
146 #define SNP_GET_ATTR_VALUE_REQ 0x85
147 #define SNP_SET_ATTR_VALUE_REQ 0x86
148 #define SNP_CHAR_READ_CNF 0x87
149 #define SNP_CHAR_WRITE_CNF 0x88
150 #define SNP_SEND_NOTIF_IND_REQ 0x89
151 #define SNP_CCCD_UPDATED_CNF 0x8B
152 #define SNP_SET_GATT_PARAM_REQ 0x8C
153 #define SNP_GET_GATT_PARAM_REQ 0x8D
154 #define SNP_REG_PREDEF_SRV_REQ 0x8E
155 
161 #define SNP_ADD_SERVICE_RSP 0x81
162 #define SNP_ADD_CHAR_VAL_DECL_RSP 0x82
163 #define SNP_ADD_CHAR_DESC_DECL_RSP 0x83
164 #define SNP_REGISTER_SERVICE_RSP 0x84
165 #define SNP_GET_ATTR_VALUE_RSP 0x85
166 #define SNP_SET_ATTR_VALUE_RSP 0x86
167 #define SNP_CHAR_READ_IND 0x87
168 #define SNP_CHAR_WRITE_IND 0x88
169 #define SNP_SEND_NOTIF_IND_CNF 0x89
170 #define SNP_CCCD_UPDATED_IND 0x8B
171 #define SNP_SET_GATT_PARAM_RSP 0x8C
172 #define SNP_GET_GATT_PARAM_RSP 0x8D
173 #define SNP_REG_PREDEF_SRV_RSP 0x8E
174 
180 #define SNP_SUCCESS 0x00
181 #define SNP_FAILURE 0x83
182 #define SNP_INVALID_PARAMS 0x84
183 #define SNP_CMD_ALREADY_IN_PROGRESS 0x85
184 #define SNP_CMD_REJECTED 0x86
185 #define SNP_OUT_OF_RESOURCES 0x87
186 #define SNP_UNKNOWN_ATTRIBUTE 0x88
187 #define SNP_UNKNOWN_SERVICE 0x89
188 #define SNP_ALREADY_ADVERTISING 0x8A
189 #define SNP_NOT_ADVERTISING 0x8B
190 #define SNP_HCI_RSP_COLLISION_RSP 0x8C
191 #define SNP_HCI_CMD_UNKNOWN 0x8D
192 #define SNP_GATT_COLLISION 0x8E
193 #define SNP_NOTIF_IND_NOT_ENABLE_BY_CLIENT 0x8F
194 #define SNP_NOTIF_IND_NOT_ALLOWED 0x90
195 #define SNP_NOTIF_IND_NO_CCCD_ATTRIBUTE 0x91
196 #define SNP_NOT_CONNECTED 0x92
197 #define SNP_FAILURE_NO_ATT_RSP 0x93
198 
212 #define SNP_BLE_NO_RESOURCES bleNoResources
213 #define SNP_BLE_GAP_BOND_REJECTED bleGAPBondRejected
214 #define SNP_BLE_MEM_ALLOC_ERROR bleMemAllocError
215 #define SNP_BLE_TIMEOUT bleTimeout
216 #define SNP_INVALIDPARAMETER INVALIDPARAMETER
217 #define SNP_LL_ENC_KEY_REQ_REJECTED LL_ENC_KEY_REQ_REJECTED
218 #define SNP_LL_ENC_KEY_REQ_UNSUPPORTED_FEATURE LL_ENC_KEY_REQ_UNSUPPORTED_FEATURE
219 #define SNP_LL_CTRL_PKT_TIMEOUT_TERM LL_CTRL_PKT_TIMEOUT_TERM
220 #define SNP_LL_STATUS_ERROR_BAD_PARAMETER LL_STATUS_ERROR_BAD_PARAMETER
221 #define SNP_LL_STATUS_ERROR_COMMAND_DISALLOWED LL_STATUS_ERROR_COMMAND_DISALLOWED
222 #define SNP_LL_STATUS_ERROR_FEATURE_NOT_SUPPORTED LL_STATUS_ERROR_FEATURE_NOT_SUPPORTED
223 #define SNP_LL_STATUS_ERROR_CTRL_PROC_ALREADY_ACTIVE LL_STATUS_ERROR_CTRL_PROC_ALREADY_ACTIVE
224 #define SNP_LL_STATUS_ERROR_INACTIVE_CONNECTION LL_STATUS_ERROR_INACTIVE_CONNECTION
225 #define SNP_SMP_PAIRING_FAILED_UNSPECIFIED SMP_PAIRING_FAILED_UNSPECIFIED
226 #define SNP_SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED
227 #define SNP_SMP_PAIRING_FAILED_NOT_SUPPORTED SMP_PAIRING_FAILED_NOT_SUPPORTED
228 #define SNP_SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED
229 #define SNP_SMP_PAIRING_FAILED_AUTH_REQ SMP_PAIRING_FAILED_AUTH_REQ
230 #define SNP_SMP_PAIRING_FAILED_ENC_KEY_SIZE SMP_PAIRING_FAILED_ENC_KEY_SIZE
231 #define SNP_SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED
232 #define SNP_SMP_PAIRING_FAILED_OOB_NOT_AVAIL SMP_PAIRING_FAILED_OOB_NOT_AVAIL
233 #define SNP_SMP_PAIRING_FAILED_CONFIRM_VALUE SMP_PAIRING_FAILED_CONFIRM_VALUE
234 #define SNP_SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED
235 
236 
242 #define SNP_CONN_EST_EVT 0x0001
243 #define SNP_CONN_TERM_EVT 0x0002
244 #define SNP_CONN_PARAM_UPDATED_EVT 0x0004
245 #define SNP_ADV_STARTED_EVT 0x0008
246 #define SNP_ADV_ENDED_EVT 0x0010
247 #define SNP_ATT_MTU_EVT 0x0020
248 #define SNP_SECURITY_EVT 0x0040
249 #define SNP_AUTHENTICATION_EVT 0x0080
250 #define SNP_ERROR_EVT 0x8000
251 
254 #define SNP_DEV_ALL_EVENT_MASK (SNP_CONN_EST_EVT | SNP_CONN_TERM_EVT | \
256 SNP_CONN_PARAM_UPDATED_EVT | SNP_ADV_STARTED_EVT | SNP_ADV_ENDED_EVT | \
257  SNP_ATT_MTU_EVT | SNP_ERROR_EVT)
258 
259 /* HCI Opcodes */
263 #define SNP_HCI_OPCODE_EXT_SET_TX_POWER 0xFC01
264 #define SNP_HCI_OPCODE_EXT_MODEM_TEST_TX 0xFC08
265 #define SNP_HCI_OPCODE_EXT_MODEM_HOP_TEST_TX 0xFC09
266 #define SNP_HCI_OPCODE_EXT_MODEM_TEST_RX 0xFC0A
267 #define SNP_HCI_OPCODE_EXT_END_MODEM_TEST 0xFC0B
268 #define SNP_HCI_OPCODE_EXT_SET_BDADDR 0xFC0C
269 #define SNP_HCI_OPCODE_EXT_SET_SCA 0xFC0D
270 #define SNP_HCI_OPCODE_EXT_ENABLE_PTM 0xFC0E
271 #define SNP_HCI_OPCODE_EXT_SET_MAX_DTM_TX_POWER 0xFC11
272 #define SNP_HCI_OPCODE_EXT_RESET_SYSTEM 0xFC1D
273 #define SNP_HCI_OPCODE_READ_BDADDR 0x1009
274 #define SNP_HCI_OPCODE_READ_RSSI 0x1405
275 #define SNP_HCI_OPCODE_LE_RECEIVER_TEST 0x201D
276 #define SNP_HCI_OPCODE_LE_TRANSMITTER_TEST 0x201E
277 #define SNP_HCI_OPCODE_LE_TEST_END 0x201F
278 #define SNP_HCI_OPCODE_EXT_PER 0xFC14
279 #define SNP_HCI_OPCODE_EXT_DECRYPT 0xFC05
280 #define SNP_HCI_OPCODE_LE_ENCRYPT 0x2017
281 #define SNP_HCI_OPCODE_EXT_OVERRIDE_SL 0xFC1A
282 #define SNP_HCI_OPCODE_EXT_SET_FAST_TX_RESP_TIME 0xFC07
283 #define SNP_HCI_OPCODE_EXT_ONE_PKT_PER_EVT 0xFC02
284 #define SNP_HCI_OPCODE_EXT_GET_CONNECTION_INFO 0xFC20
285 
289 #define SNP_HCI_OPCODE_SIZE 0x02
291 
292 
293 /* Advertising */
297 #define SNP_ADV_TYPE_CONN 0x00
298 #define SNP_ADV_TYPE_SCANABLE 0x02
299 #define SNP_ADV_TYPE_NONCONN 0x03
300 
307 #define SNP_FILTER_POLICY_ALL 0x00
308 #define SNP_FILTER_POLICY_WHITE 0x03
309 
316 #define SNP_ADV_STOP_ON_CONN 0x00
318 #define SNP_ADV_RESTART_ON_CONN_EST 0x01
321 #define SNP_ADV_RESTART_ON_CONN_TERM 0x02
324 
331 #define SNP_SCANRSP_DATA 0x00 // Scan response data
333 #define SNP_NONCONN_ADV_DATA 0x01 // Non-connectable advertising data.
335 #define SNP_CONN_ADV_DATA 0x02 // Connectable advertising data.
337 
341 #define SNP_MAX_ADVDATA_LENGTH 31
343 
345 
348 #define SNP_CT_SUPERVISOR_TO 0x08
349 #define SNP_CT_PEER_REQ 0x13
350 #define SNP_CT_HOST_REQ 0x16
351 #define SNP_CT_CTRL_PKT_TO 0x22
352 #define SNP_CT_CTRL_PKT_INST_PASS 0x28
353 #define SNP_CT_LSTO_VIOLATION 0x3B
354 #define SNP_CT_MIC_FAILURE 0x3D
355 
359 /* Connection Parameters and Updates */
360 #define SNP_CONN_INT_MIN 0x0006
362 #define SNP_CONN_INT_MAX 0x0C80
363 
364 #define SNP_CONN_SL_MIN 0x0000
366 #define SNP_CONN_SL_MAX 0x01F3
367 
368 #define SNP_CONN_SUPERVISOR_TIMEOUT_MIN 0x000A
370 #define SNP_CONN_SUPERVISOR_TIMEOUT_MAX 0x0C80
371 
372 
375 #define SNP_PRIMARY_SERVICE 1
377 #define SNP_SECONDARY_SERVICE 2
379 
381 #define SNP_CHAR_MANAGED_BY_AP 0x00
382 #define SNP_CHAR_MANAGED_BY_NP 0x01
383 
384 
387 #define SNP_16BIT_UUID_SIZE 2
388 #define SNP_128BIT_UUID_SIZE 16
389 
394 #define SNP_GATT_PERMIT_READ 0x01
397 #define SNP_GATT_PERMIT_WRITE 0x02
399 #define SNP_GATT_PERMIT_AUTHEN_READ 0x04
401 #define SNP_GATT_PERMIT_AUTHEN_WRITE 0x08
403 #define SNP_GATT_PERMIT_ENCRYPT_READ 0x40
405 #define SNP_GATT_PERMIT_ENCRYPT_WRITE 0x80
407 
410 #define SNP_GATT_PERM_RFU_MASK (SNP_GATT_PERMIT_READ | \
412  SNP_GATT_PERMIT_WRITE | \
413  SNP_GATT_PERMIT_AUTHEN_READ | \
414  SNP_GATT_PERMIT_AUTHEN_WRITE | \
415  SNP_GATT_PERMIT_ENCRYPT_READ | \
416  SNP_GATT_PERMIT_ENCRYPT_WRITE)
417 
421 #define SNP_GATT_PROP_READ 0x0002
422 #define SNP_GATT_PROP_WRITE_NORSP 0x0004
423 #define SNP_GATT_PROP_WRITE 0x0008
424 #define SNP_GATT_PROP_NOTIFICATION 0x0010
425 #define SNP_GATT_PROP_INDICATION 0x0020
426 
428 #define SNP_GATT_CHAR_MAX_LENGTH 512
430 
434 #define SNP_SEND_NOTIFICATION 0x01
436 #define SNP_SEND_INDICATION 0x02
438 
444 #define SNP_GGS_SERV_ID 0x01
445 #define SNP_DIS_SERV_ID 0x02
446 
451 #define SNP_DEVINFO_SYSTEM_ID 0
452 #define SNP_DEVINFO_MODEL_NUMBER 1
453 #define SNP_DEVINFO_SERIAL_NUMBER 2
454 #define SNP_DEVINFO_FIRMWARE_REV 3
455 #define SNP_DEVINFO_HARDWARE_REV 4
456 #define SNP_DEVINFO_SOFTWARE_REV 5
457 #define SNP_DEVINFO_MANUFACTURER_NAME 6
458 #define SNP_DEVINFO_11073_CERT_DATA 7
459 #define SNP_DEVINFO_PNP_ID 8
460 
461 #define SNP_DEVINFO_SYSTEM_ID_LEN 8
463 
465 #define SNP_DEVINFO_PNP_ID_LEN 7
466 
468 // this is for information only, do not change it here.
469 #define SNP_DEVINFO_STRING_LEN 21
470 
475 #define SNP_GGS_DEVICE_NAME_ATT 0
476 #define SNP_GGS_APPEARANCE_ATT 1
477 #define SNP_GGS_PERI_PRIVACY_FLAG_ATT 2
478 #define SNP_GGS_RECONNCT_ADDR_ATT 3
479 #define SNP_GGS_PERI_CONN_PARAM_ATT 4
480 #define SNP_GGS_PERI_PRIVACY_FLAG_PROPS 5
481 #define SNP_GGS_W_PERMIT_DEVICE_NAME_ATT 6
482 #define SNP_GGS_W_PERMIT_APPEARANCE_ATT 7
483 #define SNP_GGS_W_PERMIT_PRIVACY_FLAG_ATT 8
484 
485 #define SNP_GAP_DEVICE_NAME_LEN 21
487 
488 // Privacy Flag States
489 #define SNP_GAP_PRIVACY_DISABLED 0x00
490 #define SNP_GAP_PRIVACY_ENABLED 0x01
491 
492 
497 #define SNP_DESC_HEADER_GEN_SHORT_UUID 0x01
498 #define SNP_DESC_HEADER_GEN_LONG_UUID 0x02
499 #define SNP_DESC_HEADER_CCCD 0x04
500 #define SNP_DESC_HEADER_FORMAT 0x08
501 #define SNP_DESC_HEADER_USER_DESC 0x80
502 #define SNP_DESC_HEADER_UNSUPPORTED_MASK 0x70
503 
505 #define SNP_GATT_CLIENT_CFG_NOTIFY 0x0001
506 #define SNP_GATT_CLIENT_CFG_INDICATE 0x0002
507 
508 
511 #define SNP_RESPONSE_NOT_NEEDED 0x00
512 #define SNP_RESPONSE_NEEDED 0x01
513 
515 #define SNP_INVALID_HANDLE 0x0000
516 
517 
521 #define SNP_GAP_TERM_CONN_DEFAULT 0x00
522 #define SNP_GAP_TERM_CONN_IMMEDIATLY 0x01
523 
528 #define SNP_GAPBOND_PAIRING_MODE 0x00
529 #define SNP_GAPBOND_IO_CAPABILITIES 0x01
530 #define SNP_GAPBOND_BONDING_ENABLED 0x02
531 #define SNP_GAPBOND_ERASE_ALLBONDS 0x03
532 #define SNP_GAPBOND_LRU_BOND_REPLACEMENT 0x04
533 
538 #define SNP_GAPBOND_PAIRING_STATE_COMPLETE 0x01
539 #define SNP_GAPBOND_PAIRING_STATE_BONDED 0x02
540 #define SNP_GAPBOND_PAIRING_STATE_BOND_SAVED 0x03
541 
545 /*-------------------------------------------------------------------
546 * TYPEDEFS - Initialization and Configuration
547 */
548 /*** Device Data Types ***/
549 
561 PACKED_TYPEDEF_STRUCT
562 {
563  uint16_t eventMask;
567 
575 PACKED_TYPEDEF_STRUCT
576 {
577  uint16_t maskedEvent;
581 
589 PACKED_TYPEDEF_STRUCT
590 {
591  uint16_t memAlo;
592  uint16_t memMax;
593  uint16_t memSize;
595 
603 PACKED_TYPEDEF_STRUCT
604 {
605  uint16_t opcode;
606  uint8_t *pData;
614 
622 PACKED_TYPEDEF_STRUCT
623 {
624  uint8_t status;
625  uint16_t opcode;
626  uint8_t *pData;
633 
641 PACKED_TYPEDEF_STRUCT
642 {
643  uint8_t status;
644  uint16_t snpVer;
645  uint8_t stackBuildVer[10];
647 
655 PACKED_TYPEDEF_STRUCT
656 {
657  uint32_t rand;
659 
665 PACKED_TYPEDEF_STRUCT
666 {
667  uint8_t gapRoleStatus;
668  uint8_t advStatus;
672  uint8_t ATTstatus;
676  uint8_t ATTmethod;
681 
682 /*** GAP Data Types ***/
683 
691 PACKED_TYPEDEF_STRUCT
692 {
693  uint8_t type;
694  uint16_t timeout;
695  uint16_t interval;
698  uint8_t filterPolicy;
702  uint8_t initiatorAddress[6];
703  uint8_t behavior;
705 
706 
716 PACKED_TYPEDEF_STRUCT
717 {
718  uint8_t type;
719  uint8_t *pData;
721 
731 PACKED_TYPEDEF_STRUCT
732 {
733  uint16_t connHandle;
734  uint8_t option;
736 
744 PACKED_TYPEDEF_STRUCT
745 {
746  uint16_t connHandle;
747  uint16_t intervalMin;
748  uint16_t intervalMax;
754  uint16_t slaveLatency;
760  uint16_t supervisionTimeout;
763 
769 
779 PACKED_TYPEDEF_STRUCT
780 {
781  uint8_t status;
782  uint16_t connHandle;
784 
818 PACKED_TYPEDEF_STRUCT
819 {
820  uint16_t paramId;
821  uint16_t value;
823 
833 PACKED_TYPEDEF_STRUCT
834 {
835  uint8_t status;
836  uint16_t paramId;
837  uint16_t value;
839 
851 PACKED_TYPEDEF_STRUCT
852 {
853  uint32_t authData;
855 
856 /*** GATT Data Types ***/
857 
865 PACKED_TYPEDEF_STRUCT
866 {
867  uint8_t type;
868  uint8_t UUID[16];
874 
895 PACKED_TYPEDEF_STRUCT
896 {
897  uint8_t charValPerms;
898  uint16_t charValProps;
899  uint8_t mgmtOption;
900  uint16_t charValMaxLen;
901  uint8_t UUID[16];
909 
917 PACKED_TYPEDEF_STRUCT
918 {
919  uint8_t status;
920  uint16_t attrHandle;
922 
937 PACKED_TYPEDEF_STRUCT
938 {
939  uint8_t perms;
941 
951 PACKED_TYPEDEF_STRUCT
952 {
953  uint8_t format;
954  uint8_t exponent;
955  uint16_t unit;
956  uint8_t namespace;
957  uint16_t desc;
959 
969 PACKED_TYPEDEF_STRUCT
970 {
971  uint8_t perms;
972  uint16_t maxLen;
973  uint16_t initLen;
974  uint8_t *pDesc;
976 
986 PACKED_TYPEDEF_STRUCT
987 {
988  uint8_t perms;
989  uint16_t maxLen;
990  uint8_t UUID[2];
994 
1004 PACKED_TYPEDEF_STRUCT
1005 {
1006  uint8_t perms;
1007  uint16_t maxLen;
1008  uint8_t UUID[16];
1012 
1033 PACKED_TYPEDEF_STRUCT
1034 {
1035  uint8_t header;
1042 
1053 PACKED_TYPEDEF_STRUCT
1054 {
1055  uint8_t status;
1056  uint8_t header;
1057  uint16_t handles[6];
1062 
1070 PACKED_TYPEDEF_STRUCT
1071 {
1072  uint8_t status;
1073  uint16_t startHandle;
1074  uint16_t endHandle;
1076 
1084 PACKED_TYPEDEF_STRUCT
1085 {
1086  uint16_t connHandle;
1087  uint16_t attrHandle;
1088  uint16_t offset;
1089  uint16_t maxSize;
1091 
1099 PACKED_TYPEDEF_STRUCT
1100 {
1101  uint8_t status;
1102  uint16_t connHandle;
1103  uint16_t attrHandle;
1104  uint16_t offset;
1105  uint8_t *pData;
1108 
1118 PACKED_TYPEDEF_STRUCT
1119 {
1120  uint16_t connHandle;
1121  uint16_t attrHandle;
1122  uint8_t rspNeeded;
1123  uint16_t offset;
1124  uint8_t *pData;
1127 
1147 PACKED_TYPEDEF_STRUCT
1148 {
1149  uint8_t status;
1150  uint16_t connHandle;
1152 
1158 PACKED_TYPEDEF_STRUCT
1159 {
1160  uint16_t connHandle;
1161  uint16_t attrHandle;
1162  uint8_t authenticate;
1163  uint8_t type;
1164  uint8_t *pData;
1166 
1235 PACKED_TYPEDEF_STRUCT
1236 {
1237  uint8_t status;
1241 
1257 PACKED_TYPEDEF_STRUCT
1258 {
1259  uint8_t serviceID;
1260  uint8_t paramID;
1263  uint8_t *pData;
1265 
1273 PACKED_TYPEDEF_STRUCT
1274 {
1275  uint16_t attrHandle;
1276  uint8_t *pData;
1278 
1286 PACKED_TYPEDEF_STRUCT
1287 {
1288  uint8_t status;
1289  uint16_t attrHandle;
1291 
1299 PACKED_TYPEDEF_STRUCT
1300 {
1301  uint16_t attrHandle;
1303 
1311 PACKED_TYPEDEF_STRUCT
1312 {
1313  uint8_t status;
1314  uint16_t attrHandle;
1315  uint8_t *pData;
1317 
1325 PACKED_TYPEDEF_STRUCT
1326 {
1327  uint8_t serviceID;
1328  uint8_t paramID;
1330 
1340 PACKED_TYPEDEF_STRUCT
1341 {
1342  uint16_t connHandle;
1343  uint16_t cccdHandle;
1344  uint8_t rspNeeded;
1345  uint16_t value;
1347 
1355 PACKED_TYPEDEF_STRUCT
1356 {
1357  uint8_t useWhiteList;
1359 
1364 typedef union
1365 {
1366  //Mask events
1369 
1370  //Revision
1372 
1373  //Rand
1375 
1376  //HCI
1379 
1380  //Status
1382 
1383  //Test
1385 
1386  //Advertising
1389  snpSetAdvDataCnf_t setAdvDataCnf;
1390 
1391  //Connection
1395 
1396  //GAP Parameters
1398  snpSetGapParamRsp_t setGapParamRsp;
1399  snpGetGapParamReq_t getGapParamReq;
1401 
1402  //Security
1403  snpSetSecParamReq_t setSecParamReq;
1404  snpSetSecParamRsp_t setSecParamRsp;
1406  snpSetAuthDataRsp_t setAuthDataRsp;
1407 
1408  //White List
1410  snpSetWhiteListRsp_t setWhiteListRsp;
1411 
1412  //Services
1414  snpAddServiceRsp_t addServiceRsp;
1420 
1421  //Incoming GATT Requests
1427  snpNotifIndCnf_t notifIndCnf;
1428 
1429  //NP GATT Parameters of predefined services
1433  snpGetGattParamRsp_t getGattParamRsp;
1434 
1435  //CCCD Updates
1437  snpCharCfgUpdatedRsp_t charcfgUpdatedRsp;
1438 } snp_msg_t;
1439 
1440 /*** SNP EVENTS ***/
1441 
1451 PACKED_TYPEDEF_STRUCT
1452 {
1453  uint16_t connHandle;
1454  uint16_t connInterval;
1455  uint16_t slaveLatency;
1457  uint8_t addressType;
1458  uint8_t pAddr[6];
1459 } snpConnEstEvt_t;
1460 
1470 PACKED_TYPEDEF_STRUCT
1471 {
1472  uint16_t connHandle;
1473  uint8_t reason;
1475 
1485 PACKED_TYPEDEF_STRUCT
1486 {
1487  uint16_t connHandle;
1488  uint16_t connInterval;
1489  uint16_t slaveLatency;
1492 
1502 PACKED_TYPEDEF_STRUCT
1503 {
1504  uint8_t status;
1506 
1516 PACKED_TYPEDEF_STRUCT
1517 {
1518  uint8_t state;
1519  uint8_t status;
1521 
1531 PACKED_TYPEDEF_STRUCT
1532 {
1533  uint16_t opcode;
1534  uint8_t status;
1535 } snpErrorEvt_t;
1536 
1546 PACKED_TYPEDEF_STRUCT
1547 {
1548  uint16_t connHandle;
1549  uint16_t attMtuSize;
1551 
1561 PACKED_TYPEDEF_STRUCT
1562 {
1563  uint8_t display;
1564  uint8_t input;
1565  uint32_t numCmp;
1567 
1572 typedef union
1573 {
1582 } snpEventParam_t;
1583 
1591 PACKED_TYPEDEF_STRUCT
1592 {
1593  uint16_t event;
1595 } snpEvt_t;
1596 
1606 typedef struct
1607 {
1608  uint16_t intervalMin;
1609  uint16_t intervalMax;
1610  uint16_t latency;
1611  uint16_t timeout;
1613 
1616 /*********************************************************************
1617  * MACROS
1618  */
1619 
1624 #define SNP_CMD1_HDR_MASK 0xC0
1626 
1628 #define SNP_CMD1_HDR_POS 0x6
1629 
1631 #define SNP_GET_OPCODE_HDR_CMD1(cmd) (((cmd) & SNP_CMD1_HDR_MASK) >> SNP_CMD1_HDR_POS)
1632 
1634 #define SNP_CMD1_ID_MASK 0x3F
1635 
1637 #define SNP_GET_OPCODE_ID_CMD1(cmd) ((cmd) & SNP_CMD1_ID_MASK)
1638 
1641 /*********************************************************************
1642 *********************************************************************/
1643 
1644 #ifdef __cplusplus
1645 }
1646 #endif
1647 
1648 #endif /* SNP_H */
1649 
Parameter Structure for the ATT MTU size updated Event data.
Definition: snp.h:1546
uint16_t offset
2 Byte Offset of the characteristic to start writing to
Definition: snp.h:1123
uint8_t addressType
1 Byte Type of initiator address
Definition: snp.h:1457
Parameter Structure for the Error Event SNP_ERROR_EVT.
Definition: snp.h:1531
uint8_t perms
1 Byte Permissions of the attribute, see GATT Attribute Access Permissions Bit Fields, force to Read only
Definition: snp.h:988
uint16_t intervalMax
2 Byte
Definition: snp.h:1609
uint8_t status
1 Byte Status of the request List of SNP error codes
Definition: snp.h:1534
Parameter Structure for SNP_updateConnParam.
Definition: snp.h:744
uint8_t perms
1 Byte Permissions of the attribute, see GATT Attribute Access Permissions Bit Fields, force to Read only
Definition: snp.h:1006
Parameter Structure for the Security Event.
Definition: snp.h:1516
Parameter Structure for SNP_CHAR_READ_IND / @ ref SNP_charRead.
Definition: snp.h:1084
snpEventParam_t * pEvtParams
snpEventParam_t
Definition: snp.h:1594
snpGetRevisionRsp_t revisionRsp
Get revision Response.
Definition: snp.h:1371
uint16_t connInterval
2 Byte
Definition: snp.h:1488
Parameter Structure for the Characteristic Configuration Update Indication.
Definition: snp.h:1340
uint8_t * pData
Pointer to.
Definition: snp.h:1164
uint8_t status
1 Byte Command Status (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:1237
snpSetGattParamRsp_t setGattParamRsp
Set GATT parameter response.
Definition: snp.h:1431
snpAddCharDescDeclRsp_t addCharDescDeclRsp
Add characteristic descriptor Response.
Definition: snp.h:1418
uint16_t timeout
2 Byte
Definition: snp.h:1611
struct snpCharWriteCnf_t snpNotifIndCnf_t
Parameter Structure for SNP_sendNotifcnf_rsp - Same Structure as snpCharWriteCnf_t.
snpGetGattParamReq_t getGattParamReq
Get GATT parameter response.
Definition: snp.h:1432
uint8_t initiatorAddrType
1 Byte Initiator Address Type, Reserved for Future Use
Definition: snp.h:701
Connection parameters for the peripheral device.
Definition: snp.h:1606
snpGetRandRsp_t randRsp
Get Random Number Response.
Definition: snp.h:1374
snpHciCmdRsp_t hciCmdRsp
HCI command response (event)
Definition: snp.h:1378
snpConnEstEvt_t connEstEvt
Parameter Structure snpConnEstEvt_t.
Definition: snp.h:1574
Parameter Structure for SNP_setGATTParam / SNP_SET_GATT_PARAM_RSP.
Definition: snp.h:1257
Parameter Structure for SNP_getGATTParam / SNP_GET_GATT_PARAM_REQ.
Definition: snp.h:1325
Parameter Structure for the Characteristic Write Request Indication data.
Definition: snp.h:1118
snpRegisterServiceRsp_t registerService
Register service Response.
Definition: snp.h:1419
snpUpdateConnParamReq_t updateConnParamsReq
Update connection parameters indication.
Definition: snp.h:1393
uint16_t startHandle
2 Byte First attribute handle of the registered service
Definition: snp.h:1073
uint16_t attrHandle
2 Byte Attribute handle of the characteristic value.
Definition: snp.h:1314
uint16_t charValMaxLen
Definition: snp.h:900
uint8_t behavior
1 Byte Behavior of Advertisement on connection event, Adv. behavior when connection are established o...
Definition: snp.h:703
snpAddAttrUserDesc_t * pUserDesc
Pointer to Parameter Structure, snpAddAttrUserDesc_t.
Definition: snp.h:1040
snpSetGapParamReq_t setGapParamReq
Set GAP parameter Request.
Definition: snp.h:1397
uint16_t maxLen
Definition: snp.h:1007
Parameter Structure for SNP_UPDATE_CONN_PARAM_CNF.
Definition: snp.h:779
uint16_t opcode
2 Byte HCI opcode that was executed in the request, list of all HCI commands allowed by the SNP...
Definition: snp.h:625
Parameter Structure for SNP_setAuthenticationData / SNP_SET_AUTHENTICATION_DATA_REQ.
Definition: snp.h:851
uint8_t status
1 Byte Status of the request (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:1313
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1487
uint16_t connInterval
2 Byte
Definition: snp.h:1454
snpAddCharValueDeclReq_t addCharValueDecReq
Add characteristic value Request.
Definition: snp.h:1415
uint16_t charValProps
2 Byte property of the value attribute, see GATT Characteristic Properties Bit Fields ...
Definition: snp.h:898
uint16_t attrHandle
2 Byte Handle of the characteristic value attribute being read
Definition: snp.h:1103
uint8_t useWhiteList
1 Byte White List Filter Policy, Advertisement Filter Policy Type
Definition: snp.h:1357
snpSetSecParamRsp_t setSecParamRsp
Set Security Requirements response.
Definition: snp.h:1404
snpAddAttrGenLongUUID_t * pLongUUID
Pointer to Parameter Structure, snpAddAttrGenLongUUID_t.
Definition: snp.h:1037
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1102
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1120
uint8_t perms
1 Byte permissions of the attribute, GATT Attribute Access Permissions Bit Fields ...
Definition: snp.h:939
struct snpSetGattParamRsp_t snpAddServiceRsp_t
1 Byte Command Status Response
uint8_t charValPerms
1 Byte permissions of the value attribute, see GATT Attribute Access Permissions Bit Fields ...
Definition: snp.h:897
snpSetGapParamRsp_t setGapParamRsp
Set GAP parameter Response.
Definition: snp.h:1398
Parameter Structure for the Connection Established Event.
Definition: snp.h:1451
snpSetGattParamReq_t setGattParamReq
Set GATT parameter request.
Definition: snp.h:1430
snpCharReadCnf_t readCnf
Characteristic read confirmation.
Definition: snp.h:1423
struct snpSetGattParamReq_t snpGetGattParamRsp_t
Parameter Structure for SNP_getGATTParam / SNP_GET_GATT_PARAM_RSP.
Parameter Structure for SNP_writeCharCnf / SNP_CHAR_WRITE_CNF.
Definition: snp.h:1147
uint8_t type
1 Byte Type of Advertisement, see Advertisement Type
Definition: snp.h:693
uint8_t * pData
Pointer of Data to write/retrieved.
Definition: snp.h:1263
snpGetGattParamRsp_t getGattParamRsp
Get GATT parameter request.
Definition: snp.h:1433
uint32_t rand
32-bit Random Number generated by TRNG
Definition: snp.h:657
Parameter Structure for the Connection terminated Event.
Definition: snp.h:1470
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1086
uint16_t attrHandle
2 Byte Attribute handle of the characteristic value.
Definition: snp.h:1275
snpMaskEventRsp_t maskEventCnf
event mask confirmation.
Definition: snp.h:1368
snpTermConnReq_t connTermReq
Connection terminated Request.
Definition: snp.h:1392
uint16_t unit
2 Byte Unit, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:955
uint16_t paramId
2 Byte GAP Parameter ID, GAP Parameter IDs
Definition: snp.h:836
uint16_t connHandle
2 Byte Connection Handle to terminate
Definition: snp.h:733
uint8_t * pData
Definition: snp.h:626
struct snpSetGattParamRsp_t snpSetGapParamRsp_t
1 Byte Command Status Response
Parameter Structure for SNP_addDescriptionValue.
Definition: snp.h:1033
snpUpdateConnParamCnf_t updateConnParamsCnf
Update connection parameters, request.
Definition: snp.h:1394
snpNotifIndCnf_t notifIndCnf
Indication Confirmation.
Definition: snp.h:1427
uint8_t state
1 Byte New Security State Security States
Definition: snp.h:1518
Parameter Structure for the Advertising state change Event.
Definition: snp.h:1502
Parameter Structure used to add a generic attribute descriptor (long UUID)
Definition: snp.h:1004
snpAdvStatusEvt_t advStatusEvt
Parameter Structure snpAdvStatusEvt_t.
Definition: snp.h:1577
Parameter Structure used to add a Format attribute.
Definition: snp.h:951
Parameter Structure to add new Characteristic Description Response SNP_ADD_CHAR_DESC_DECL_RSP.
Definition: snp.h:1053
Parameter Structure for MITM Authentication data to be displayed.
Definition: snp.h:1561
uint16_t value
2 Byte Value to write to the CCCD
Definition: snp.h:1345
SNP Event Parameters.
Definition: snp.h:1572
uint8_t exponent
1 Byte Exponent, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:954
uint8_t paramID
1 Byte ID of the parameter to retrieved.
Definition: snp.h:1328
uint8_t header
1 Byte Header Field, SNP GATT Descriptors Header
Definition: snp.h:1035
uint16_t memMax
2 Byte maximum HEAP ever allocated since startup
Definition: snp.h:592
uint8_t input
1 Byte TRUE if device must input passcode.
Definition: snp.h:1564
struct snpSetGattParamRsp_t snpSetWhiteListRsp_t
1 Byte Command Status Response
uint8_t authenticate
1 Byte Reserved for future use
Definition: snp.h:1162
snpAuthenticationEvt_t authenticationEvt
Parameter Structure snpAuthenticationEvt_t.
Definition: snp.h:1581
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1453
uint8_t type
1 Byte Type of the service to add. see Service Type
Definition: snp.h:867
snpStartAdvReq_t startAdv
Start advertising request.
Definition: snp.h:1387
uint8_t rspNeeded
1 Byte Indicate if the AP must answer this indication or not, Options for Response Needed Field ...
Definition: snp.h:1344
uint16_t maxLen
Definition: snp.h:989
Parameter Structure for the response to SNP_getRev.
Definition: snp.h:655
uint16_t offset
2 Byte Offset of the characteristic to start reading from
Definition: snp.h:1104
uint8_t option
1 Byte Type of disconnection requested. see GAP GATT Terminate connection request option field...
Definition: snp.h:734
snpUpdateConnParamEvt_t updateConnParamEvt
Parameter Structure snpUpdateConnParamEvt_t.
Definition: snp.h:1576
Parameter Structure for SNP_registerService / SNP_REGISTER_SERVICE_RSP.
Definition: snp.h:1070
uint16_t cccdHandle
2 Byte Handle of the characteristic value attribute to notify/indicate
Definition: snp.h:1343
snpCharCfgUpdatedInd_t charCfgUpdatedReq
Characteristic configuration updated indication.
Definition: snp.h:1436
snpAddAttrGenShortUUID_t * pShortUUID
Pointer to Parameter Structure, snpAddAttrGenShortUUID_t.
Definition: snp.h:1036
snpHciCmdReq_t hciCmdReq
HCI command request.
Definition: snp.h:1377
Parameter Structure for the Update Connection Parameter Event.
Definition: snp.h:1485
uint16_t maxLen
2 Byte Maximum possible length of the string, plus one byte for null terminator (range from 1 to 512)...
Definition: snp.h:972
uint16_t intervalMin
2 Byte
Definition: snp.h:1608
Parameter Structure for SNP_CHAR_READ_CNF / snpCharReadCnf_t.
Definition: snp.h:1099
snpCharWriteInd_t charWriteInd
Characteristic write request.
Definition: snp.h:1424
uint8_t gapRoleStatus
1 Byte Current state of the GAP Role ( gaprole_States_t)
Definition: snp.h:667
struct snpSetGapParamReq_t snpGetGapParamReq_t
Parameter Structure for SNP_getGapParam / SNP_GET_GAP_PARAM_REQ - Same Structure as snpSetGapParamReq...
uint16_t attMtuSize
2 Byte New ATT MTU Size negotiated between GATT client and GATT server.
Definition: snp.h:1549
snpCharWriteCnf_t charWriteCnf
Characteristic write confirmation.
Definition: snp.h:1425
struct snpCharWriteCnf_t snpCharCfgUpdatedRsp_t
Parameter Structure for SNP_processCharConfigUpdatedCnf / SNP_CCCD_UPDATED_CNF - Same Structure as sn...
uint8_t display
1 Byte TRUE if device must display passcode.
Definition: snp.h:1563
uint16_t slaveLatency
2 Byte
Definition: snp.h:1455
uint8_t status
1 Byte Status List of SNP error codes
Definition: snp.h:1504
snpErrorEvt_t advErrorEvt
Parameter Structure snpErrorEvt_t.
Definition: snp.h:1579
uint8_t status
1 Byte Status of the request (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:835
snpAddCharValueDeclRsp_t addCharValueDecRsp
Add characteristic value Response.
Definition: snp.h:1416
uint8_t status
status of the request (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:781
Parameter Structure used for SNP_addCharValueDecl / SNP_ADD_CHAR_VAL_DECL_REQ.
Definition: snp.h:895
1 Byte Command Status Response
Definition: snp.h:1235
snpTestCmdRsp_t testCmdRsp
Test command response.
Definition: snp.h:1384
uint16_t attrHandle
2 Byte Attribute handle of the characteristic value.
Definition: snp.h:1301
uint8_t status
1 Byte status of the request (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:643
struct snpSetGapParamReq_t snpSetSecParamReq_t
Parameter Structure for SNP_setSecurityParams / SNP_SET_SECURITY_PARAM_REQ - Same Structure as snpSet...
Parameter Structure used to add a Client Characteristic Configuration Description Attribute...
Definition: snp.h:937
uint16_t opcode
2 Byte SNP opcode that triggered the error
Definition: snp.h:1533
uint16_t value
2 Byte Parameter Value set if for SET command
Definition: snp.h:821
uint16_t connHandle
handle of the connection the parameter update was intended for
Definition: snp.h:782
uint8_t * pData
Pointer of data value to set.
Definition: snp.h:1276
snpAddAttrFormat_t * pFormat
Pointer to Parameter Structure, snpAddAttrFormat_t.
Definition: snp.h:1039
snpSetWhiteListReq_t setWhiteListReq
Set the White List Filter Policy request.
Definition: snp.h:1409
SNP_CMD1_HDR_TYPE
list of subgroup
Definition: snp.h:72
uint16_t timeout
2 Byte Timeout of the advertisement.
Definition: snp.h:694
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1472
uint8_t serviceID
1 Byte ID of the service containing the parameter to define
Definition: snp.h:1327
Add Service Request Structure for SNP_addService / SNP_ADD_SERVICE_REQ.
Definition: snp.h:865
snpSecurityEvt_t securityEvt
Parameter Structure snpSecurityEvt_t.
Definition: snp.h:1580
Parameter Structure for SNP_maskEvt.
Definition: snp.h:561
uint16_t opcode
Definition: snp.h:605
snpSetAdvDataCnf_t setAdvDataCnf
Set advertising data Response.
Definition: snp.h:1389
uint16_t connHandle
2 Byte handle of the connection to update parameters to.
Definition: snp.h:746
Parameter Structure for SNP_setWhiteListFilterPolicy / SNP_SET_WHITE_LIST_POLICY_REQ.
Definition: snp.h:1355
Parameter Structure for SNP_MASK_EVENT_RSP.
Definition: snp.h:575
uint16_t memSize
2 Byte total HEAP size
Definition: snp.h:593
uint8_t rspNeeded
1 Byte Indicate if the AP must answer this indication or not, Options for Response Needed Field ...
Definition: snp.h:1122
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1150
uint8_t status
1 Byte Status of the request (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:1288
uint16_t memAlo
2 Byte HEAP allocated memory
Definition: snp.h:591
struct snpSetGattParamRsp_t snpSetAuthDataRsp_t
1 Byte Command Status Response
uint16_t event
2 Byte Event, list of asynchronous events generated by the SNP.
Definition: snp.h:1593
Parameter Structure for Response to SNP_addCharValueDecl / SNP_ADD_CHAR_VAL_DECL_RSP.
Definition: snp.h:917
uint16_t attrHandle
2 Byte Handle of the characteristic value attribute being written
Definition: snp.h:1121
uint8_t mgmtOption
1 Byte Reserved for future use
Definition: snp.h:899
struct snpSetGattParamRsp_t snpSetSecParamRsp_t
1 Byte Command Status Response
uint16_t snpVer
2 Byte Version of the SNP (major, minor)
Definition: snp.h:644
uint8_t * pData
Pointer to the advertisement data buffer to update, up to 31 Bytes.
Definition: snp.h:719
uint32_t numCmp
32 bit Numeric Comparison value to display, 0 if not used.
Definition: snp.h:1565
uint8_t status
1 Byte Status of the request (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:1072
uint16_t maskedEvent
Definition: snp.h:577
Parameter Structure used to add a generic attribute descriptor (short UUID)
Definition: snp.h:986
uint8_t status
1 Byte Status upon entering this state List of SNP error codes
Definition: snp.h:1519
Parameter Structure for the Characteristic Notification and Indication Request data This is a packed ...
Definition: snp.h:1158
uint8_t status
1 Byte status of the request (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:624
uint16_t value
2 Byte Parameter Value retrieved.
Definition: snp.h:837
snpGetGapParamRsp_t getGapParamRsp
Get GAP parameter Response.
Definition: snp.h:1400
snpSetAuthDataReq_t setAuthDataReq
Set Authentication Data request.
Definition: snp.h:1405
uint8_t type
1 Byte Type of Advertisement data to update, see Adv. data buffer
Definition: snp.h:718
uint16_t attrHandle
2 Byte Attribute handle of the characteristic value.
Definition: snp.h:1289
uint16_t attrHandle
2 Byte Handle of the characteristic value attribute to notify/indicate
Definition: snp.h:1161
uint8_t status
1 Byte Status of the request (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:1101
snpSetAuthDataRsp_t setAuthDataRsp
Set Authentication Data response.
Definition: snp.h:1406
uint16_t intervalMin
2 Byte Minimum value for the connection event interval.
Definition: snp.h:747
uint8_t serviceID
Definition: snp.h:1259
uint8_t reason
1 Byte Reason of the termination connection termination reason.
Definition: snp.h:1473
Parameter Structure for SNP_setGapParam / SNP_SET_GAP_PARAM_REQ.
Definition: snp.h:818
uint8_t * pData
Pointer to data of the value to set.
Definition: snp.h:1315
uint16_t latency
2 Byte
Definition: snp.h:1610
snpGetStatusCmdRsp_t getStatusRsp
Get status Response.
Definition: snp.h:1381
uint16_t offset
2 Byte Offset of the characteristic to start reading from
Definition: snp.h:1088
snpGetGapParamReq_t getGapParamReq
Get GAP parameter Request.
Definition: snp.h:1399
uint8_t perms
1 Byte Permissions of the attribute, GATT Attribute Access Permissions Bit Fields, force to Read only
Definition: snp.h:971
Connection Termination Request Structure.
Definition: snp.h:731
uint16_t supervisionTimeout
2 Byte
Definition: snp.h:1490
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1160
snpSetAdvDataReq_t setAdvDataReq
Set advertising data Request.
Definition: snp.h:1388
uint16_t desc
< 1 Byte Namespace, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:956
uint8_t status
1 Byte Status of the request (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:1149
uint8_t header
Definition: snp.h:1056
SNP Event Structure.
Definition: snp.h:1591
Parameter Structure for the Get GAP Parameter Value Response.
Definition: snp.h:833
Parameter Structure for SNP_getAttrValue / SNP_SET_ATTR_VALUE_REQ.
Definition: snp.h:1299
uint8_t status
1 Byte Command Status List of SNP error codes
Definition: snp.h:1055
uint16_t endHandle
2 Byte Last attribute handle of the registered service
Definition: snp.h:1074
snpAddServiceRsp_t addServiceRsp
Add service response.
Definition: snp.h:1414
Parameter Structure for response to SNP_setAttrValue / SNP_SET_ATTR_VALUE_RSP.
Definition: snp.h:1286
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1342
snpAddAttrCccd_t * pCCCD
Pointer to Parameter Structure, snpAddAttrCccd_t.
Definition: snp.h:1038
The SNP message. A union of all SNP message types.
Definition: snp.h:1364
uint16_t attrHandle
2 Byte Handle of the characteristic value attribute being read
Definition: snp.h:1087
snpSetWhiteListRsp_t setWhiteListRsp
Set the White List Filter Policy response.
Definition: snp.h:1410
uint16_t maxSize
2 Byte Max Size of the data to read
Definition: snp.h:1089
uint8_t status
1 Byte status of the request (SUCCESS or Error, List of SNP error codes)
Definition: snp.h:919
struct snpSetGattParamRsp_t snpSetAdvDataCnf_t
1 Byte Command Status Response
snpATTMTUSizeEvt_t attMTUSizeEvt
Parameter Structure snpATTMTUSizeEvt_t.
Definition: snp.h:1578
Parameter Structure for SNP_startAdv.
Definition: snp.h:691
Parameter Structure for SNP_getRev.
Definition: snp.h:641
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1548
uint32_t authData
4 Byte Authentication Data. 000000 - 999999 or TRUE/FALSE
Definition: snp.h:853
snpAddServiceReq_t addServiceReq
Add service request.
Definition: snp.h:1413
uint8_t format
1 Byte Format, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:953
uint16_t attrHandle
2 Byte attribute handle of the characteristic value.
Definition: snp.h:920
uint8_t * pData
Definition: snp.h:1124
uint16_t paramId
2 Byte GAP Parameter ID, GAP Parameter IDs or snpSetSecParamReq_t
Definition: snp.h:820
snpAddCharDescDeclReq_t addCharDescDeclReq
Add characteristic descriptor Request.
Definition: snp.h:1417
Parameter Structure for response to SNP_getAttrValue / SNP_SET_ATTR_VALUE_RSP.
Definition: snp.h:1311
Parameter Structure for SNP_setAttrValue / SNP_SET_ATTR_VALUE_REQ.
Definition: snp.h:1273
Parameter Structure for SNP_HCI_CMD_RSP.
Definition: snp.h:622
uint8_t * pData
Definition: snp.h:1105
Parameter Structure for the response to SNP_getStatus This is a packed structure. see Dealing with Pa...
Definition: snp.h:665
snpMaskEventReq_t maskEventReq
event mask request.
Definition: snp.h:1367
Parameter Structure for SNP_setAdvData.
Definition: snp.h:716
snpCharCfgUpdatedRsp_t charcfgUpdatedRsp
Characteristic configuration update response.
Definition: snp.h:1437
snpConnTermEvt_t connTermEvt
Parameter Structure snpConnTermEvt_t.
Definition: snp.h:1575
uint16_t initLen
2 Byte initial length of the string, plus one byte for null terminator (must be <= snpAddAttrUserDesc...
Definition: snp.h:973
snpCharReadInd_t readInd
Characteristic read request.
Definition: snp.h:1422
uint8_t * pDesc
Pointer to initial string (must be null terminated)
Definition: snp.h:974
uint16_t eventMask
Definition: snp.h:563
uint8_t type
1 Byte Type of the request, see SNP indication type
Definition: snp.h:1163
Parameter Structure used to add a User Descriptor attribute.
Definition: snp.h:969
snpSetSecParamReq_t setSecParamReq
Set the Security Requirements request.
Definition: snp.h:1403
Parameter Structure for SNP_executeHCIcmd.
Definition: snp.h:603
snpNotifIndReq_t notifIndReq
Notification or indication request.
Definition: snp.h:1426
uint16_t supervisionTimeout
2 Byte
Definition: snp.h:1456
Parameter Structure for SNP_executeTestCmd.
Definition: snp.h:589
uint16_t slaveLatency
2 Byte
Definition: snp.h:1489
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale