![]() |
![]() |
TI BLE-Stack for Bluetooth API Documentation
3.03.00.00
|
Parameter Structure for the Error Event SNP_ERROR_EVT. More...
Data Fields | |
uint16_t | opcode |
2 Byte SNP opcode that triggered the error | |
uint8_t | status |
1 Byte Status of the request List of SNP error codes | |
Parameter Structure for the Error Event SNP_ERROR_EVT.
See SNP Event Indication for more information.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.