SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
_device_commands_t Union Reference

Data Fields

SlSocketCommand_t EventMask
 
SlSendRecvCommand_t DeviceInit
 

Detailed Description

Definition at line 1149 of file protocol.h.

Field Documentation

§ DeviceInit

SlSendRecvCommand_t DeviceInit

Definition at line 1152 of file protocol.h.

§ EventMask

SlSocketCommand_t EventMask

Definition at line 1151 of file protocol.h.


The documentation for this union was generated from the following file: