CC26xx Driver Library
systick.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_ints.h"
#include "../inc/hw_nvic.h"
#include "../inc/hw_types.h"
#include "debug.h"
#include "interrupt.h"

Functions

static void SysTickEnable (void)
 Enables the SysTick counter. More...
 
static void SysTickDisable (void)
 Disables the SysTick counter. More...
 
static void SysTickIntRegister (void(*pfnHandler)(void))
 Registers an interrupt handler for the SysTick interrupt in the dynamic interrupt table. More...
 
static void SysTickIntUnregister (void)
 Unregisters the interrupt handler for the SysTick interrupt in the dynamic interrupt table. More...
 
static void SysTickIntEnable (void)
 Enables the SysTick interrupt. More...
 
static void SysTickIntDisable (void)
 Disables the SysTick interrupt. More...
 
static void SysTickPeriodSet (uint32_t ui32Period)
 Sets the period of the SysTick counter. More...
 
static uint32_t SysTickPeriodGet (void)
 Gets the period of the SysTick counter. More...
 
static uint32_t SysTickValueGet (void)
 Gets the current value of the SysTick counter. More...