TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_mlmecommstatusind Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_status_t status
 
ApiMac_sAddr_t srcAddr
 
ApiMac_sAddr_t dstAddr
 
uint16_t panId
 
ApiMac_commStatusReason_t reason
 
ApiMac_sec_t sec
 

Detailed Description

MAC_MLME_COMM_STATUS_IND type

Field Documentation

§ status

ApiMac_status_t _apimac_mlmecommstatusind::status

status of the event

§ srcAddr

ApiMac_sAddr_t _apimac_mlmecommstatusind::srcAddr

The source address associated with the event

§ dstAddr

ApiMac_sAddr_t _apimac_mlmecommstatusind::dstAddr

The destination address associated with the event

§ panId

uint16_t _apimac_mlmecommstatusind::panId

The PAN ID associated with the event

§ reason

ApiMac_commStatusReason_t _apimac_mlmecommstatusind::reason

The reason the event was generated

§ sec

ApiMac_sec_t _apimac_mlmecommstatusind::sec

The security parameters for this message


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale