TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_mlmediassociatecnf Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_status_t status
 
ApiMac_sAddr_t deviceAddress
 
uint16_t panId
 

Detailed Description

MAC_MLME_DISASSOCIATE_CNF type

Field Documentation

§ status

ApiMac_status_t _apimac_mlmediassociatecnf::status

status of the disassociate attempt

§ deviceAddress

ApiMac_sAddr_t _apimac_mlmediassociatecnf::deviceAddress

The address of the device that has either requested disassociation or been instructed to disassociate by its coordinator

§ panId

uint16_t _apimac_mlmediassociatecnf::panId

The pan ID of the device that has either requested disassociation or been instructed to disassociate by its coordinator


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale