TI-15.4 Stack API  4.20.00.14
Data Fields
_apimac_mlmepollreq Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_sAddr_t coordAddress
 
uint16_t coordPanId
 
ApiMac_sec_t sec
 

Detailed Description

MLME poll request type

Field Documentation

§ coordAddress

ApiMac_sAddr_t _apimac_mlmepollreq::coordAddress

The address of the coordinator device to poll

§ coordPanId

uint16_t _apimac_mlmepollreq::coordPanId

The PAN ID of the coordinator

§ sec

ApiMac_sec_t _apimac_mlmepollreq::sec

The security parameters for this message


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale