CC26xx Driver Library
[ssi.h] Synchronous Serial Interface

Functions

void SSIConfigSetExpClk (uint32_t ui32Base, uint32_t ui32SSIClk, uint32_t ui32Protocol, uint32_t ui32Mode, uint32_t ui32BitRate, uint32_t ui32DataWidth)
 Configures the synchronous serial port. More...
 
static void SSIEnable (uint32_t ui32Base)
 Enables the synchronous serial port. More...
 
static void SSIDisable (uint32_t ui32Base)
 Disables the synchronous serial port. More...
 
void SSIDataPut (uint32_t ui32Base, uint32_t ui32Data)
 Puts a data element into the SSI transmit FIFO. More...
 
int32_t SSIDataPutNonBlocking (uint32_t ui32Base, uint32_t ui32Data)
 Puts a data element into the SSI transmit FIFO. More...
 
void SSIDataGet (uint32_t ui32Base, uint32_t *pui32Data)
 Gets a data element from the SSI receive FIFO. More...
 
int32_t SSIDataGetNonBlocking (uint32_t ui32Base, uint32_t *pui32Data)
 Gets a data element from the SSI receive FIFO. More...
 
static bool SSIBusy (uint32_t ui32Base)
 Determines whether the SSI transmitter is busy or not. More...
 
static uint32_t SSIStatus (uint32_t ui32Base)
 Get the status of the SSI data buffers. More...
 
void SSIIntRegister (uint32_t ui32Base, void(*pfnHandler)(void))
 Registers an interrupt handler for the Synchronous Serial Interface in the dynamic interrupt table. More...
 
void SSIIntUnregister (uint32_t ui32Base)
 Unregisters an interrupt handler for the Synchronous Serial Interface in the dynamic interrupt table. More...
 
static void SSIIntEnable (uint32_t ui32Base, uint32_t ui32IntFlags)
 Enables individual SSI interrupt sources. More...
 
static void SSIIntDisable (uint32_t ui32Base, uint32_t ui32IntFlags)
 Disables individual SSI interrupt sources. More...
 
static void SSIIntClear (uint32_t ui32Base, uint32_t ui32IntFlags)
 Clears SSI interrupt sources. More...
 
static uint32_t SSIIntStatus (uint32_t ui32Base, bool bMasked)
 Gets the current interrupt status. More...
 
static void SSIDMAEnable (uint32_t ui32Base, uint32_t ui32DMAFlags)
 Enable SSI DMA operation. More...
 
static void SSIDMADisable (uint32_t ui32Base, uint32_t ui32DMAFlags)
 Disable SSI DMA operation. More...
 

Detailed Description

Function Documentation

§ SSIBusy()

static bool SSIBusy ( uint32_t  ui32Base)
inlinestatic

Determines whether the SSI transmitter is busy or not.

Allows the caller to determine whether all transmitted bytes have cleared the transmitter hardware. If false is returned, then the transmit FIFO is empty and all bits of the last transmitted word have left the hardware shift register.

Parameters
ui32Baseis the base address of the SSI port.
Returns
Returns status of the SSI transmit buffer.
  • true : SSI is transmitting.
  • false : SSI transmissions are complete.
376 {
377  // Check the arguments.
378  ASSERT(SSIBaseValid(ui32Base));
379 
380  // Determine if the SSI is busy.
381  return((HWREG(ui32Base + SSI_O_SR) & SSI_SR_BSY) ? true : false);
382 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIConfigSetExpClk()

void SSIConfigSetExpClk ( uint32_t  ui32Base,
uint32_t  ui32SSIClk,
uint32_t  ui32Protocol,
uint32_t  ui32Mode,
uint32_t  ui32BitRate,
uint32_t  ui32DataWidth 
)

Configures the synchronous serial port.

This function configures the synchronous serial port. It sets the SSI protocol, mode of operation, bit rate, and data width.

The ui32Protocol parameter defines the data frame format. The Motorola frame formats imply the following polarity and phase configurations:

Polarity Phase       Mode
  0       0   SSI_FRF_MOTO_MODE_0
  0       1   SSI_FRF_MOTO_MODE_1
  1       0   SSI_FRF_MOTO_MODE_2
  1       1   SSI_FRF_MOTO_MODE_3

The ui32Mode parameter defines the operating mode of the SSI module. The SSI module can operate as a master or slave; if a slave, the SSI can be configured to disable output on its serial output line.

The ui32BitRate parameter defines the bit rate for the SSI. This bit rate must satisfy the following clock ratio criteria:

  • Master mode : FSSI >= 2 * bit rate
  • Slave mode : FSSI >= 12 * bit rate

where FSSI is the frequency of the clock supplied to the SSI module.

The ui32DataWidth parameter defines the width of the data transfers, and can be a value between 4 and 16, inclusive.

Note
The peripheral clock is not necessarily the same as the processor clock. The frequency of the peripheral clock is set by the system control.
Parameters
ui32Basespecifies the SSI module base address.
ui32SSIClkis the rate of the clock supplied to the SSI module.
ui32Protocolspecifies the data transfer protocol. The parameter can be one of the following values:
ui32Modespecifies the mode of operation. The parameter can be one of the following values:
ui32BitRatespecifies the clock rate.
ui32DataWidthspecifies number of bits transferred per frame. Must be a value between 4 and 16, both included.
Returns
None
71 {
72  uint32_t ui32MaxBitRate;
73  uint32_t ui32RegVal;
74  uint32_t ui32PreDiv;
75  uint32_t ui32SCR;
76  uint32_t ui32SPH_SPO;
77 
78  // Check the arguments.
79  ASSERT(SSIBaseValid(ui32Base));
80  ASSERT((ui32Protocol == SSI_FRF_MOTO_MODE_0) ||
81  (ui32Protocol == SSI_FRF_MOTO_MODE_1) ||
82  (ui32Protocol == SSI_FRF_MOTO_MODE_2) ||
83  (ui32Protocol == SSI_FRF_MOTO_MODE_3) ||
84  (ui32Protocol == SSI_FRF_TI) ||
85  (ui32Protocol == SSI_FRF_NMW));
86  ASSERT((ui32Mode == SSI_MODE_MASTER) ||
87  (ui32Mode == SSI_MODE_SLAVE) ||
88  (ui32Mode == SSI_MODE_SLAVE_OD));
89  ASSERT(((ui32Mode == SSI_MODE_MASTER) && (ui32BitRate <= (ui32SSIClk / 2))) ||
90  ((ui32Mode != SSI_MODE_MASTER) && (ui32BitRate <= (ui32SSIClk / 12))));
91  ASSERT((ui32SSIClk / ui32BitRate) <= (254 * 256));
92  ASSERT((ui32DataWidth >= 4) && (ui32DataWidth <= 16));
93 
94  // Set the mode.
95  ui32RegVal = (ui32Mode == SSI_MODE_SLAVE_OD) ? SSI_CR1_SOD : 0;
96  ui32RegVal |= (ui32Mode == SSI_MODE_MASTER) ? 0 : SSI_CR1_MS;
97  HWREG(ui32Base + SSI_O_CR1) = ui32RegVal;
98 
99  // Set the clock predivider.
100  ui32MaxBitRate = ui32SSIClk / ui32BitRate;
101  ui32PreDiv = 0;
102  do
103  {
104  ui32PreDiv += 2;
105  ui32SCR = (ui32MaxBitRate / ui32PreDiv) - 1;
106  }
107  while(ui32SCR > 255);
108  HWREG(ui32Base + SSI_O_CPSR) = ui32PreDiv;
109 
110  // Set protocol and clock rate.
111  ui32SPH_SPO = (ui32Protocol & 3) << 6;
112  ui32Protocol &= SSI_CR0_FRF_M;
113  ui32RegVal = (ui32SCR << 8) | ui32SPH_SPO | ui32Protocol | (ui32DataWidth - 1);
114  HWREG(ui32Base + SSI_O_CR0) = ui32RegVal;
115 }
#define SSI_MODE_SLAVE_OD
Definition: ssi.h:128
#define SSI_FRF_MOTO_MODE_0
Definition: ssi.h:119
#define SSI_FRF_MOTO_MODE_2
Definition: ssi.h:121
#define SSI_FRF_TI
Definition: ssi.h:123
#define ASSERT(expr)
Definition: debug.h:71
#define SSI_MODE_SLAVE
Definition: ssi.h:127
#define SSI_FRF_NMW
Definition: ssi.h:124
#define SSI_FRF_MOTO_MODE_3
Definition: ssi.h:122
#define SSI_FRF_MOTO_MODE_1
Definition: ssi.h:120
#define SSI_MODE_MASTER
Definition: ssi.h:126

§ SSIDataGet()

void SSIDataGet ( uint32_t  ui32Base,
uint32_t *  pui32Data 
)

Gets a data element from the SSI receive FIFO.

This function gets received data from the receive FIFO of the specified SSI module and places that data into the location specified by the pui32Data parameter.

Note
Only the lower N bits of the value written to pui32Data contain valid data, where N is the data width as configured by SSIConfigSetExpClk(). For example, if the interface is configured for 8-bit data width, only the lower 8 bits of the value written to pui32Data contain valid data.
Parameters
ui32Basespecifies the SSI module base address.
pui32Datais a pointer to a storage location for data that was received over the SSI interface.
Returns
None

Referenced by SSIDisable().

171 {
172  // Check the arguments.
173  ASSERT(SSIBaseValid(ui32Base));
174 
175  // Wait until there is data to be read.
176  while(!(HWREG(ui32Base + SSI_O_SR) & SSI_SR_RNE))
177  {
178  }
179 
180  // Read data from SSI.
181  *pui32Data = HWREG(ui32Base + SSI_O_DR);
182 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIDataGetNonBlocking()

int32_t SSIDataGetNonBlocking ( uint32_t  ui32Base,
uint32_t *  pui32Data 
)

Gets a data element from the SSI receive FIFO.

This function gets received data from the receive FIFO of the specified SSI module and places that data into the location specified by the ui32Data parameter. If there is no data in the FIFO, then this function returns a zero.

Note
Only the lower N bits of the value written to pui32Data contain valid data, where N is the data width as configured by SSIConfigSetExpClk(). For example, if the interface is configured for 8-bit data width, only the lower 8 bits of the value written to pui32Data contain valid data.
Parameters
ui32Basespecifies the SSI module base address.
pui32Datais a pointer to a storage location for data that was received over the SSI interface.
Returns
Returns the number of elements read from the SSI receive FIFO.

Referenced by SSIDisable().

191 {
192  // Check the arguments.
193  ASSERT(SSIBaseValid(ui32Base));
194 
195  // Check for data to read.
196  if(HWREG(ui32Base + SSI_O_SR) & SSI_SR_RNE)
197  {
198  *pui32Data = HWREG(ui32Base + SSI_O_DR);
199  return(1);
200  }
201  else
202  {
203  return(0);
204  }
205 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIDataPut()

void SSIDataPut ( uint32_t  ui32Base,
uint32_t  ui32Data 
)

Puts a data element into the SSI transmit FIFO.

This function places the supplied data into the transmit FIFO of the specified SSI module.

Note
The upper 32 - N bits of the ui32Data are discarded by the hardware, where N is the data width as configured by SSIConfigSetExpClk(). For example, if the interface is configured for 8-bit data width, the upper 24 bits of ui32Data are discarded.
Parameters
ui32Basespecifies the SSI module base address.
ui32Datais the data to be transmitted over the SSI interface.
Returns
None

Referenced by SSIDisable().

149 {
150  // Check the arguments.
151  ASSERT(SSIBaseValid(ui32Base));
152  ASSERT((ui32Data & (0xfffffffe << (HWREG(ui32Base + SSI_O_CR0) &
153  SSI_CR0_DSS_M))) == 0);
154 
155  // Wait until there is space.
156  while(!(HWREG(ui32Base + SSI_O_SR) & SSI_SR_TNF))
157  {
158  }
159 
160  // Write the data to the SSI.
161  HWREG(ui32Base + SSI_O_DR) = ui32Data;
162 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIDataPutNonBlocking()

int32_t SSIDataPutNonBlocking ( uint32_t  ui32Base,
uint32_t  ui32Data 
)

Puts a data element into the SSI transmit FIFO.

This function places the supplied data into the transmit FIFO of the specified SSI module. If there is no space in the FIFO, then this function returns a zero.

Note
The upper 32 - N bits of the ui32Data are discarded by the hardware, where N is the data width as configured by SSIConfigSetExpClk(). For example, if the interface is configured for 8-bit data width, the upper 24 bits of ui32Data are discarded.
Parameters
ui32Basespecifies the SSI module base address.
ui32Datais the data to be transmitted over the SSI interface.
Returns
Returns the number of elements written to the SSI transmit FIFO.

Referenced by SSIDisable().

124 {
125  // Check the arguments.
126  ASSERT(SSIBaseValid(ui32Base));
127  ASSERT((ui32Data & (0xfffffffe << (HWREG(ui32Base + SSI_O_CR0) &
128  SSI_CR0_DSS_M))) == 0);
129 
130  // Check for space to write.
131  if(HWREG(ui32Base + SSI_O_SR) & SSI_SR_TNF)
132  {
133  HWREG(ui32Base + SSI_O_DR) = ui32Data;
134  return(1);
135  }
136  else
137  {
138  return(0);
139  }
140 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIDisable()

static void SSIDisable ( uint32_t  ui32Base)
inlinestatic

Disables the synchronous serial port.

This function disables operation of the synchronous serial port.

Parameters
ui32Basespecifies the SSI module base address.
Returns
None
262 {
263  // Check the arguments.
264  ASSERT(SSIBaseValid(ui32Base));
265 
266  // Read-modify-write the enable bit.
267  HWREG(ui32Base + SSI_O_CR1) &= ~(SSI_CR1_SSE);
268 }
#define ASSERT(expr)
Definition: debug.h:71
Here is the call graph for this function:

§ SSIDMADisable()

static void SSIDMADisable ( uint32_t  ui32Base,
uint32_t  ui32DMAFlags 
)
inlinestatic

Disable SSI DMA operation.

This function is used to disable SSI DMA features that were enabled by SSIDMAEnable(). The specified SSI DMA features are disabled.

Parameters
ui32Baseis the base address of the SSI port.
ui32DMAFlagsis a bit mask of the DMA features to disable. The parameter is the bitwise OR of any of the following values:
Returns
None
635 {
636  // Check the arguments.
637  ASSERT(SSIBaseValid(ui32Base));
638 
639  // Clear the requested bits in the SSI DMA control register.
640  HWREG(ui32Base + SSI_O_DMACR) &= ~ui32DMAFlags;
641 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIDMAEnable()

static void SSIDMAEnable ( uint32_t  ui32Base,
uint32_t  ui32DMAFlags 
)
inlinestatic

Enable SSI DMA operation.

The specified SSI DMA features are enabled. The SSI can be configured to use DMA for transmit and/or receive data transfers.

Note
The uDMA controller must also be set up before DMA can be used with the SSI.
Parameters
ui32Baseis the base address of the SSI port.
ui32DMAFlagsis a bit mask of the DMA features to enable. The parameter is the bitwise OR of any of the following values:
Returns
None
609 {
610  // Check the arguments.
611  ASSERT(SSIBaseValid(ui32Base));
612 
613  // Set the requested bits in the SSI DMA control register.
614  HWREG(ui32Base + SSI_O_DMACR) |= ui32DMAFlags;
615 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIEnable()

static void SSIEnable ( uint32_t  ui32Base)
inlinestatic

Enables the synchronous serial port.

This function enables operation of the synchronous serial port. The synchronous serial port must be configured before it is enabled.

Parameters
ui32Basespecifies the SSI module base address.
Returns
None
241 {
242  // Check the arguments.
243  ASSERT(SSIBaseValid(ui32Base));
244 
245  // Read-modify-write the enable bit.
246  HWREG(ui32Base + SSI_O_CR1) |= SSI_CR1_SSE;
247 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIIntClear()

static void SSIIntClear ( uint32_t  ui32Base,
uint32_t  ui32IntFlags 
)
inlinestatic

Clears SSI interrupt sources.

The specified SSI interrupt sources are cleared so that they no longer assert. This function must be called in the interrupt handler to keep the interrupts from being recognized again immediately upon exit.

Note
Due to write buffers and synchronizers in the system it may take several clock cycles from a register write clearing an event in a module and until the event is actually cleared in the NVIC of the system CPU. It is recommended to clear the event source early in the interrupt service routine (ISR) to allow the event clear to propagate to the NVIC before returning from the ISR. At the same time, an early event clear allows new events of the same type to be pended instead of ignored if the event is cleared later in the ISR. It is the responsibility of the programmer to make sure that enough time has passed before returning from the ISR to avoid false re-triggering of the cleared event. A simple, although not necessarily optimal, way of clearing an event before returning from the ISR is:
  1. Write to clear event (interrupt source). (buffered write)
  2. Dummy read from the event source module. (making sure the write has propagated)
  3. Wait two system CPU clock cycles (user code or two NOPs). (allowing cleared event to propagate through any synchronizers)
Parameters
ui32Basespecifies the SSI module base address.
ui32IntFlagsis a bit mask of the interrupt sources to be cleared. The parameter can consist of either or both of:
Returns
None
542 {
543  // Check the arguments.
544  ASSERT(SSIBaseValid(ui32Base));
545 
546  // Clear the requested interrupt sources.
547  HWREG(ui32Base + SSI_O_ICR) = ui32IntFlags;
548 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIIntDisable()

static void SSIIntDisable ( uint32_t  ui32Base,
uint32_t  ui32IntFlags 
)
inlinestatic

Disables individual SSI interrupt sources.

Disables the indicated SSI interrupt sources.

Parameters
ui32Basespecifies the SSI module base address.
ui32IntFlagsis a bit mask of the interrupt sources to be disabled.
Returns
None
500 {
501  // Check the arguments.
502  ASSERT(SSIBaseValid(ui32Base));
503 
504  // Disable the specified interrupts.
505  HWREG(ui32Base + SSI_O_IMSC) &= ~(ui32IntFlags);
506 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIIntEnable()

static void SSIIntEnable ( uint32_t  ui32Base,
uint32_t  ui32IntFlags 
)
inlinestatic

Enables individual SSI interrupt sources.

Enables the indicated SSI interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
ui32Basespecifies the SSI module base address.
ui32IntFlagsis a bit mask of the interrupt sources to be enabled.
Returns
None
474 {
475  // Check the arguments.
476  ASSERT(SSIBaseValid(ui32Base));
477 
478  // Enable the specified interrupts.
479  HWREG(ui32Base + SSI_O_IMSC) |= ui32IntFlags;
480 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIIntRegister()

void SSIIntRegister ( uint32_t  ui32Base,
void(*)(void)  pfnHandler 
)

Registers an interrupt handler for the Synchronous Serial Interface in the dynamic interrupt table.

Note
Only use this function if you want to use the dynamic vector table (in SRAM)!

This function registers a function as the interrupt handler for a specific interrupt and enables the corresponding interrupt in the interrupt controller.

Specific SSI interrupts must be enabled via SSIIntEnable(). If necessary, it is the interrupt handler's responsibility to clear the interrupt source via SSIIntClear().

Parameters
ui32Basespecifies the SSI module base address.
pfnHandleris a pointer to the function to be called when the synchronous serial port interrupt occurs.
Returns
None
See also
IntRegister() for important information about registering interrupt handlers.

Referenced by SSIStatus().

214 {
215  uint32_t ui32Int;
216 
217  // Check the arguments.
218  ASSERT(SSIBaseValid(ui32Base));
219 
220  // Determine the interrupt number based on the SSI port.
221  ui32Int = (ui32Base == SSI0_BASE) ? INT_SSI0_COMB : INT_SSI1_COMB;
222 
223  // Register the interrupt handler.
224  IntRegister(ui32Int, pfnHandler);
225 
226  // Enable the synchronous serial port interrupt.
227  IntEnable(ui32Int);
228 }
#define ASSERT(expr)
Definition: debug.h:71
void IntRegister(uint32_t ui32Interrupt, void(*pfnHandler)(void))
Registers a function as an interrupt handler in the dynamic vector table.
Definition: interrupt.c:151
void IntEnable(uint32_t ui32Interrupt)
Enables an interrupt or system exception.
Definition: interrupt.c:281
Here is the call graph for this function:

§ SSIIntStatus()

static uint32_t SSIIntStatus ( uint32_t  ui32Base,
bool  bMasked 
)
inlinestatic

Gets the current interrupt status.

This function returns the interrupt status for the SSI module. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.

Parameters
ui32Basespecifies the SSI module base address.
bMaskedselects either raw or masked interrupt. false : Raw interrupt status is required. true : Masked interrupt status is required.
Returns
Returns the current interrupt status as an OR'ed combination of:
572 {
573  // Check the arguments.
574  ASSERT(SSIBaseValid(ui32Base));
575 
576  // Return either the interrupt status or the raw interrupt status as
577  // requested.
578  if(bMasked)
579  {
580  return(HWREG(ui32Base + SSI_O_MIS));
581  }
582  else
583  {
584  return(HWREG(ui32Base + SSI_O_RIS));
585  }
586 }
#define ASSERT(expr)
Definition: debug.h:71

§ SSIIntUnregister()

void SSIIntUnregister ( uint32_t  ui32Base)

Unregisters an interrupt handler for the Synchronous Serial Interface in the dynamic interrupt table.

This function will clear the handler to be called when a SSI interrupt occurs. This will also mask off the interrupt in the interrupt controller so that the interrupt handler no longer is called.

Parameters
ui32Basespecifies the SSI module base address.
Returns
None
See also
IntRegister() for important information about registering interrupt handlers.

Referenced by SSIStatus().

237 {
238  uint32_t ui32Int;
239 
240  // Check the arguments.
241  ASSERT(SSIBaseValid(ui32Base));
242 
243  // Determine the interrupt number based on the SSI port.
244  ui32Int = (ui32Base == SSI0_BASE) ? INT_SSI0_COMB : INT_SSI1_COMB;
245 
246  // Disable the interrupt.
247  IntDisable(ui32Int);
248 
249  // Unregister the interrupt handler.
250  IntUnregister(ui32Int);
251 }
#define ASSERT(expr)
Definition: debug.h:71
void IntUnregister(uint32_t ui32Interrupt)
Unregisters an interrupt handler in the dynamic vector table.
Definition: interrupt.c:187
void IntDisable(uint32_t ui32Interrupt)
Disables an interrupt or system exception.
Definition: interrupt.c:325
Here is the call graph for this function:

§ SSIStatus()

static uint32_t SSIStatus ( uint32_t  ui32Base)
inlinestatic

Get the status of the SSI data buffers.

This function is used to poll the status of the internal FIFOs in the SSI module. The status of both TX and RX FIFO is returned.

Parameters
ui32Basespecifies the SSI module base address.
Returns
Returns the current status of the internal SSI data buffers. The status is a bitwise OR'ed combination of:
403 {
404  // Check the arguments.
405  ASSERT(SSIBaseValid(ui32Base));
406 
407  // Return the status
408  return (HWREG(ui32Base + SSI_O_SR) & SSI_STATUS_MASK);
409 }
#define ASSERT(expr)
Definition: debug.h:71
#define SSI_STATUS_MASK
Definition: ssi.h:112
Here is the call graph for this function:

Macro Definition Documentation

§ SSI_DMA_RX

#define SSI_DMA_RX   0x00000001

§ SSI_DMA_TX

#define SSI_DMA_TX   0x00000002

§ SSI_FRF_MOTO_MODE_0

#define SSI_FRF_MOTO_MODE_0   0x00000000

Referenced by SSIConfigSetExpClk().

§ SSI_FRF_MOTO_MODE_1

#define SSI_FRF_MOTO_MODE_1   0x00000002

Referenced by SSIConfigSetExpClk().

§ SSI_FRF_MOTO_MODE_2

#define SSI_FRF_MOTO_MODE_2   0x00000001

Referenced by SSIConfigSetExpClk().

§ SSI_FRF_MOTO_MODE_3

#define SSI_FRF_MOTO_MODE_3   0x00000003

Referenced by SSIConfigSetExpClk().

§ SSI_FRF_NMW

#define SSI_FRF_NMW   0x00000020

Referenced by SSIConfigSetExpClk().

§ SSI_FRF_TI

#define SSI_FRF_TI   0x00000010

Referenced by SSIConfigSetExpClk().

§ SSI_MODE_MASTER

#define SSI_MODE_MASTER   0x00000000

Referenced by SSIConfigSetExpClk().

§ SSI_MODE_SLAVE

#define SSI_MODE_SLAVE   0x00000001

Referenced by SSIConfigSetExpClk().

§ SSI_MODE_SLAVE_OD

#define SSI_MODE_SLAVE_OD   0x00000002

Referenced by SSIConfigSetExpClk().

§ SSI_RX_FULL

#define SSI_RX_FULL   0x00000008

§ SSI_RX_NOT_EMPTY

#define SSI_RX_NOT_EMPTY   0x00000004

§ SSI_RXFF

#define SSI_RXFF   0x00000004

§ SSI_RXOR

#define SSI_RXOR   0x00000001

§ SSI_RXTO

#define SSI_RXTO   0x00000002

§ SSI_STATUS_MASK

#define SSI_STATUS_MASK   0x0000000F

Referenced by SSIStatus().

§ SSI_TX_EMPTY

#define SSI_TX_EMPTY   0x00000001

§ SSI_TX_NOT_FULL

#define SSI_TX_NOT_FULL   0x00000002

§ SSI_TXFF

#define SSI_TXFF   0x00000008