TI BLE-Stack for Bluetooth 4.2 API Documentation
3.02.03.00
|
Macros | |
#define | SNP_ADV_RESTART_ON_CONN_EST 0x01 |
Advertising will continue with non-connectable advertising when connection is established. period and interval of advertising are different when the device is in a connection. see SNP_startAdv. | |
#define | SNP_ADV_RESTART_ON_CONN_TERM 0x02 |
Advertising will start with connectable advertising when a connection is terminated. | |
#define | SNP_ADV_STOP_ON_CONN 0x00 |
Advertising is disabled during connection and will not start after. | |