SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlDeviceVersionReadResponseFull_t Struct Reference

Data Fields

SlDeviceVersionReadResponsePart_t part
 
_u32 NwpVersion [4]
 
_u16 RomVersion
 
_u16 Padding
 

Detailed Description

Definition at line 497 of file protocol.h.

Field Documentation

§ NwpVersion

_u32 NwpVersion[4]

Definition at line 500 of file protocol.h.

§ Padding

_u16 Padding

Definition at line 502 of file protocol.h.

§ part

Definition at line 499 of file protocol.h.

§ RomVersion

_u16 RomVersion

Definition at line 501 of file protocol.h.


The documentation for this struct was generated from the following file: