Radio Control Layer (RCL)
|
#include <stdint.h>
#include <stddef.h>
#include <stdbool.h>
Go to the source code of this file.
Data Structures | |
struct | LRF_TOPsmImage |
union | LRF_ConfigWord |
struct | LRF_RegConfigList |
struct | LRF_ApplySettingsState |
struct | LRF_ConfigWord.region |
struct | LRF_ConfigWord.sparse |
struct | LRF_ConfigWord.masked |
struct | LRF_ConfigWord.segment |
Macros | |
#define | LRF_TxPower_Use_Min ((LRF_TxPowerTable_Index){.rawValue = -128}) |
#define | LRF_TxPower_Use_Max ((LRF_TxPowerTable_Index){.rawValue = 125}) |
#define | LRF_TxPower_Use_Raw ((LRF_TxPowerTable_Index){.rawValue = 126}) |
#define | LRF_TxPower_None ((LRF_TxPowerTable_Index){.rawValue = 127}) |
#define | LRF_SETTINGS_BUFFER_UNLIMITED 0x3FFF |
#define | LRF_RSSI_INVALID (127) |
#define | LRF_PhyFeatures_Default 0 |
#define | LRF_NUM_CLK_ENA 2 /* Number of clock enable sets */ |
#define | LRF_CLK_ENA_APP 0 /* Clock enable set to use for the application */ |
#define | LRF_CLK_ENA_RCL 1 /* Clock enable set to use by the RCL */ |
#define | __ERROR_Address_is_in_an_invalid_range_for_LRF_setup 0x00040000 |
#define | _ADDRESS_REGION_BIT(_address) |
#define | LRF_SETTINGS_CLEAR(_startAddress, _numWords) |
#define | LRF_SETTINGS_16BIT_BLOCK(_startAddress, _numWords) |
#define | LRF_SETTINGS_16BIT_DUAL_ENTRY(_value0, _value1) (((_value0) & 0xFFFF) | (((_value1) & 0xFFFF) << 16)) |
#define | LRF_SETTINGS_32BIT_BLOCK(_startAddress, _numWords) |
#define | LRF_SETTINGS_16BIT_SPARSE_BLOCK(_startAddress, _numWords) |
#define | LRF_SETTINGS_16BIT_SPARSE_ENTRY(_address, _value) (((((uintptr_t)(_address)) & 0xFFFF) << 16) | ((_value) & 0xFFFF)) |
#define | LRF_SETTINGS_16BIT_MASKED_BLOCK(_startAddress, _numWords) |
#define | LRF_SETTINGS_16BIT_MASKED_ENTRY(_mask, _value) ((((_mask) & 0xFFFF) << 16) | ((_value) & 0xFFFF)) |
Enumerations | |
enum | LRF_RadioState { RadioState_Down = 0, RadioState_ImagesLoaded, RadioState_Configured } |
enum | LRF_SetupResult { SetupResult_Ok, SetupResult_Ok_Partial, SetupResult_ErrorImageLen, SetupResult_ErrorConfigLen, SetupResult_ErrorElemLen, SetupResult_ErrorElemType, SetupResult_ErrorElemAddrAlign, SetupResult_ErrorParRange, SetupResult_ErrorSwConfig } |
Setup operation result. More... | |
enum | LRF_RegionOperation { HW_Region_Clear = 0, HW_Write_16bit = 1, HW_Write_32bit = 2, HW_Write_16bit_sparse = 3, SW_Region_Clear = 4, SW_Write_16bit = 5, SW_Write_32bit = 6, SW_Write_16bit_sparse = 7, Par_Region_Clear = 8, Par_Reference_32bit = 9, Par_Write_32bit = 10, HW_Write_16bit_masked = 11, LRF_RegionOperation_Skip = 254, LRF_RegionOperation_Invalid = 255 } |
enum | LRF_ApplySettingsBase { LRF_ApplySettings_NoBase = 0, LRF_ApplySettings_IncludeBase = 1 } |
Functions | |
LRF_SetupResult | LRF_setupRadio (const LRF_Config *lrfConfig, uint16_t phyFeatures, LRF_RadioState lrfState) |
LRF_SetupResult | LRF_loadImage (const LRF_TOPsmImage *image, uint32_t destinationAddress) |
static void | LRF_resetSettingsState (LRF_ApplySettingsState *state) |
void | LRF_initSettingsState (LRF_ApplySettingsState *state, LRF_ApplySettingsBase includeBase, uint16_t phyFeatures) |
LRF_SetupResult | LRF_applySettings (LRF_ConfigWord *config, LRF_ApplySettingsState *state, int32_t bufferAvailWords) |
void | LRF_enable (void) |
void | LRF_disable (void) |
void | LRF_powerDown (void) |
void | LRF_sendHardStop (void) |
void | LRF_sendGracefulStop (void) |
void | LRF_hardStop (void) |
void | LRF_waitForTopsmReady (void) |
uint32_t | LRF_prepareRxFifo (void) |
uint32_t | LRF_prepareTxFifo (void) |
uint32_t | LRF_peekRxFifo (int32_t offset) |
uint32_t | LRF_peekTxFifo (int32_t offset) |
uint8_t * | LRF_getTxFifoWrAddr (int32_t offset) |
void | LRF_skipTxFifoWords (uint32_t wordLength) |
void | LRF_discardRxFifoWords (uint32_t wordLength) |
void | LRF_readRxFifoWords (uint32_t *data32, uint32_t wordLength) |
void | LRF_writeTxFifoWords (const uint32_t *data32, uint32_t wordLength) |
void | LRF_setRxFifoEffSz (uint32_t maxSz) |
void | LRF_programFrequency (uint32_t frequency, bool tx) |
uint32_t | LRF_enableSynthRefsys (void) |
void | LRF_disableSynthRefsys (void) |
void | LRF_setClockEnable (uint16_t mask, uint8_t entryNumber) |
void | LRF_clearClockEnable (uint16_t mask, uint8_t entryNumber) |
int8_t | LRF_readRssi (void) |
void | LRF_setRawTxPower (uint32_t value, uint32_t temperatureCoefficient) |
LRF_TxPowerTable_Entry | LRF_getRawTxPower (void) |
bool | LRF_imagesNeedUpdate (const LRF_Config *lrfConfig) |
LRF_TxPowerTable_Entry | LRF_TxPowerTable_findValue (const LRF_TxPowerTable *table, LRF_TxPowerTable_Index powerLevel) |
Search for settings corresponding to the highest tx power lower than specified value in the tx power table. More... | |
void | LRF_rclEnableRadioClocks (void) |
void | LRF_rclDisableRadioClocks (void) |
static void | LRF_setAppClockEnable (uint16_t mask) |
static void | LRF_clearAppClockEnable (uint16_t mask) |
Variables | |
uint32_t | swParamList [] |
const size_t | swParamListSz |
union LRF_ConfigWord |
Data Fields | ||
---|---|---|
struct LRF_ConfigWord | region | |
uint32_t | value32 | |
uint16_t | value16[2] | |
struct LRF_ConfigWord | sparse | |
struct LRF_ConfigWord | masked | |
struct LRF_ConfigWord | segment |
struct LRF_RegConfigList_s |
Data Fields | ||
---|---|---|
uint32_t | numEntries | |
LRF_ConfigWord * | entries[] |
struct LRF_ApplySettingsState |
Data Fields | ||
---|---|---|
uint16_t | phyFeatures | |
LRF_ApplySettingsBase | includeBase |
struct LRF_ConfigWord.region |
struct LRF_ConfigWord.segment |
#define LRF_TxPower_Use_Min ((LRF_TxPowerTable_Index){.rawValue = -128}) |
Special value given as a TX power to indicate that the lowest available TX power is requested
#define LRF_TxPower_Use_Max ((LRF_TxPowerTable_Index){.rawValue = 125}) |
Special value given as a TX power to indicate that the highest available TX power is requested
#define LRF_TxPower_Use_Raw ((LRF_TxPowerTable_Index){.rawValue = 126}) |
Special value given as a TX power to indicate that a given raw TX power register setting should be used.
#define LRF_TxPower_None ((LRF_TxPowerTable_Index){.rawValue = 127}) |
Special value given as a TX power to indicate that a TX power should not be programmed; instead, use the register value written through settings or register write.
#define LRF_SETTINGS_BUFFER_UNLIMITED 0x3FFF |
Buffer available limit when no limit exists
#define LRF_RSSI_INVALID (127) |
RSSI value indicating an invalid RSSI
#define LRF_PhyFeatures_Default 0 |
#define LRF_NUM_CLK_ENA 2 /* Number of clock enable sets */ |
#define LRF_CLK_ENA_APP 0 /* Clock enable set to use for the application */ |
#define LRF_CLK_ENA_RCL 1 /* Clock enable set to use by the RCL */ |
#define __ERROR_Address_is_in_an_invalid_range_for_LRF_setup 0x00040000 |
#define _ADDRESS_REGION_BIT | ( | _address | ) |
#define LRF_SETTINGS_CLEAR | ( | _startAddress, | |
_numWords | |||
) |
#define LRF_SETTINGS_16BIT_BLOCK | ( | _startAddress, | |
_numWords | |||
) |
#define LRF_SETTINGS_16BIT_DUAL_ENTRY | ( | _value0, | |
_value1 | |||
) | (((_value0) & 0xFFFF) | (((_value1) & 0xFFFF) << 16)) |
#define LRF_SETTINGS_32BIT_BLOCK | ( | _startAddress, | |
_numWords | |||
) |
#define LRF_SETTINGS_16BIT_SPARSE_BLOCK | ( | _startAddress, | |
_numWords | |||
) |
#define LRF_SETTINGS_16BIT_SPARSE_ENTRY | ( | _address, | |
_value | |||
) | (((((uintptr_t)(_address)) & 0xFFFF) << 16) | ((_value) & 0xFFFF)) |
#define LRF_SETTINGS_16BIT_MASKED_BLOCK | ( | _startAddress, | |
_numWords | |||
) |
#define LRF_SETTINGS_16BIT_MASKED_ENTRY | ( | _mask, | |
_value | |||
) | ((((_mask) & 0xFFFF) << 16) | ((_value) & 0xFFFF)) |
enum LRF_RadioState |
enum LRF_SetupResult |
Setup operation result.
enum LRF_RegionOperation |
LRF_SetupResult LRF_setupRadio | ( | const LRF_Config * | lrfConfig, |
uint16_t | phyFeatures, | ||
LRF_RadioState | lrfState | ||
) |
References LRF_applySettings(), LRF_ApplySettings_IncludeBase, LRF_ApplySettings_NoBase, LRF_applyTrim(), LRF_initSettingsState(), LRF_loadImage(), LRF_RSSI_INVALID, LRF_setTemperatureTrim(), LRF_SETTINGS_BUFFER_UNLIMITED, LRF_updateTrim(), lrfPhyState, MCE_RAM_BASE_ADDR, LRF_Config::mceImage, PBE_RAM_BASE_ADDR, LRF_Config::pbeImage, RadioState_Configured, RadioState_ImagesLoaded, LRF_Config::regConfigList, RFE_RAM_BASE_ADDR, LRF_Config::rfeImage, SetupResult_ErrorSwConfig, SetupResult_Ok, LRF_SwParam::swConfig, swParamList, and LRF_SwParam::trimDef.
Referenced by RCL_Lite_configSetPhyFeatures(), RCL_Lite_setPhyFeatures(), and rclCommandHwi().
LRF_SetupResult LRF_loadImage | ( | const LRF_TOPsmImage * | image, |
uint32_t | destinationAddress | ||
) |
References SetupResult_ErrorImageLen, SetupResult_Ok, and TOPSM_RAM_SZ.
Referenced by LRF_setupRadio().
|
inlinestatic |
Referenced by LRF_initSettingsState().
void LRF_initSettingsState | ( | LRF_ApplySettingsState * | state, |
LRF_ApplySettingsBase | includeBase, | ||
uint16_t | phyFeatures | ||
) |
References LRF_ApplySettingsState::includeBase, LRF_resetSettingsState(), and LRF_ApplySettingsState::phyFeatures.
Referenced by LRF_setupRadio().
LRF_SetupResult LRF_applySettings | ( | LRF_ConfigWord * | config, |
LRF_ApplySettingsState * | state, | ||
int32_t | bufferAvailWords | ||
) |
References HW_Region_Clear, HW_Write_16bit, HW_Write_16bit_masked, HW_Write_16bit_sparse, HW_Write_32bit, LRF_ApplySettingsState::includeBase, LRF_BASE_ADDR, LRF_RegionOperation_Invalid, LRF_RegionOperation_Skip, LRF_ConfigWord::masked, MAX_REG_CONFIG_LEN, Par_Reference_32bit, Par_Region_Clear, Par_Write_32bit, PBE_RAM_BASE_ADDR, LRF_ApplySettingsState::phyFeatures, RCL_Debug_assert, LRF_ConfigWord::region, LRF_ConfigWord::segment, SetupResult_ErrorConfigLen, SetupResult_ErrorElemAddrAlign, SetupResult_ErrorElemLen, SetupResult_ErrorElemType, SetupResult_ErrorParRange, SetupResult_Ok, SetupResult_Ok_Partial, LRF_ConfigWord::sparse, SW_Region_Clear, SW_Write_16bit, SW_Write_16bit_sparse, SW_Write_32bit, swParamList, swParamListSz, LRF_ConfigWord::value16, and LRF_ConfigWord::value32.
Referenced by LRF_setupRadio().
void LRF_enable | ( | void | ) |
Referenced by RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_dtmTx(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_genericTx(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Ble5_txTest(), RCL_Handler_BLE_CS(), RCL_Handler_Generic_Fs(), RCL_Handler_Generic_FsOff(), RCL_Handler_Generic_PbeOperation(), RCL_Handler_Generic_Rx(), RCL_Handler_Generic_Tx(), RCL_Handler_Generic_TxRepeat(), RCL_Handler_Generic_TxTest(), RCL_Handler_Nesb_Prx(), and RCL_Handler_Nesb_Ptx().
void LRF_disable | ( | void | ) |
Referenced by RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_dtmTx(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_genericTx(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Ble5_txTest(), RCL_Handler_BLE_CS(), RCL_Handler_Generic_Fs(), RCL_Handler_Generic_FsOff(), RCL_Handler_Generic_PbeOperation(), RCL_Handler_Generic_Rx(), RCL_Handler_Generic_Tx(), RCL_Handler_Generic_TxRepeat(), RCL_Handler_Generic_TxTest(), RCL_Handler_Nesb_Prx(), and RCL_Handler_Nesb_Ptx().
void LRF_powerDown | ( | void | ) |
void LRF_sendHardStop | ( | void | ) |
Referenced by RCL_Command_stop(), and RCL_Lite_Command_stop().
void LRF_sendGracefulStop | ( | void | ) |
Referenced by RCL_Command_stop(), and RCL_Lite_Command_stop().
void LRF_hardStop | ( | void | ) |
Referenced by RCL_Lite_CommandHwi(), and rclCommandHwi().
void LRF_waitForTopsmReady | ( | void | ) |
Referenced by RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_dtmTx(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_genericTx(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Ble5_txTest(), RCL_Handler_BLE_CS(), RCL_Handler_Generic_Fs(), RCL_Handler_Generic_FsOff(), RCL_Handler_Generic_PbeOperation(), RCL_Handler_Generic_Rx(), RCL_Handler_Generic_Tx(), RCL_Handler_Generic_TxRepeat(), RCL_Handler_Generic_TxTest(), RCL_Handler_Nesb_Prx(), and RCL_Handler_Nesb_Ptx().
uint32_t LRF_prepareRxFifo | ( | void | ) |
uint32_t LRF_prepareTxFifo | ( | void | ) |
uint32_t LRF_peekRxFifo | ( | int32_t | offset | ) |
uint32_t LRF_peekTxFifo | ( | int32_t | offset | ) |
References BUF_RAM_BASE_ADDR.
uint8_t* LRF_getTxFifoWrAddr | ( | int32_t | offset | ) |
References BUF_RAM_BASE_ADDR.
Referenced by RCL_Handler_BLE5_scan_init(), and RCL_Handler_BLE5_updateTxBuffers().
void LRF_skipTxFifoWords | ( | uint32_t | wordLength | ) |
Referenced by RCL_Handler_BLE5_updateTxBuffers().
void LRF_discardRxFifoWords | ( | uint32_t | wordLength | ) |
Referenced by RCL_Handler_BLE5_genericRx(), RCL_Handler_Generic_Rx(), and RCL_Handler_Nesb_Prx().
void LRF_readRxFifoWords | ( | uint32_t * | data32, |
uint32_t | wordLength | ||
) |
void LRF_writeTxFifoWords | ( | const uint32_t * | data32, |
uint32_t | wordLength | ||
) |
void LRF_setRxFifoEffSz | ( | uint32_t | maxSz | ) |
void LRF_programFrequency | ( | uint32_t | frequency, |
bool | tx | ||
) |
References LRF_findCalM(), LRF_findFoff(), LRF_findPllM(), LRF_programCMixN(), LRF_programPQ(), LRF_programShape(), LRF_scaleFreqWithHFXTOffset(), LRF_SwConfig::modFrequencyDeviation, LRF_SwConfig::rxFrequencyOffset, LRF_SwConfig::rxIntFrequency, LRF_SwParam::swConfig, swParamList, LRF_SwConfig::txFrequencyOffset, and LRF_SwConfig::txShape.
Referenced by RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_dtmTx(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_genericTx(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Ble5_txTest(), RCL_Handler_Generic_Fs(), RCL_Handler_Generic_Rx(), RCL_Handler_Generic_Tx(), RCL_Handler_Generic_TxRepeat(), RCL_Handler_Generic_TxTest(), RCL_Handler_Nesb_Prx(), and RCL_Handler_Nesb_Ptx().
uint32_t LRF_enableSynthRefsys | ( | void | ) |
References LRF_REFSYS_ENABLE_TIME, and RCL_Scheduler_getCurrentTime().
Referenced by RCL_Handler_ADC_Noise_getNoise(), RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_dtmTx(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_genericTx(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Ble5_txTest(), RCL_Handler_BLE_CS(), RCL_Handler_Generic_Fs(), RCL_Handler_Generic_Rx(), RCL_Handler_Generic_Tx(), RCL_Handler_Generic_TxRepeat(), RCL_Handler_Generic_TxTest(), RCL_Handler_Nesb_Prx(), and RCL_Handler_Nesb_Ptx().
void LRF_disableSynthRefsys | ( | void | ) |
Referenced by RCL_Handler_ADC_Noise_getNoise(), RCL_Handler_Adc_Noise_powerDown(), RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_dtmTx(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_genericTx(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Ble5_txTest(), RCL_Handler_BLE_CS(), and RCL_Handler_Generic_setSynthPowerState().
void LRF_setClockEnable | ( | uint16_t | mask, |
uint8_t | entryNumber | ||
) |
void LRF_clearClockEnable | ( | uint16_t | mask, |
uint8_t | entryNumber | ||
) |
References LRF_applyNewClockEnable(), LRF_NUM_CLK_ENA, and lrfPhyState.
Referenced by LRF_clearAppClockEnable(), LRF_rclDisableRadioClocks(), and RCL_Handler_Adc_Noise_powerDown().
int8_t LRF_readRssi | ( | void | ) |
Referenced by RCL_Lite_readRssi(), and RCL_readRssi().
void LRF_setRawTxPower | ( | uint32_t | value, |
uint32_t | temperatureCoefficient | ||
) |
References LRF_TxPower_Use_Raw, and lrfPhyState.
Referenced by RCL_Command_setRawTxPower().
LRF_TxPowerTable_Entry LRF_getRawTxPower | ( | void | ) |
References LRF_TxPower_Use_Raw, LRF_TxPowerEntry_INVALID_VALUE, and lrfPhyState.
Referenced by LRF_TxPowerTable_findValue().
bool LRF_imagesNeedUpdate | ( | const LRF_Config * | lrfConfig | ) |
References lrfPhyState, LRF_Config::mceImage, LRF_Config::pbeImage, and LRF_Config::rfeImage.
Referenced by rclSchedulerHwi().
LRF_TxPowerTable_Entry LRF_TxPowerTable_findValue | ( | const LRF_TxPowerTable * | table, |
LRF_TxPowerTable_Index | powerLevel | ||
) |
Search for settings corresponding to the highest tx power lower than specified value in the tx power table.
table | pointer to the tx power table to be searched |
powerLevel | maximum allowed power level |
References LRF_getRawTxPower(), LRF_TxPower_Use_Max, LRF_TxPower_Use_Min, LRF_TxPower_Use_Raw, LRF_TxPowerEntry_INVALID_VALUE, LRF_TxPowerTable::numEntries, LRF_TxPowerTable_Entry::power, LRF_TxPowerTable::powerTable, and LRF_TxPowerTable_Index::rawValue.
Referenced by LRF_programTxPower().
void LRF_rclEnableRadioClocks | ( | void | ) |
References LRF_CLK_ENA_RCL, and LRF_setClockEnable().
Referenced by RCL_Lite_configSetPhyFeatures(), RCL_open(), and rclPowerNotify().
void LRF_rclDisableRadioClocks | ( | void | ) |
References LRF_clearClockEnable(), and LRF_CLK_ENA_RCL.
Referenced by RCL_close().
|
inlinestatic |
References LRF_CLK_ENA_APP, and LRF_setClockEnable().
Referenced by RCL_AdcNoise_get_samples_blocking(), and RCL_AdcNoise_get_samples_callback().
|
inlinestatic |
References LRF_clearClockEnable(), and LRF_CLK_ENA_APP.
Referenced by adcNoiseCallback(), and RCL_AdcNoise_get_samples_blocking().
uint32_t swParamList[] |
Referenced by LRF_applySettings(), LRF_programFrequency(), LRF_programTxPower(), and LRF_setupRadio().
const size_t swParamListSz |
Referenced by LRF_applySettings().