Data Structures | Typedefs | Variables
PWMTimerLPF3.h File Reference

Detailed Description

PWM driver implementation for Low Power F3 devices.


Overview

The general PWM API should be used in application code, i.e. PWM_open() should be used instead of PWMTimerLPF3_open(). The board file will define the device specific config, and casting in the general API will ensure that the correct device specific functions are called.

General Behavior

Before using PWM on LPF3:

Error handling

If unsupported arguments are provided to an API returning an error code, the PWM configuration will not be updated and PWM will stay in the mode it was already configured to.

Power Management

The SimpleLink power management framework will try to put the device into the most power efficient mode whenever possible. Please see the technical reference manual for further details on each power mode.

The PWMTimerLPF3.h driver is not explicitly setting a power constraint when the PWM is running to prevent standby as this is assumed to be done in the underlying LGPTimer driver. The following statements are valid:

Accuracy

The PWM output period and duty cycle are limited by the underlying timer. The LGPT peripherals have the following counter widths:

Note that some LPF3 device types do not support all four LGPT peripherals.

The frequency of the underlying timer counter can be divided by configuring the preScalerDivision element of the PWMTimerLPF3_HwAttrs struct. This configuration can be used to extend the PWM signal period but will decrease the accuracy. The minimum obtainable PWM signal frequency is dependent on the width of the counter for the LGPT peripheral used and the configured preScalerDivision value. When using the LGPT3 peripheral with the default preScalerDivision value of 1, the minimal frequency is 48MHz / (2^24-1) = 2.86Hz (349.525ms).

When using high output frequencies the duty cycle resolution is reduced correspondingly. For a 24MHz PWM only a 0%/50%/100% duty is available as the timer uses only counts 0 and 1. Similarly for a 12MHz period the duty cycle will be limited to a 12.5% resolution.

Note
The PWM signals are generated by the LGPT peripheral using the timer clock which is dependent on the high frequency clock (CLKSVT).

Limitations

Basic PWM output

The below example will output a 8MHz PWM signal with 50% duty cycle.

PWM_Handle pwmHandle;
PWM_Params_init(&params);
params.periodValue = 8e6;
params.dutyValue = PWM_DUTY_FRACTION_MAX / 2;
pwmHandle = PWM_open(CONFIG_PWM0, &params);
if(pwmHandle == NULL) {
Log_error0("Failed to open PWM");
Task_exit();
}
PWM_start(pwmHandle);
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/PWM.h>
#include <ti/drivers/timer/LGPTimerLPF3.h>
Include dependency graph for PWMTimerLPF3.h:

Go to the source code of this file.

Data Structures

struct  PWMTimerLPF3_HwAttrs
 PWMTimerLPF3 Hardware attributes. More...
 
struct  PWMTimerLPF3_Object
 PWMTimerLPF3 Object. More...
 

Macros

PWMTimerLPF3 specific control commands and arguments
#define PWMTimerLPF3_CMD_DEBUG_STALL
 
Arguments for PWMTimerLPF3_CMD_DEBUG_STALL
#define CMD_ARG_DEBUG_STALL_OFF
 
#define CMD_ARG_DEBUG_STALL_ON
 

Typedefs

typedef struct PWMTimerLPF3_HwAttrs PWMTimerLPF3_HwAttrs
 PWMTimerLPF3 Hardware attributes. More...
 
typedef struct PWMTimerLPF3_Object PWMTimerLPF3_Object
 PWMTimerLPF3 Object. More...
 

Variables

const PWM_FxnTable PWMTimerLPF3_fxnTable
 

Macro Definition Documentation

§ PWMTimerLPF3_CMD_DEBUG_STALL

#define PWMTimerLPF3_CMD_DEBUG_STALL

Timer debug stall mode (stop PWM output debugger halts CPU) When enabled, PWM output will be HIGH when CPU is halted

§ CMD_ARG_DEBUG_STALL_OFF

#define CMD_ARG_DEBUG_STALL_OFF

§ CMD_ARG_DEBUG_STALL_ON

#define CMD_ARG_DEBUG_STALL_ON

Typedef Documentation

§ PWMTimerLPF3_HwAttrs

PWMTimerLPF3 Hardware attributes.

These fields are used by the driver to set up the underlying LGPTimer driver statically.

§ PWMTimerLPF3_Object

PWMTimerLPF3 Object.

These fields are used by the driver to store and modify PWM configuration during run-time. The application must not edit any member variables of this structure. Applications should also not access member variables of this structure as backwards compatibility is not guaranteed.

Variable Documentation

§ PWMTimerLPF3_fxnTable

const PWM_FxnTable PWMTimerLPF3_fxnTable
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale