TI-RTOS Drivers  tidrivers_cc13xx_cc26xx_2_21_00_04
Macros | Functions
SensorBmp280.h File Reference

Detailed Description

Driver for the Bosch BMP280 Pressure Sensor.

============================================================================


#include "stdint.h"
#include "stdbool.h"
Include dependency graph for SensorBmp280.h:

Go to the source code of this file.

Macros

#define SENSOR_BMP280_DATASIZE   6
 

Functions

bool SensorBmp280_init (void)
 
void SensorBmp280_enable (bool enable)
 
bool SensorBmp280_test (void)
 
bool SensorBmp280_read (uint8_t *pBuf)
 
void SensorBmp280_convert (uint8_t *raw, int32_t *temp, uint32_t *press)
 

Macro Definition Documentation

#define SENSOR_BMP280_DATASIZE   6

Function Documentation

bool SensorBmp280_init ( void  )
void SensorBmp280_enable ( bool  enable)
bool SensorBmp280_test ( void  )
bool SensorBmp280_read ( uint8_t *  pBuf)
void SensorBmp280_convert ( uint8_t *  raw,
int32_t *  temp,
uint32_t *  press 
)
Copyright 2016, Texas Instruments Incorporated