![]() |
![]() |
Contains the states for the flux estimator (EST_Flux) module routines.
Go to the source code of this file.
Enumerations | |
enum | EST_Flux_ErrorCode_e { EST_FLUX_ERRORCODE_NOERROR =0, EST_FLUX_ERRORCODE_SHIFTOVERFLOW, EST_FLUX_ERRORCODE_CLIP, EST_FLUX_NUMERRORCODES, EST_FLUX_ERRORCODE_NOERROR =0, EST_FLUX_ERRORCODE_SHIFTOVERFLOW, EST_FLUX_ERRORCODE_CLIP, EST_FLUX_NUMERRORCODES } |
Enumeration for the estimator error codes. More... | |
enum | EST_Flux_State_e { EST_FLUX_STATE_ERROR = 0, EST_FLUX_STATE_IDLE = 1, EST_FLUX_STATE_CL1 = 2, EST_FLUX_STATE_CL2 = 3, EST_FLUX_STATE_FINE = 4, EST_FLUX_STATE_DONE = 5, EST_FLUX_NUMSTATES = 6, EST_FLUX_STATE_ERROR = 0, EST_FLUX_STATE_IDLE = 1, EST_FLUX_STATE_CL1 = 2, EST_FLUX_STATE_CL2 = 3, EST_FLUX_STATE_FINE = 4, EST_FLUX_STATE_DONE = 5, EST_FLUX_NUMSTATES = 6 } |
Enumeration for the estimator states. More... | |