![]() |
![]() |
Files | |
file | include/est.h [code] |
Contains the public interface to the estimator (EST) module routines. | |
file | include/est_Flux_states.h [code] |
Contains the states for the flux estimator (EST_Flux) module routines. | |
file | include/est_Ls_states.h [code] |
Contains the states for the stator inductance estimator (EST_Ls) module routines. | |
file | include/est_Rr_states.h [code] |
Contains the public interface to the rotor resistance estimator (EST_Rr) module routines. | |
file | include/est_Rs_states.h [code] |
Contains the public interface to the stator resistance estimator (EST_Rs) module routines. | |
file | include/est_states.h [code] |
file | include/est_Traj_states.h [code] |
Contains the states for the flux estimator (EST_Flux) module routines. | |
file | include/motor.h [code] |
file | include/userParams.h [code] |