![]() |
![]() |
Contains the states for the stator inductance estimator (EST_Ls) module routines.
Go to the source code of this file.
Enumerations | |
enum | EST_Ls_ErrorCode_e { EST_LS_ERRORCODE_NOERROR =0, EST_LS_ERRORCODE_SHIFTOVERFLOW, EST_LS_NUMERRORCODES, EST_LS_ERRORCODE_NOERROR =0, EST_LS_ERRORCODE_SHIFTOVERFLOW, EST_LS_NUMERRORCODES } |
Enumeration for the stator inductance estimator error codes. More... | |
enum | EST_Ls_State_e { EST_LS_STATE_ERROR = 0, EST_LS_STATE_IDLE = 1, EST_LS_STATE_RAMPUP = 2, EST_LS_STATE_INIT = 3, EST_LS_STATE_COARSE = 4, EST_LS_STATE_FINE = 5, EST_LS_STATE_DONE = 6, EST_LS_NUMSTATES = 7, EST_LS_STATE_ERROR = 0, EST_LS_STATE_IDLE = 1, EST_LS_STATE_RAMPUP = 2, EST_LS_STATE_INIT = 3, EST_LS_STATE_COARSE = 4, EST_LS_STATE_FINE = 5, EST_LS_STATE_DONE = 6, EST_LS_NUMSTATES = 7 } |
Enumeration for the stator inductance estimator states. More... | |