Go to the documentation of this file.
37 #ifndef EST_RS_STATES_H
38 #define EST_RS_STATES_H
95 #endif // end of EST_RS_STATES_H definition
the fine estimation state
Definition: include/est_Rs_states.h:76
idle
Definition: include/est_Rs_states.h:73
the coarse estimation state
Definition: include/est_Rs_states.h:75
number of stator resistance estimator states
Definition: include/est_Rs_states.h:78
the Id ramp up state
Definition: include/est_Rs_states.h:74
the done state
Definition: include/est_Rs_states.h:77
error
Definition: include/est_Rs_states.h:72
EST_Rs_State_e
Enumeration for the stator resistance estimator states.
Definition: include/est_Rs_states.h:70
Copyright 2023, Texas Instruments Incorporated