Go to the documentation of this file.
37 #ifndef EST_RR_STATES_H
38 #define EST_RR_STATES_H
94 #endif // end of EST_RR_STATES_H definition
EST_Rr_State_e
Enumeration for the rotor resistance estimator states.
Definition: lib/include/est_Rr_states.h:70
the done state
Definition: lib/include/est_Rr_states.h:76
the coarse estimation state
Definition: lib/include/est_Rr_states.h:74
number of stator resistance estimator states
Definition: lib/include/est_Rr_states.h:77
the Id ramp up state
Definition: lib/include/est_Rr_states.h:73
error
Definition: lib/include/est_Rr_states.h:71
the fine estimation state
Definition: lib/include/est_Rr_states.h:75
idle
Definition: lib/include/est_Rr_states.h:72
Copyright 2023, Texas Instruments Incorporated